Sensors
  • Technologies
  • More
Sensors
Sensor Forum AHT10 - I2C problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 344 subscribers
  • Views 13234 views
  • Users 0 members are here
  • sensors
  • AHT10
Related

AHT10 - I2C problem

msimon
msimon over 3 years ago

I just bought AHT10 humidity and temperature sensor. I have seen that it supports I2C and it is cheap so I didn't think thoroughly and bought two. I wanted to try them then I encounter a problem that only a single AHT10 can be connected to single I2C bus. I thought it is related to static address but it is worse (breakout board also showing two address but no details in the datasheet). The datasheet says that "Only a single AHT10 can be connected to the I2C bus and no other I2C devices can be connected." It sounds like traditional serial communication like RS232 not I2C. 

Is it normal to advertise it as an I2C device? and I also wonder what is the technical issue preventing to connect other devices with different address. Did you have any experience similar to this on any other sensor?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 3 years ago +4
    Have you tried using the AHT10 with another device on the same I²C bus to see what happens ? It may be that it doesn't observe the stop condition so doesn't release itself from the host and continues…
  • BigG
    BigG over 3 years ago in reply to beacon_dave +4
    Both datasheets (AHT10 & AHT20) show that the sensor operates on microAmps, so powering by GPIO is possible too...
  • michaelkellett
    michaelkellett over 3 years ago +3
    I had a quick look at the data sheet. They don't appear to offer an explanation for why it doesn't work with other devices. I've used several other I2C humidity sensors and lots of I2C devices of other…
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    It might be possible to use two or more AHT10 devices with a 'chip select' type setup.

    The AHT20 data sheet shows a power control application design like this for power saving applications which may be able to be applied to the AHT10: 

    image

    'GND_CTRL' effectively becomes a chip select line allowing you to activate the device you want to communicate with using the same I²C addresses.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 3 years ago in reply to beacon_dave

    Both datasheets (AHT10 & AHT20) show that the sensor operates on microAmps, so powering by GPIO is possible too...

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to BigG

    That design disconnects the I²C bus pull-up resistors from VDD presumably to prevent current drain through the pull-ups and driver IC to ground in power saving applications.

    If not concerned about power saving, then another approach may be to leave the sensor powered and look at connecting/disconnecting the SDA/SCL lines from the I²C bus with the 'chip select'.

    Keeping the sensor powered may improve measurement accuracy if it requires time to stabilise after power up. Although a 'chip deselect' approach may also work here or simply factoring in stabilisation times prior to a measurement.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • msimon
    msimon over 3 years ago in reply to BigG

    Hi  BigG, I will try it to see it works or not. Sounds logical but I am not sure if the product brings other problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • msimon
    msimon over 3 years ago in reply to beacon_dave

    Hi  beacon_dave ,  it takes around 20 ms to reach idle state. I am gonna use it measure hive temperature. So power efficiency is more important than the timing. I will try to select the sensor with power line and see how it works. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • msimon
    msimon over 3 years ago in reply to BigG

    I connected two sensors on the same bus and then connect their Vin pins to GPIO. I also attach another I2C sensor TMP102.  It looks like working but there is a reliability issue. Sometimes it stops. I also suspect the serial port of Arduino IDE. I will check that. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • msimon
    msimon over 3 years ago in reply to BigG

    I connected two sensors on the same bus and then connect their Vin pins to GPIO. I also attach another I2C sensor TMP102.  It looks like working but there is a reliability issue. Sometimes it stops. I also suspect the serial port of Arduino IDE. I will check that.