Sensors
  • Technologies
  • More
Sensors
Sensor Forum AHT10 - I2C problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 344 subscribers
  • Views 13260 views
  • Users 0 members are here
  • sensors
  • AHT10
Related

AHT10 - I2C problem

msimon
msimon over 3 years ago

I just bought AHT10 humidity and temperature sensor. I have seen that it supports I2C and it is cheap so I didn't think thoroughly and bought two. I wanted to try them then I encounter a problem that only a single AHT10 can be connected to single I2C bus. I thought it is related to static address but it is worse (breakout board also showing two address but no details in the datasheet). The datasheet says that "Only a single AHT10 can be connected to the I2C bus and no other I2C devices can be connected." It sounds like traditional serial communication like RS232 not I2C. 

Is it normal to advertise it as an I2C device? and I also wonder what is the technical issue preventing to connect other devices with different address. Did you have any experience similar to this on any other sensor?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 3 years ago +4
    Have you tried using the AHT10 with another device on the same I²C bus to see what happens ? It may be that it doesn't observe the stop condition so doesn't release itself from the host and continues…
  • BigG
    BigG over 3 years ago in reply to beacon_dave +4
    Both datasheets (AHT10 & AHT20) show that the sensor operates on microAmps, so powering by GPIO is possible too...
  • michaelkellett
    michaelkellett over 3 years ago +3
    I had a quick look at the data sheet. They don't appear to offer an explanation for why it doesn't work with other devices. I've used several other I2C humidity sensors and lots of I2C devices of other…
Parents
  • jerosq
    jerosq over 2 years ago

    Hi msimon ! I just ordered a couple ATH10 sensors without thinking much about it and when I downloaded the datasheet to start coding in advance I found the very sentence you are mentioning: "Only a single AHT10 can be connected to the I2C bus and no other I2C devices can be connected". I read this whole thread but I wanted to ask if you were able to share the I2C bus with other devices and if so, which ones ? 

    My idea is to also include a BMP180 atmospheric pressure sensor, as well as a I2C LCD display. Of course, they have different addresses, so in theory it should work, but this claim on the datasheet is alarming. I read about that library to make I2C work with any two pins, but I just couldn't understand how to couple that with the AHTxx or AHT10 library. It goes a bit over my head, and I couldn't find any examples.

    On a side note, were you able to change the address by moving the resistor? Did it work normally with address 0x39? 

    Thanks in advance, this thread alone has been super informative so far. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jerosq
    jerosq over 2 years ago in reply to jerosq

    UPDATE: 

    Sensors have arrived. It definitely seems like a translation error, as I was able to share the bus with the BMP180 sensor with no issues.

    Regarding the address change, I managed to move the resistor to the 0x39 spot and after wrestling a bit with the library I managed to get it working in said address. I'm yet to connect two sensors (0x38 & 0x39) simultaneously, but I think it'll work.

    Maybe the ATH10 wasn't as bad as I expected when reading about it in forums! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jerosq
    jerosq over 2 years ago in reply to jerosq

    UPDATE: 

    Sensors have arrived. It definitely seems like a translation error, as I was able to share the bus with the BMP180 sensor with no issues.

    Regarding the address change, I managed to move the resistor to the 0x39 spot and after wrestling a bit with the library I managed to get it working in said address. I'm yet to connect two sensors (0x38 & 0x39) simultaneously, but I think it'll work.

    Maybe the ATH10 wasn't as bad as I expected when reading about it in forums!