Sensors
  • Technologies
  • More
Sensors
Sensor Forum Temperature sensor accuracy
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Subscribers 345 subscribers
  • Views 8835 views
  • Users 0 members are here
  • temperature
  • temperature sensor
Related

Temperature sensor accuracy

ntewinkel
ntewinkel over 2 years ago

Hi all,

I have two temperature sensors near each other, outside. In the winter I was using one to keep track of the nectar temperature in a hummingbird feeder, but I just left it hanging there for the summer.

Here is the typical result:

image

The top line is a dht11 or could be 12. It includes pressure and humidity. The bottom line is a ds18b20 in a metal tube.

Both are digital, but one is nearly always about 1 or 2 degrees higher than the other. Generally it’s fine to give me a close enough idea of what’s going on, but I think I should be more accurate when looking at the freezing point.

Do I need to calibrate them? How would I go about doing that? Ie, what can I trust as a proper baseline? I don’t have access to any really guaranteed kind of thermometer, I think. Thinking 

Thanks in advance for any wisdom you can send my way!

-Nico

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +5 verified
    If they are waterproof you can stick them in a slush of ice and water to get a zero degrees reference. If they aren't waterproof you can put them in a plastic bag in the ice/water mix. If they can take…
  • beacon_dave
    beacon_dave over 2 years ago +5 verified
    Comparing data sheets it looks like the accuracy of the DHT11 is ±2°C whereas the DS18B20 is ±0.5°C It will be interesting to see what your testing shows.
  • wolfgangfriedrich
    wolfgangfriedrich over 2 years ago in reply to dougw +4 verified
    During the ice-water test, you have to be careful not to touch the ice-cubes. They are still colder than zero degC. I learnt this during a thermocouple roadtest.
Parents
  • dougw
    +1 dougw over 2 years ago

    If they are waterproof you can stick them in a slush of ice and water to get a zero degrees reference. If they aren't waterproof you can put them in a plastic bag in the ice/water mix.

    If they can take 100 degrees, you can put them in a plastic bag in boiling water for a second reference point.

    This will tell you which sensor is more accurate and allows 2-point (linear curve fit) calibration.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 2 years ago in reply to dougw

    Thanks Doug!

    I think the ds18b20 is water proof, I’ll give that a shot.

    I didn’t realize these things needed the ole physics class tricks to get them set up!

    And then do I just add or subtract from the readings they give?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 2 years ago in reply to dougw

    Thanks Doug!

    I think the ds18b20 is water proof, I’ll give that a shot.

    I didn’t realize these things needed the ole physics class tricks to get them set up!

    And then do I just add or subtract from the readings they give?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 2 years ago in reply to ntewinkel

    If a subtraction fixes both zero and 100 than that is all that is needed. If it doesn't fix both readings, you need to add or subtract a number and multiply by a scaling factor so that the result matches both at 0 and at 100. If you publish your readings we can explain how to calibrate them.