Sensors
  • Technologies
  • More
Sensors
Sensor Forum Temperature sensor accuracy
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Subscribers 345 subscribers
  • Views 8840 views
  • Users 0 members are here
  • temperature
  • temperature sensor
Related

Temperature sensor accuracy

ntewinkel
ntewinkel over 2 years ago

Hi all,

I have two temperature sensors near each other, outside. In the winter I was using one to keep track of the nectar temperature in a hummingbird feeder, but I just left it hanging there for the summer.

Here is the typical result:

image

The top line is a dht11 or could be 12. It includes pressure and humidity. The bottom line is a ds18b20 in a metal tube.

Both are digital, but one is nearly always about 1 or 2 degrees higher than the other. Generally it’s fine to give me a close enough idea of what’s going on, but I think I should be more accurate when looking at the freezing point.

Do I need to calibrate them? How would I go about doing that? Ie, what can I trust as a proper baseline? I don’t have access to any really guaranteed kind of thermometer, I think. Thinking 

Thanks in advance for any wisdom you can send my way!

-Nico

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +5 verified
    If they are waterproof you can stick them in a slush of ice and water to get a zero degrees reference. If they aren't waterproof you can put them in a plastic bag in the ice/water mix. If they can take…
  • beacon_dave
    beacon_dave over 2 years ago +5 verified
    Comparing data sheets it looks like the accuracy of the DHT11 is ±2°C whereas the DS18B20 is ±0.5°C It will be interesting to see what your testing shows.
  • wolfgangfriedrich
    wolfgangfriedrich over 2 years ago in reply to dougw +4 verified
    During the ice-water test, you have to be careful not to touch the ice-cubes. They are still colder than zero degC. I learnt this during a thermocouple roadtest.
Parents
  • battlecoder
    0 battlecoder over 2 years ago

    I've also observed ~ 2° differences when comparing temperature sensors,  and in most cases that's their actual stated accuracy.

    As others have told you, you can measure known temperatures and see what the sensors read at those points, and you can do a simple fit regression over them.
    For two points is a lot simpler.
    Let's say, for example, that you measure the ice melting point (which should be 0°C) and the thermometer says it's 2°C. Then you measure the water boiling point (that should be 100°C) and the sensor reads 99°C That means that near 0 degrees the sensor is measuring 2 degrees higher, and near 100 is 1°C too low.


    You want to create a linear function that takes the sensor reading and converts it into a "closer to reality" reading, this is: F(what_the_sensor_says) = what_it_should_be
    So F(-2) = 0 and F(99)  = 100.

    Since we assume the relationship is linear, the function would have the form F(x) = m*x + b

    We can compute the slope (m) with our two points, as [F(x2) - F(x1)] / (x2 - x1), In my example that would be  (100 - 0) / (99 - [-2]) = 100 / 101 = 0.9901

    Our function is looking like this now:

    F(x) = 0.9901*x + b


    We only need to compute b. Replacing any of the two values we know, should allow us to get it. Let's use our reading at 100C:

    100 = 0.9901*(99) + b
    100 = 98.0199 + b
    b = 100 - 98.0199

    b = 1.9801


    So the final function would be F(x) = 0.9901*x + 1.9801 and you should be able to plug your sensor reading in place of x, and get an adjusted reading. This is of course, for my made-up example. You need to make your own measurements and follow this procedure. It doesn't need to be at 100 and 0, but those are good because you can compare against an actual physical phenomenon.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • battlecoder
    0 battlecoder over 2 years ago

    I've also observed ~ 2° differences when comparing temperature sensors,  and in most cases that's their actual stated accuracy.

    As others have told you, you can measure known temperatures and see what the sensors read at those points, and you can do a simple fit regression over them.
    For two points is a lot simpler.
    Let's say, for example, that you measure the ice melting point (which should be 0°C) and the thermometer says it's 2°C. Then you measure the water boiling point (that should be 100°C) and the sensor reads 99°C That means that near 0 degrees the sensor is measuring 2 degrees higher, and near 100 is 1°C too low.


    You want to create a linear function that takes the sensor reading and converts it into a "closer to reality" reading, this is: F(what_the_sensor_says) = what_it_should_be
    So F(-2) = 0 and F(99)  = 100.

    Since we assume the relationship is linear, the function would have the form F(x) = m*x + b

    We can compute the slope (m) with our two points, as [F(x2) - F(x1)] / (x2 - x1), In my example that would be  (100 - 0) / (99 - [-2]) = 100 / 101 = 0.9901

    Our function is looking like this now:

    F(x) = 0.9901*x + b


    We only need to compute b. Replacing any of the two values we know, should allow us to get it. Let's use our reading at 100C:

    100 = 0.9901*(99) + b
    100 = 98.0199 + b
    b = 100 - 98.0199

    b = 1.9801


    So the final function would be F(x) = 0.9901*x + 1.9801 and you should be able to plug your sensor reading in place of x, and get an adjusted reading. This is of course, for my made-up example. You need to make your own measurements and follow this procedure. It doesn't need to be at 100 and 0, but those are good because you can compare against an actual physical phenomenon.