Sensors
  • Technologies
  • More
Sensors
Sensor Forum Temperature sensor accuracy
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Subscribers 347 subscribers
  • Views 8621 views
  • Users 0 members are here
  • temperature
  • temperature sensor
Related

Temperature sensor accuracy

ntewinkel
ntewinkel over 2 years ago

Hi all,

I have two temperature sensors near each other, outside. In the winter I was using one to keep track of the nectar temperature in a hummingbird feeder, but I just left it hanging there for the summer.

Here is the typical result:

image

The top line is a dht11 or could be 12. It includes pressure and humidity. The bottom line is a ds18b20 in a metal tube.

Both are digital, but one is nearly always about 1 or 2 degrees higher than the other. Generally it’s fine to give me a close enough idea of what’s going on, but I think I should be more accurate when looking at the freezing point.

Do I need to calibrate them? How would I go about doing that? Ie, what can I trust as a proper baseline? I don’t have access to any really guaranteed kind of thermometer, I think. Thinking 

Thanks in advance for any wisdom you can send my way!

-Nico

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +5 verified
    If they are waterproof you can stick them in a slush of ice and water to get a zero degrees reference. If they aren't waterproof you can put them in a plastic bag in the ice/water mix. If they can take…
  • beacon_dave
    beacon_dave over 2 years ago +5 verified
    Comparing data sheets it looks like the accuracy of the DHT11 is ±2°C whereas the DS18B20 is ±0.5°C It will be interesting to see what your testing shows.
  • wolfgangfriedrich
    wolfgangfriedrich over 2 years ago in reply to dougw +4 verified
    During the ice-water test, you have to be careful not to touch the ice-cubes. They are still colder than zero degC. I learnt this during a thermocouple roadtest.
Parents
  • ntewinkel
    0 ntewinkel over 2 years ago

    I think shabaz  was onto something... it looks like the other sensor was maybe getting warmed up? Possibly because the Wemos D1 Mini is right next to it in the enclosure, even though it does have a separation.

    And I was wrong - the other sensor is a BME280, not the DHT I thought I was using in there. Funny, I guess it's been up there long enough for my short memory to keep up with it Laughing

    imageimage

    I tried an ice bath, but it didn't work well. It dipped down close to zero and then I think the bag started floating.

    imageimage

    BUT... once I removed it from the enclosure, the BME280 (light blue line, previously always on top) was recording predictably about a degree lower than the DS18b20 probe.

    I had it in the container of water overnight (with the bag clipped down better), and then removed it this morning with the two sensors being side by side in the air afterwards. This is the resulting graph:

    image

    So it looks like the BME280 is probably the accurate one (based on it hitting 0 in the ice bath), with the DS18b20 always recording a degree higher.

    I'll try the ice bath again, this time with more insulation all around, and I'm going to have to print a new enclosure that keeps the BME280 away from the Wemos D1 Mini. After that, if the ice bath result is stable, I'll update the code to just do a simple +/- adjustment.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 2 years ago

    I think shabaz  was onto something... it looks like the other sensor was maybe getting warmed up? Possibly because the Wemos D1 Mini is right next to it in the enclosure, even though it does have a separation.

    And I was wrong - the other sensor is a BME280, not the DHT I thought I was using in there. Funny, I guess it's been up there long enough for my short memory to keep up with it Laughing

    imageimage

    I tried an ice bath, but it didn't work well. It dipped down close to zero and then I think the bag started floating.

    imageimage

    BUT... once I removed it from the enclosure, the BME280 (light blue line, previously always on top) was recording predictably about a degree lower than the DS18b20 probe.

    I had it in the container of water overnight (with the bag clipped down better), and then removed it this morning with the two sensors being side by side in the air afterwards. This is the resulting graph:

    image

    So it looks like the BME280 is probably the accurate one (based on it hitting 0 in the ice bath), with the DS18b20 always recording a degree higher.

    I'll try the ice bath again, this time with more insulation all around, and I'm going to have to print a new enclosure that keeps the BME280 away from the Wemos D1 Mini. After that, if the ice bath result is stable, I'll update the code to just do a simple +/- adjustment.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • battlecoder
    0 battlecoder over 2 years ago in reply to ntewinkel

    It looks like the gap is a tad narrower at lower temperatures, but it still seem to remain around a degree almost consistently across the board, so it's probably enough to just subtract that 1 degree difference from the DS18B20, as you said. Fancier math is not going to give you a lot more accuracy considering what we are seeing in those graphs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 1 year ago in reply to battlecoder
    battlecoder said:
    Fancier math is not going to give you a lot more accuracy

    That’s what I’m thinking too. 80-20 rule.

    Looks like I have a good zero degree bath set up now. I used an insulated cooler with ice packs and a yogurt container with ice and water in the centre.

    image

    Now to add the fine tuning adjustments…

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • battlecoder
    0 battlecoder over 1 year ago in reply to ntewinkel

    There's definitely a difference at lower temps but that's still a lot better than the initial readings. Whether that's a good fit or not will depend on the accuracy you need, and in this case, how often it's going to be close to freezing in their actual real locations :D

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 1 year ago in reply to battlecoder
    battlecoder said:
    There's definitely a difference at lower temps

    Yes, it went from a one degree difference in the 10 to 20C range to nearly 2 degrees at freezing.

    It’s only for my specific use case for the hummingbird feeder, and freezing is the key thing I’m interested in. Our area might go down to -15C and up to maybe +35C, and those are interesting but not critical.

    I might get more fancy later, but this should do the trick for now.