Sensors
  • Technologies
  • More
Sensors
Sensor Forum Camera Playstation 5 Hack
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 346 subscribers
  • Views 2548 views
  • Users 0 members are here
  • PS5
  • camera
  • Playstation Camera
  • Playstation 5
Related

Camera Playstation 5 Hack

maxpowerr
maxpowerr over 1 year ago

I want to ask the Element14 community for help. I'm trying to study the PS5 camera device in order to use it as a cheap solution for computer vision. There is already a way to upload firmware to the camera via USB on the Internet, but this method is not very convenient, since it requires constantly uploading firmware when connecting the camera to USB and not all devices work with it. I would like to find a more universal solution.

What needs to be found out:
1. What controller is on the camera, and is it possible to flash it somehow? It seems to be OV580 with 32-bit RISC CPU. But I can't find a datasheet for this chip.

image

image

2. What elements are used on the board?

imageimageimage

If anyone is interested in this camera, join the discussion.

  • Sign in to reply
  • Cancel

Top Replies

  • maxpowerr
    maxpowerr over 1 year ago in reply to misaz +4
    Thank you for your advice I really appreciate it. I have a cheap logic analyzer SALEAE LOGIC 24 MHz and also have a T48 programmer I hope I can come up with something with it.
  • maxpowerr
    maxpowerr over 1 year ago in reply to anniel747 +2
    I can't answer what kind of solder is above the chip. I will definitely do some probing, but first I wanted to visually identify all the elements. I was hoping that maybe someone from the community had…
  • misaz
    misaz over 1 year ago in reply to maxpowerr +2
    You can try to read it. flashrom open source project likely know the protocol. Alternative approach is to observe what main chip reads from it. If you decide to probing, do not probe it at chip pins. Instead…
Parents
  • vmate
    vmate over 1 year ago

    Possibly you could add a USB mux and microcontroller between the camera and PC, where the microcontroller acts as a USB host and sends the firmware to the camera, before switching the mux over so the PC has USB access to the camera?

    Not a particularly elegant solution, but it's very easily reversible, and should let you use the camera from any device without having to worry about flashing the OV580.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • maxpowerr
    maxpowerr over 1 year ago in reply to vmate

    Interesting idea, but I still think if it doesn’t work out to flash the original controller, then try to replace it with some other one or FPGA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • maxpowerr
    maxpowerr over 1 year ago in reply to vmate

    Interesting idea, but I still think if it doesn’t work out to flash the original controller, then try to replace it with some other one or FPGA.