Sensors
  • Technologies
  • More
Sensors
Sensor Forum CO2 sensor recommendation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 354 subscribers
  • Views 8742 views
  • Users 0 members are here
  • gas sensor
  • co2 sensor
Related

CO2 sensor recommendation

koudelad
koudelad over 9 years ago

Hello,

 

I'd like to ask you for a CO2 sensor recommendation. My goal is to measure an air quality indoors (at home, office...) and take this as one of factors to control a ventilation. It is a hobby project to be installed at my home.

So far, I've found quite famous MQ-XX sensors, using various metal compounds. They are cheap (ca. €4), but need to be calibrated. Then I found quite a few Amphenol sensors, using IR light, priced ca. €150 - €350.

There are also volatile organic compounds (VOC) sensors, which provide output that correlates with CO2 level.

My requirements are: package solder-able at home (or a ready made module with a connector), some common interface (I2C for example), no need to calibrate the sensor.

 

Did you use any of the mentioned above in your projects?

 

Thank you, David

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +4
    Hi Shabaz, Your table is a bit old - the current atmospheric base level is 406ppm: https://www.co2.earth/daily-co2 The other numbers are broadly correct. I did find the video totally weird (doom background…
  • shabaz
    shabaz over 6 years ago in reply to mrlvy +3
    Hi Matthew, The example you give doesn't seem to be a reason to 'stay away' from senseair products. If anything, I appreciate that they made this information available to the layman. mrlvy wrote: WARNING…
  • kas.lewis
    kas.lewis over 9 years ago +2
    K30 CO2 Sensor is one I have running full time in my room (part of my LivPi ). It auto calibrates using an interesting method. Its also not to costly for a full module (depending on your idea of costly…
Parents
  • koudelad
    koudelad over 9 years ago

    Hello,
    I just wanted to let you know some information I found over the past few weeks. I asked a few sensors manufacturers about their sensors for indoor air monitoring. I don't have any of the sensors at home yet.

     

    The most reliable sensors of CO2 concentration seem to be the nondispersive infrared sensors (NDIR). An IR light is absorbed by the double bond in CO2 molecules. In a common house environment is practically no cross sensitivity, as other gases like H2O, SO2, NO2 have much lower concentrations. These sensors start at ca. € 100. I only found sensors interfaced via UART, some of them use MODBUS over UART. Powered by 3.3 Volts and have tens of mA consumption during measurement.
    The interesting process is a calibration. All sensors have customer calibration possibility, but require proper equipment image Since most of the customers don't have sealed chambers with known concentration of some gasses and another measurement device to perform the calibration, the devices are calibrated in factory. However the sensors have some significant drift that requires periodical calibration. That's why the manufacturers came with autocalibration feature. Basically, if the sensor measures CO2 concentration over some period (a week for example), the lowest CO2 concentration measured is considered as a fresh air and all higher values are relative to that.
    (I am quite interested to have one in hands to try leave it in a house in the countryside and then place it in a larger city.)

    Example: https://www.gassensing.co.uk/products/ambient-air-sensors/cozir-lp-ambient-air-co2-sensor/

     

    There are also some total volatile organic compounds (TVOC) sensors, that are claimed to have the ability to measure CO2 concentration, as well as other pollutants in the air. I googled for trustworthy information and asked one manufacturer of these sensors about the functionality and got quite a surprising answer.

    They are suitable for:
    1) Environment occupied (and air polluted) only by breathing, nothing else (see below).
    2) Detect anything unusual in environment (start of some chemical process, cooking, ...) - either human occupied, or not.

    In fact, the sensors have no CO2 sensitivity at all. The correlation between TVOC level and CO2 levels comes from experiments and do not work if the air is polluted by anything not produced by a human (like cleaning agents, cooking, ...) or generally humidity not caused by breathing (ironing clothes, having a shower...). The most import fact is, they produce output that has no unit and meaning - it is just a value and it is up to you to interpret it. You can't determine whether the air is breathable or not.
    That could explain the weird measurements that kas.lewis mentioned.

    Example: CCS811 / Gas Sensors / Environmental Sensors / Products / Home - ams AG , this is the one features on Thunderboard.

    http://uk.farnell.com/silicon-labs/sltb001a/thunderboard-sense/dp/2581458

     

    A useful sensor for home / industrial environment (especially with any combustion device) is a CO sensor. The air can be poisoned by CO and CO2/TVOC sensor won't detect it at all. I guess the sensors can be helpful, however, I would be careful about threshold limit to warn the occupants of the measured environment. For example I found a sensor that outputs a current of 50 ± 20 nA / ppm , which makes it 40 % inaccurate and that could be the difference between a headache and poisoning concentration.

    Example: http://www.ddscientific.com/co-sensors.html

     

    Another approach might be measuring the O2 levels. Obviously, O2 is needed by humans to stay alive. The more CO and/or CO2 is in the air, the less oxygen is measured. I found an optical oxygen sensor that outputs partial pressure of O2. If you also measure a barometric air pressure, you can calculate the percentage of O2 in the air.

    Example: LuminOx Optical Oxygen SensorsSST Sensing

     

    I will probably order all of the sensors mentioned above and try to make an air quality measurement device.

     

    Note: About two years ago, I bought an SHT21 sensor and use it as thermometer and humidity meter at home. I started watching the humidity carefully and ventilating the apartment at least twice a day. Since that time, I have a much better sleep. According to all the information I've read, it is very probable that humidity, TVOC and CO2 concentration correlate with the human breathing process.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to koudelad

    I will definitely be interested in reading about your results.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 9 years ago in reply to koudelad

    I will definitely be interested in reading about your results.