Sensors
  • Technologies
  • More
Sensors
Sensor Forum Choosing a sensor for detecting swimming pool entry
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 354 subscribers
  • Views 6770 views
  • Users 0 members are here
Related

Choosing a sensor for detecting swimming pool entry

pettitda
pettitda over 9 years ago

I'm looking for ideas on how to sense when a person or animal has entered a swimming pool.  There are several devices on the market that claim to do this, but the reviews are all pretty horrible.  False positives seem to be a big problem with existing products.  I'm thinking that something like an infrared camera would work but it would take considerable effort to set up the detection area (i.e. where the pool is) in the camera's view.  Does anyone have an idea that's not prone to false positives (i.e. leaves falling in the pool, wind blown water, etc)? 

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 9 years ago in reply to pettitda +3
    I have an interesting thought. Why not go with a capacitive sensor, I am thinking about the new TI sense board I have been testing. You could run a conductive strip around the pool and then connect it…
  • jw0752
    jw0752 over 9 years ago +2
    Hi David; How about a water level sensor that looks at the change with respect to time of the level sensed. In other words a wave detector. Anything of any size that enters the pool is going to splash…
  • jw0752
    jw0752 over 9 years ago +2
    Hi David; Another idea might be to deploy a beam along each pool edge such as those used to detect something passing under a closing garage door. These light and sensor pairs seem to work quite well at…
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi David;

    How about a water level sensor that looks at the change with respect to time of the level sensed. In other words a wave detector. Anything of any size that enters the pool is going to splash and move creating waves. If your wave sensor had a resolution that could sense one or two cm deviations you could program a microprocessor to apply a formula to differentiate between environmental waves such as those produced by the wind and more random waves such as those created by a dog or person.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to jw0752

    Ho John,

    IMHO it is not so efficient in a swimming pool where more than one can enter in the water. And there are mani other possibilities that other waves are generated unexpectedly. Then also add the option of different beaviour of the waves deoending in the entry point. This implies I suppose, using this method ti generate a lot of filters to detect the right event to sense, and only it.

    As far as I know this kind of detection is not new and I see teo possible teliable ways depending on the needs. In the case you should only detect the presence in water an rfid sensor is sufficient and the tag can be extermely small and easy to wear also for a swimmer (tipically wearing very few dresses   )

    In the case where the detection of the exact instant is a key factor instead a laser or IR sensor is better.

    In both cases therr is the advantage that very few electronic parts should be waterproof.

     

    Enrici

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to jw0752

    Ho John,

    IMHO it is not so efficient in a swimming pool where more than one can enter in the water. And there are mani other possibilities that other waves are generated unexpectedly. Then also add the option of different beaviour of the waves deoending in the entry point. This implies I suppose, using this method ti generate a lot of filters to detect the right event to sense, and only it.

    As far as I know this kind of detection is not new and I see teo possible teliable ways depending on the needs. In the case you should only detect the presence in water an rfid sensor is sufficient and the tag can be extermely small and easy to wear also for a swimmer (tipically wearing very few dresses   )

    In the case where the detection of the exact instant is a key factor instead a laser or IR sensor is better.

    In both cases therr is the advantage that very few electronic parts should be waterproof.

     

    Enrici