Sensors
  • Technologies
  • More
Sensors
Sensor Forum Choosing a sensor for detecting swimming pool entry
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 354 subscribers
  • Views 6745 views
  • Users 0 members are here
Related

Choosing a sensor for detecting swimming pool entry

pettitda
pettitda over 9 years ago

I'm looking for ideas on how to sense when a person or animal has entered a swimming pool.  There are several devices on the market that claim to do this, but the reviews are all pretty horrible.  False positives seem to be a big problem with existing products.  I'm thinking that something like an infrared camera would work but it would take considerable effort to set up the detection area (i.e. where the pool is) in the camera's view.  Does anyone have an idea that's not prone to false positives (i.e. leaves falling in the pool, wind blown water, etc)? 

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 9 years ago in reply to pettitda +3
    I have an interesting thought. Why not go with a capacitive sensor, I am thinking about the new TI sense board I have been testing. You could run a conductive strip around the pool and then connect it…
  • jw0752
    jw0752 over 9 years ago +2
    Hi David; How about a water level sensor that looks at the change with respect to time of the level sensed. In other words a wave detector. Anything of any size that enters the pool is going to splash…
  • jw0752
    jw0752 over 9 years ago +2
    Hi David; Another idea might be to deploy a beam along each pool edge such as those used to detect something passing under a closing garage door. These light and sensor pairs seem to work quite well at…
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi David;

    Another idea might be to deploy a beam along each pool edge such as those used to detect something passing under a closing garage door. These light and sensor pairs seem to work quite well at 4 meters and probably can be extended. to greater distances. This would not detect the entry to the pool only a potential entry by an animal or person as they break the beam on their way to the edge.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • pettitda
    pettitda over 9 years ago in reply to jw0752

    I guess I didn't make it clear that the pool is round.  So, there are no straight edges.  However, I might be able to use multiple pairs of sensors arranged in a pattern (see below).  Of course, it wouldn't detect something entering the center of the pool, but that is an unlikely occurrence.  I will calculate how many sensors it would require to cover a 27 foot diameter pool out to say 2 foot with gaps no bigger than 6 inches, but I think it must be large. 

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to pettitda

    How about piezo vibration sensors on the rim - they would detect activity on the rim. Or do you only want to know when something goes into the water?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 9 years ago in reply to pettitda

    How about piezo vibration sensors on the rim - they would detect activity on the rim. Or do you only want to know when something goes into the water?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • pettitda
    pettitda over 9 years ago in reply to dougw

    I'm primarily concerned with them going into the water.  If they enter the pool via the ladder, it is quite possible to enter without even touching the rim.