Sensors
  • Technologies
  • More
Sensors
Polls Poll -- How Much Do You Know about Time of Flight Sensors?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 27 Jun 2020 6:54 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 3129 views
  • Likes 1 like
  • Comments 19 comments
Related
Recommended

Poll -- How Much Do You Know about Time of Flight Sensors?

Hi all!

I'm preparing to propose an activity on element14 for a program I manage regarding Time of Flight sensors. It would be helpful for me to know everyone's knowledge level. I'd appreciate your input in this poll. Thanks.

 

Poll: How Much Do You Know about Time of Flight Sensors?

  • how much do you know about time of flight sensors?
  • community survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to neuromodulator +5
    neuromodulator wrote: I couldn't find it... Was it a roadtest blog or a common blog? Both. Here's a link: TI Ultrasonic Sensing RoadTest - Review
  • neuromodulator
    neuromodulator over 6 years ago +4
    I hope this is a hint of an upcoming roadtest
  • Jan Cumps
    Jan Cumps over 6 years ago +4
    I roatested one here on element14, end 2015.
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to phoenixcomm

    ops! Yes, and just a little trivia, mostly older movies. Past life non-degreed engineer doing mostly hardware-software integration. typical Thursday or Friday. Boss would walk into my office and drop a piece of equipment that I have never seen before with a book hopefully and tell me to interface it to some computer, which I may have had never seen after I muttered under my breath he would say I need to have this done before (some unreasonable time) next Friday. LOL. I was a systems test engineer at Interdata in NJ which we got the system before QC got to it. I learned electronics basically in grade school. my Dad worked for RCA Hightstown and always bringing stuff home. I was building stuff for the local hams, and in the 7th grade, I built a transistor 1-octave organ, using 2N404s which Dad picked up.   My first computer of adding machine was built-in HS over a two year period. It was built from RTL and some rotary stepping relays. memory was built out of surplus form H relays. So for an 8-bit word you read, write, latch relays

    It could add and subtract, It was two full relay racks.

    Later got into the M6800 eval board witch I wired into an S1000 chassis for more memory. Later it was replaced by a TDL Z80 CPU card which would not work with my IMSAI 8080 front panel. A week later it worked as well. My gig at Interdata got me a Teletype    ASR35 which was scrapped after one of the QC morons swang out the 4 or 5 power supplies without the pull-out support legs. My S100 Box was powered by the beast on the left! image

    I went to Trenton State for Industrial Engineering with Computer Science and Electronics as minors I never finished my major by my minors were almost done.

    Now I mess with flight simulators.

     

    hmm about triva? here my get out of grade school test. NO CHEATING

    Who was Galileo Galilei? what did he do, what did he invent, how and what lead up to his death.

     

    Now just for fun.  NO CHEATING  all very hard.

     

    In the movie  "It's a Wonderful Life" 1. where was the dance shot, 2. towards the end of the film he runs down the street saying "hello this or that", what was the movie playing in the Biju Theater? and for extra points name the characters in both films! LOL (No Cheating)

     

    In the movie "The Flight of the Phoenix" (19655) where any of the aircraft flying real, If so what happened?

    one more

    In the "Strategic Command" was Jimmy Stewart really flying, the B-36? Yes/No Reson   LOL

     

    Oh BTW what was the first microprocessor???

    ~~Cris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to colporteur

    yes, andimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to phoenixcomm

    The breath of your knowledge blows me away! The eyelets are your points of knowledge. You sure you're not a Borg?

    image

    Do you play much trivia?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 6 years ago

    ToF sensors appear quite interesting. Never tried any but probably will in the future.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 6 years ago in reply to navadeepganeshu

    Theoretically yes.

    Theoretically you probably are at most in 2 RoadTests at the same time.

    Quite a shame, since I'm in a roadtest and I have 2 I want to be in(probably not going to be selected but still)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • navadeepganeshu
    navadeepganeshu over 6 years ago

    Is it possible to get into a RoadTest while same person is in another Roadtest which is being done? Or what if already done but 60 days are'nt over.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 6 years ago in reply to robogary

    I guess it depends on what you mean by "Time of Flight" sensor.  If you are referring to devices that are labeled this, then most seem to be i2c based where others are not.  Something like the Parallax Laser Ping just has a SIG line to control and read from the sensor. 

     

    The VL53L0X is a ST device and there is an App note AN4846 "Using multiple VL53L0X in a single design" for changing the address on the sensors:

    https://www.st.com/en/imaging-and-photonics-solutions/vl53l0x.html#resource

     

    There is an API where you can change the device address of the VL53L0X.  This may be temporary and reset back to default after power reset as in the Adafruit example. I have not tried this.

    VL53L0X_SetDeviceAddress()

     

    The other option, if you have enough available GPIO pins, then you could use that to select individual devices or use an expander.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to robogary

    "...Using multiple time of flight sensors would also require an "address expander" to multiplex them..."

     

    The Adafruit VL53L0X may be of interest as it appears to have a software programmable I2C address which can be set to any address below 0x7F (0x29 power on default)

     

    You would need an initialisation routine to set a unique address to them on power up but would allow you to have multiple sensors on the one bus without the expander.

    See 'Connecting Multiple Sensors' at:

    https://learn.adafruit.com/adafruit-vl53l0x-micro-lidar-distance-sensor-breakout/arduino-code 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 6 years ago

    Ive seen them used in projects, but havent done a project with them, but would be willing to try.

    Maybe due to my ignorance, I understand the time of flight sensors are I2C based, all having the same I2C address.

    Using multiple time of flight sensors would also require an "address expander" to multiplex them.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 6 years ago

    When you say Time of Flight Sensor (ToF), are you referring to devices such as Ultrasonic, IR, LiDAR and generic distance sensors or are you referring to devices that are labeled Time of Flight Sensors such as the ST VL6180?

     

    I'll be using both the ST VL53L0X and VL53L1X ToF sensors in my RoadTest of the ST32H7B3i-DK.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>