Test & Tools
  • Technologies
  • More
Test & Tools
Blog Benchwave, a free Mac app that will help oragnise your workshop
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sebnast
  • Date Created: 2 Jul 2026 2:17 PM Date Created
  • Views 443 views
  • Likes 6 likes
  • Comments 5 comments
  • Benchwave
  • test equipment
  • open tools
  • 2D15P
  • macos
  • LCR-P1
  • oscilloscope
  • lcr meter
  • FNIRSI
Related
Recommended

Benchwave, a free Mac app that will help oragnise your workshop

sebnast
sebnast
2 Jul 2026

A while back I picked up a couple of FNIRSI instruments, a 2D15P scope and an LCR-P1 component tester. Good kit for the money, but the software is a letdown: mostly Windows-only, so on a Mac you're stuck dragging screenshot files off a USB drive by hand, or booting a VM just to flash firmware.

I wanted two things fixed: get the scope's captures onto my Mac properly, and update the LCR-P1's firmware without touching Windows. So I built Benchwave to do exactly that. It kept growing from there, and it's now a full bench companion, free, and public: https://benchwave.co.uk

What it does today

Captures land in a proper library instead of a USB folder. Add a drive or folder as a Sync Location, the scope's USB share, an SD card, a camera, whatever holds your captures, and Benchwave imports new screenshots automatically. Nothing hardcoded to one instrument; it just watches wherever you point it.

You can pick two or more captures and compare them side by side, with readings plotted on a graph across the sequence, handy for before/after checks like a voltage drop under load.

On a supported Mac, Benchwave reads the numbers off a capture itself using Apple's on-device models, no cloud round-trip, and gives you a plain-English summary of what it's looking at.

Firmware updating for the LCR-P1, natively on macOS. FNIRSI only ship a Windows updater, so I reverse engineered the IAP serial protocol and reimplemented it myself. I've flashed a real LCR-P1 from a Mac with it, which as far as I can tell makes it the first non-Windows updater for the device.

There's a proper component inventory too: quantities, locations, datasheets, low-stock alerts, with categories and manufacturers that suggest themselves as you type.

Projects tie it together. Each one holds its own captures, a parts list you build straight from inventory or import as a BOM CSV, and a running set of notes. Add a part and it deducts stock automatically, and flags anything you're short on.

From a project you can export a branded Project Sheet or a customer Quote as a PDF, resell prices only, your cost and margin stay private, itemised or combined, however you bill.

Any datasheet or image you attach can be marked up, arrows, text notes, freehand, without touching the original file. If the same document is shared across several projects, each one keeps its own markup on top of it, nothing gets duplicated or overwritten.

Everything backs itself up automatically on launch, plus a one-click full export if you want a copy off the machine.

What's next

Benchwave on iPhone and iPad, so your library, inventory and notes travel with you, synced through your own iCloud (firmware flashing stays on the Mac). A cross-platform version for Windows and Linux, already in progress, so this doesn't stay Mac-only. Deeper on-device AI for reading and summarising captures. And support for more instruments beyond FNIRSI's two, depending on what people ask for.

Give it a try

Grab it here: https://benchwave.co.uk

If you've got a 2D15P, an LCR-P1, or any bench gear that dumps screenshots to a USB drive, I'd like to hear how it goes: what works, what's missing, what you'd want next. There's also a community translation kit if you want to get it into your language (Polish is already done).

Thanks for reading, and happy building.
Seb




image
image
image
image

  • Sign in to reply
Parents
  • shabaz
    shabaz 4 months ago

    Hi,

    It might be good to split up the project, because the chances of someone owning those same precise two instruments, _and_ requiring a component inventory system might be low. It likely needs configurability (or is it planned to be open source), so that users can configure different instruments.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sebnast
    sebnast 4 months ago in reply to shabaz

    Hey, you’re right and i think it’s due to my not very clear message, I’ll explain :) All the functionality can be used without those specific bits of kit, i have made it possible to turn them off.

    It was supposed to go open source from the start but i made bunch of direction changes and moved away from it for now.

    I am still working out a good way to go about it, one of the ideas was a plugin system that would allow creation of add-ons for different equipment types, I’m now trying to collect information on protocols and the way equipment is interacting with computers.

    I think the comms should be leaning more towards the inventory and project management then the hardware to start with because i put a lot of effort in making this useful, I just thought the Mac support for fnirsi gear would be appreciated as they don’t have the updater for mac as far as i know for the lcr-p1.

    The 2d15p is just a storage but how they did it is you start the usb share and you have to go in copy what you need then when you stop the share mode the storage is “yanked” out and you get angry popup, i made it sync automatically and eject the volume gracefully by unmounting it. And since it is just storage it would be very easy to adapt it for other devices working in the same way.

    Thank you for the comments! 
    Seb

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sebnast
    sebnast 4 months ago in reply to shabaz

    Hey, you’re right and i think it’s due to my not very clear message, I’ll explain :) All the functionality can be used without those specific bits of kit, i have made it possible to turn them off.

    It was supposed to go open source from the start but i made bunch of direction changes and moved away from it for now.

    I am still working out a good way to go about it, one of the ideas was a plugin system that would allow creation of add-ons for different equipment types, I’m now trying to collect information on protocols and the way equipment is interacting with computers.

    I think the comms should be leaning more towards the inventory and project management then the hardware to start with because i put a lot of effort in making this useful, I just thought the Mac support for fnirsi gear would be appreciated as they don’t have the updater for mac as far as i know for the lcr-p1.

    The 2d15p is just a storage but how they did it is you start the usb share and you have to go in copy what you need then when you stop the share mode the storage is “yanked” out and you get angry popup, i made it sync automatically and eject the volume gracefully by unmounting it. And since it is just storage it would be very easy to adapt it for other devices working in the same way.

    Thank you for the comments! 
    Seb