Test & Tools
  • Technologies
  • More
Test & Tools
Blog Build your own MP3 Deck Player with a Cassette Tape
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 4 Jun 2018 7:01 PM Date Created
  • Views 6234 views
  • Likes 4 likes
  • Comments 6 comments
  • audiophile
  • tape
  • audio
  • project
  • 1980s
  • diy
  • cabeatwell
  • 80s
Related
Recommended

Build your own MP3 Deck Player with a Cassette Tape

Catwell
Catwell
4 Jun 2018

Have you ever wondered if it's possible to convert your cassette tape players into an mp3 music player? Thanks to TapelessDeckPlayer, the idea is now possible and seems both inviting and enticing for music enthusiasts who are still in possession of their cassettes. After all, who'd be crazy enough to throw them out - especially in this modern and music digital age?

The TapLess Deck Player features some pretty nifty add-ons that you would be surprised to know exists on this deck player. It has wireless capabilities - so that you can upload songs/albums and manage your music library from your PC or Mac system. It just requires a standard web browser. Nothing too fancy.

 

It features the perfect size and has animated functions for cassette reels and tape playability. It also enables you to use the player with the touch of a finger - you can play, rewind and even skip tracks and manage your library with the on-screen functionality. The ability to play MP3 and lossless FLAC files is a major possibility - giving the opportunity to play the sound perfectly and at higher sound quality.

 

All your favorite songs and albums will be stored into one device on the tape player - allowing access to a large storage on this device. You can also have the ability to use the internet radio on the MP3 Deck using built-in software or additional applications. You also have the option to use it as a Spotify player, as well.

 

The MP3 Player also has an FM Radio attached to it. All you'll need to do is switch the player on and toggle through your favorite stations to use this feature. There are also more ideas and applications that can be installed to this player to enhance functionality and playability of this device - the options are there and should be provided on the player.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

MP3 Deck Player. (Video Credit: TapeLess Deck Project)

 

To build the player, first, it is essential that the one interested in listening to their cassettes chooses a tape recorder that is suitable for the type of music they'll listen to. This is to enhance the modification of the tape itself and apply the final effect to the modifications.

 

In the center of the system, there is a smartphone touchscreen that uses special software to allow ease of playability. However, the phone must have some sufficient space for memory or an added memory card for the music storage. Chargers, connectors, audio cables, and jacks are also required to run and play the music. Inserting the smartphone into the cassette compartment might be a bit tricky, however. Connecting electronic sources to the circuits with no distortions may be quite a challenge, as well. The end result is the device acts as a real tape deck - which includes animations, level meters, adjustable output signal and much more. The unique system is the only handcrafted device in the world.

 

Remember those tape to CD adapters? How would those compare, I wonder...

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago in reply to genebren +3
    I quite liked the system in Minority Report : ) Recordings on acrylic or glass squares.. waiting for Sony to produce that : )
  • balearicdynamics
    balearicdynamics over 8 years ago in reply to shabaz +3
    Hi Shabaz, I have patented this method some years ago (before the film ) and I am seriously thinking to release the technology as open (together with another AI learning system) Enrico
  • shabaz
    shabaz over 8 years ago +2
    Interesting hack : ) I feel something significant is lost though : ( shame to destroy the mechanism to stick the mobile phone inside!
Parents
  • phoenixcomm
    phoenixcomm over 8 years ago

    At first, I thought what a way to trash a nice deck. But after thinking about it I kind of like it. But the dam touchscreen is well to easy. The Display is a good idea but not touch. You have the nice switches you could have used them (left to right). 

    Eject ( Menu)

    Record

    Rewind (Go Back one Song)

    Play

    Fast Forward (Skip to the next Song)E

    Pause

    ----

    Menu    

         FF Next Album

         RW Album before current Album.

         PLAY puts you in play mode on track #1

         Record (next playlist)

     

    So you leave the amp alone. 600 ohms for the stereo image

    Add a network connection RJ45 for my network image

    Make sure that this box can mount a standard NFS mount for my music. image

     

    NOW this is all well an good but remember, we are supposed to be engineers. AND that means you should not have re-invent the wheel. LOL

    Duh, that's what I use Kodi.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 8 years ago

    At first, I thought what a way to trash a nice deck. But after thinking about it I kind of like it. But the dam touchscreen is well to easy. The Display is a good idea but not touch. You have the nice switches you could have used them (left to right). 

    Eject ( Menu)

    Record

    Rewind (Go Back one Song)

    Play

    Fast Forward (Skip to the next Song)E

    Pause

    ----

    Menu    

         FF Next Album

         RW Album before current Album.

         PLAY puts you in play mode on track #1

         Record (next playlist)

     

    So you leave the amp alone. 600 ohms for the stereo image

    Add a network connection RJ45 for my network image

    Make sure that this box can mount a standard NFS mount for my music. image

     

    NOW this is all well an good but remember, we are supposed to be engineers. AND that means you should not have re-invent the wheel. LOL

    Duh, that's what I use Kodi.