Test & Tools
  • Technologies
  • More
Test & Tools
Blog Building Kelvin (4-Wire) Test Leads
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 12 Sep 2018 6:00 PM Date Created
  • Views 22174 views
  • Likes 17 likes
  • Comments 27 comments
  • kelvin measurement
  • 2-wire measurement
  • passive_featured
  • 4 wire measurement
  • kelvin
Related
Recommended

Building Kelvin (4-Wire) Test Leads

shabaz
shabaz
12 Sep 2018

Introduction

This short blog post discusses an attempt to make test leads for hopefully better measurements!

image

 

Measuring small resistances is really difficult with the usual 2-wire measurement with multimeters. The multimeter will measure the resistance of the leads as well as the resistance-under-test. Although this could in theory be nulled out, the result can still be poor because the connection still depends on the variable resistance between the probes and the device, i.e. contact resistance. This can vary by tens of milliohms, or a lot worse (hundreds of milliohms). It’s not possible to easily apply a precise, unchanging amount of force using the test probes.

image

 

How can it be solved? The multimeter passes some current through the device, and measures the voltage to derive the resistance using R=V/I. But, that voltage happens to be the sum of the voltage across the device under test, but also the voltage across the red and black test leads (because the current is passing through them too and developing a potential across them), as well as the connectors or contacts. It follows that if a separate voltmeter was used to measure the voltage using two separate probes, the measured voltage would not include the voltage across the test leads and contact resistance. That’s the solution – find a bench meter with 4 connections on it. This solution is a 4-wire measurement (also known as a Kelvin measurement). The diagram below shows how it works. The thickened wires carry the driving current to make the measurement. The voltmeter is of a very high impedance and no significant current passes through the wires directly attached to it. With this method however, it is awkward to have 4 test leads or test clips. It’s a messy amount of clips and wires.

image

 

But, there are some nice reasonable cost test clipstest clips with dual isolated metal contacts that can be used instead - they will grip the wire of the device under test on both sides, with a separate connection. They are very fancy gold-plated parts, for about £8.50 / $11 USD each. I also picked up some nice gold-plated banana plugs in redbanana plugs in red and blackblack, and set about assembling it all together.

 

Note that for cheaper clips, there is ebay, but word on the street is that some may be constructed of aluminium with some gold coating. It shouldn't be an issue, but it is a judgement call if that is ok. I've been bitten in the past by strange gold plating on connectors that darken or discolour over time, so I avoid any gold-plated connectors from ebay. I am only going to be making one or two sets of these for my personal use, so I want them to last, so I went with the known material clips.

 

There are also ready-made test leads from ebay, that cost under $10, so that’s another option. However they may require some modifications (see the strange photos below). In any case, sometimes it’s nice hand-assembling stuff to your precise requirements.

image

 

 

Building the Leads

The red red and black wiresblack wires had silicone insulation for flexibility. The wire is 5 metres long; I only used one metre, so there is plenty left over to make various other test leads too.

image

 

Since 4 wires will tangle on the desk, plastic braidplastic braid could be an option. It does reduce the flexibility a bit, but not much. I decided to run with it. Adhesive lined heat shrink tubingAdhesive lined heat shrink tubing was applied to stop it fraying. To get the braid over the wires easily, I taped the wires at 15-cm spacing, and removed the tape when the braid was pushed close to it.

image

 

The braid could melt while using the heat-shrink tubing, so I protected it with some paper tape (or use Kapton tape) while applying the heat gun, and it worked fine.

image

 

The clips come with screw terminals, but it felt awkward putting the stranded wire inside there. I did consider using a ring terminal, but in the end it seemed it could be easier to just solder the wires. The plastic clips didn’t feel too soft, so I felt they could take the temporary heat from a soldering iron.

image

 

The screws play a structural role with these clips though. Without them, the metal portion of the clips slide around. With hindsight, I would have replaced them with 3mm grub screws, but in my case, I just left the supplied screws in there, and it means the wire insulation has to pass over the screw head. It is not a big deal, and provides some grippy area to hold the clips actually!

image

 

Since the clips are gold-plated, they are very easy to solder onto. I used a 3mm soldering iron bit and turned up the heat to 350 degrees C, since the aim was to get the heat quickly onto the clip, and finish the soldering task in 5-10 seconds if possible, to reduce the risk of damaging the plastic. It worked fine. Three hands are needed though. I used a flat blade screwdriver to gently press the wire strands against the clip while I soldered it.

 

Summary

I was happy that with little effort, I've got reasonable 4-wire measurement capability. I have not used them much yet, but as a quick test, I took a length (about 60cm, I didn’t measure it) of 0.15mm diameter enamelled copper wire and stripped the ends, and measured it with the clips. It was 798 milliohms. In contrast the handheld multimeter was measuring 2 or 3 ohms, fluctuating all over the place.

 

Next I folded it in half and cut it and re-measured one length using the clips, and it was 398 milliohms, so it’s clearly functioning, allowing resistance measurements without the inaccuracies of the 2-wire method.

 

Overall, these test leads cost under £40 for all parts, which is not bad – and costs can be further reduced by using old test lead wire : )

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 8 years ago +8
    That's quite a good project - in fact, I should probably build some myself. My excuse for not bothering with 4W mode on most of the instruments boils down to either the sense terminals being at the back…
  • fmilburn
    fmilburn over 8 years ago in reply to three-phase +7
    This might be a fun project to try and make your own meter. I am assuming you could set up a constant current source and then use a microcontroller with a good ADC to measure and display resistance. Not…
  • fmilburn
    fmilburn over 8 years ago +6
    Very nice. Another project added to my list :-)
Parents
  • Andrew J
    Andrew J over 6 years ago

    These looked so good, I made some:

     

    image

    Readings with these,

    25cm, 16 AWG stranded copper:

    2-wire: 0.063Ohms

    4-wire: 0.009Ohms

     

    50cm, 28 AWG (0.32mm) single strand copper:

    2-wire: 164 mOhm

    4-wire: 106.7 mOhm

     

    25cm, 28 AWG (0.32mm) single strand copper:

    2-wire: 108 mOhm

    4-wire: 052.3 mOhm

     

    I also made some Micrograbbers, redred and blackblack:

     

    image

    These were a little awkward - the Grabber cap had only a small outlet for the wire, approximately 1mm, maybe 1.5mm:

    image

    Farnell did have some that used a 4mm banana plug connection but the red ones were out of stock; the datasheet for these made no mention of the wire size to use so I got these rather than wait.  I used a 3mm bit in a pin drill and a chisel tip craft knife to enlarge the hole and wire slit to around 2.5mm which is the size of wire I have:

    image

    Bit blurry, but it did the job reasonably neatly.  For connecting to Banana Plugs I used some bootlace ferrules and a crimpercrimper:

    image

    This one is a bit different to the tool you used here and there seem to be 3 types - the one above that creates a flat, 'serrated' pentagon crimp; a hexagon crimp and a square crimp.  This one is a heck of a lot cheaper than the one you used though and it makes a good crimp:

    imageimage

     

    The Deltron banana plugs I had are not very good so I need to change them - the pin pushes out of the housing if not careful, rather than into the meter.

     

    Now all I need to do is make some SMT tweezers!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    Nice test leads! Perfect for your new DMM.

    Incidentally, CPC has some low-cost test-lead wire (search term was 'test lead wire' on the site) that seems quite reasonable. Not as good nor as flexible as the one mentioned in the blog post, but cheap enough to keep 5-10 metres of it handy for constructing up the occasional test leads.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    Nice test leads! Perfect for your new DMM.

    Incidentally, CPC has some low-cost test-lead wire (search term was 'test lead wire' on the site) that seems quite reasonable. Not as good nor as flexible as the one mentioned in the blog post, but cheap enough to keep 5-10 metres of it handy for constructing up the occasional test leads.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Andrew J
    Andrew J over 6 years ago in reply to shabaz

    I had some silicon cable left over from when I made some leads for my power supply which I got on special offer from CPC's bargain corner - Staubili Silivolt IIRC.  I've got about a meter of black and red left now!  I got those lousy Deltron banana plugs at the same time image 

    • Cancel
    • Vote Up +3 Vote Down