Test & Tools
  • Technologies
  • More
Test & Tools
Blog DC Voltage Measurement Accuracy: fact check Shabaz' graph
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 10 Jun 2023 4:50 PM Date Created
  • Views 1838 views
  • Likes 11 likes
  • Comments 2 comments
Related
Recommended

DC Voltage Measurement Accuracy: fact check Shabaz' graph

Jan Cumps
Jan Cumps
10 Jun 2023

 shabaz created a DMM measurement accuracy graph for his  MP730624 Multimeter Quick Review: Surprisingly Accurate! blog. The graph shows the spec-ed accuracy of a MP730624 . He also shows graphs for other meters, like the 121GW. And I have one of those.

image

image source: shabaz' blog

I ordered a reasonable accurate (0.01%), calibrated voltage reference to put that meter to the test. And compare theory to reality. While I'm waiting for that reference to arrive, I'm playing around a little. I'm testing it with two voltage references on the Digilent/TI Analog Shield. A LM4128-2.5 and a REF5020.

I don't want to achieve or prove anything in this post. Just measure. I added a DMM6500 for comparison.
Circumstances:

  • It's a hot but dry +30°C day. The references and meters have been on for more than half an hour.
  • 5 V input is the 5 V from an Arduino  UNO R3 powered by a laptop's USB.

LM4128-2.5

This is a 2.5 V reference.

image

Results:

image

REF5020 Low-Noise, Very Low Drift, Precision Voltage Reference

This is a 2.048 V reference.

image

Results:

image

That's it. I did not analyse, just power on, let it stabilise, and measure. Thoughts and comments below Slight smile

  • Sign in to reply
  • shabaz
    shabaz over 3 years ago

    Hi Jan,

    This is awesome, it allowed me to add your 121GW data points to the chart, since the DMM6500 is super-accurate! I've updated the multimeter blog post with this chart too. The results are comfortably within spec.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Also it has to be said, it's amazing how much granularity and accuracy there is on the DMM6500 and these handhelds. Brilliant for modern work. I can still remember my first analog MM, think it was Altai, with maybe 5.0% accuracy at best, and the cramped resistance readings that would be even worse accuracy : )