Test & Tools
  • Technologies
  • More
Test & Tools
Blog DC Voltage Measurement Accuracy: Measuring DC voltage with high accuracy on a DMM6500
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 11 Jun 2023 2:35 PM Date Created
  • Views 3930 views
  • Likes 13 likes
  • Comments 16 comments
  • dmm6500
  • keithley
Related
Recommended

DC Voltage Measurement Accuracy: Measuring DC voltage with high accuracy on a DMM6500

Jan Cumps
Jan Cumps
11 Jun 2023

A little follow-up on  DC Voltage Measurement Accuracy: fact check Shabaz' graph . The DMM6500 has functions to improve  DC Volt measurements. 

  • nplc or number of power line cycles: you can set the sample time in function of the main utility line frequency. This is one of the big causes of noise. By measuring over a high number of cycles (Keithley advices 100), this effect can be "integrated away" at the cost of measurement speed.
  • using an average filter: take multiple measurements and use the average
  • autozero: let the measurement validate itself by sampling a known internal reference

image

image source: Keithley Test Script Builder documentation for the Measuring DC voltage with high accuracy example

Measuring a 2.5 and 2.048 V reference

In the previous blog I measured voltage with one of the preconfigured DC Voltage presets: Autozero, 5 nplc, 20 moving average filter. Now I'm doing that with the settings from the example.

First measurement, on a 2.5V LM4128-2.5 reference , I configured the meter via the touch screen:

image

The second measurement, on a REF5020 2.048 V reference, was done by running the Measuring DC voltage with high accuracy example from the Test Script Builder:

image

As you can see on the 121GW, the measurements were made under tropical conditions. Comments and feedback welcome below.

  • Sign in to reply
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    That works too, measuring from reference out to buffer out, I had thought maybe REF1/2 were available on pin headers, I guess not.

    I assume the board is 4Layer with a solid ground plane. But on a two layer board with a patch work of ground islands you can see the ground reference drift all over the place due to various load currents. But even with a solid ground plane you can see get ground offset potentials....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to Jan Cumps

    (Sorry to be off-topic. But I wanted to comment that I sincerely like the Dymo label on the meter!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    I measured pin 6. I'll get at measuring that difference if I manage to tack a bodge wire to those two pins. For the reference itself, I could tack the wire to C24.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    Nice references! Were you measuring at pin6 of the REF5020 or the buffered ADC outputs ADC_REFX?

    You could measure between ADC_REF1 and ADC_REF2 to get an idea of what kind of uncertainty the OPA2350 is adding, ideally it should be zero Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    They reference these articles in the schematic:

    Miro Oljaca and Bonnie Baker, “How the Voltage Reference Affects ADC Performance, Part 2,” Analog Applications Journal (3Q 2009)

    How the voltage reference affects ADC performance, Part 3

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>