Test & Tools
  • Technologies
  • More
Test & Tools
Blog DIY $10 Solder-in Oscilloscope Probe
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 29 Nov 2020 4:51 PM Date Created
  • Views 7660 views
  • Likes 9 likes
  • Comments 6 comments
  • probing
  • oscilloscope probe
Related
Recommended

DIY $10 Solder-in Oscilloscope Probe

Jan Cumps
Jan Cumps
29 Nov 2020

It's sometimes hard to probe a point on a PCB.

Manufacturers sell "consumable" solder-in solutions.

You can temporarily or permanently attach them to your design, and it makes probing easier and reliable.

 

I have a suggestion for a DIY solder-in solution that takes little effort and is cheap + reusable:

 

image

 

Needed:

  • Vertical Mini Probe Socket, Keysight Infiniium Series Oscilloscopes
  • Two short ends of single stranded wire
  • A bit of heat shrink or isolation tape

 

image

source: keysight

 

How to Make:

  • Cut one of the ground pins away
  • Take a short piece of black and red single strand wire (what you use on your breadboard). Remove a small end of isolation at both ends.
  • Tin all the ends.
  • Solder the red wire to the middle pin
  • Solder the Black wire to the remaining outside pin
  • Apply heat shrink to avoid shortcuts when the device rests on the PCB. Don't overdo it, so that you can remove it later when the wires are worn out.

 

How to use:

Solder the two wires to the desired component in the circuit.

Typically, you'll want to solder the black one to ground, the red one to the point of interest.

If you're careful, you can solder this in many times. If needed, cut away a little end of the wire and you are set for many future uses.

Insert the probe, without hook and crocodile wire attached.

 

Why?

  • Keeping probes fixed is difficult. Once you have 2 probes in your hand and have to adjust a button, you are in trouble.
  • If you keep the 2 wires short, this is a decent probing technique. Way better than the crocodile ground loop and hook.
  • It's so cheap that, when you are working long time on a design, you can leave this in your prototype.
  • Sign in to reply

Top Comments

  • ajcc
    ajcc over 5 years ago +7
    Those are really nice probe holders for a DIY solution! Alan just use two coils of wire to hold his probes, although I think I've seen him use a single pin socket for the pointy tip in his later videos…
  • shabaz
    shabaz over 5 years ago +5
    Hi Jan, Great find! I didn't think of this idea - very neat! Also, it looks like it could be adapted to be soldered onto a nearby earth terminal using one of the sides, and then run a single wire, if the…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to ajcc +4
    I'm an Alan fan! I learned the techniques of DIY pitail winding and "make your own PCB inserts with wire" from him. edit: from the video you show above .
Parents
  • shabaz
    shabaz over 5 years ago

    Hi Jan,

     

    Great find! I didn't think of this idea - very neat! Also, it looks like it could be adapted to be soldered onto a nearby earth terminal using one of the sides, and then run a single wire, if the distance isn't far.

    By coincidence I was working a couple of nights ago to probe some stuff and really wished for solderable probes too. This was my attempt, it's still a work-in-progress. The yellow blob contains a 950 ohm resistor. I'll write it up once it is slightly more ruggedised implementation for anyone to assemble. It won't be as good as a normal probe of course, but sometimes a measurement is better than no measurement, at least to get some initial insight!

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 5 years ago

    Hi Jan,

     

    Great find! I didn't think of this idea - very neat! Also, it looks like it could be adapted to be soldered onto a nearby earth terminal using one of the sides, and then run a single wire, if the distance isn't far.

    By coincidence I was working a couple of nights ago to probe some stuff and really wished for solderable probes too. This was my attempt, it's still a work-in-progress. The yellow blob contains a 950 ohm resistor. I'll write it up once it is slightly more ruggedised implementation for anyone to assemble. It won't be as good as a normal probe of course, but sometimes a measurement is better than no measurement, at least to get some initial insight!

    image

    • Cancel
    • Vote Up +5 Vote Down