Test & Tools
  • Technologies
  • More
Test & Tools
Blog Easy Grounding for USB Soldering Irons
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 5 Jan 2023 12:45 AM Date Created
  • Views 12502 views
  • Likes 13 likes
  • Comments 23 comments
  • usb-c
  • earth bonding
  • usb-c pd
  • grounding
  • soldering iron
  • usb pd
  • esd
Related
Recommended

Easy Grounding for USB Soldering Irons

shabaz
shabaz
5 Jan 2023

Table of Contents

  • Introduction
  • What’s the Problem?
  • What’s the Solution?
  • Building It
  • Using It
  • Useful Items


Introduction

USB powered soldering irons are handy tools, however, they are fundamentally different to normal mains-powered soldering irons in that the tip is not grounded by default. This is not a major issue if the iron is battery-powered, but it can be a big problem if the iron is plugged into a mains-powered USB supply or USB phone charger. This blog post explains why, and what can be done about it.

What’s the Problem?

The problem is, some electronic components are sensitive to electrostatic discharge (ESD) and other voltage sources. It doesn’t even need to be a very high voltage; MOSFET gates for instance, could be damaged by a few tens of volts.

When the USB soldering iron is connected to a mains-powered USB source, due to the nature of how power supplies and phone chargers are built, there usually isn’t a good path to ground from either the USB 0V connection or from the USB metal shield. Instead, there can be a high voltage present on the 0V connection, relative to ground.

The photo shows this. The meter has one end connected to the tip of the soldering iron (plugged into a USB power source), and the other end of the meter was just held in the hand. The voltage, at 44V, is high enough that the warning indicator is present on the meter.

image

If you’re soldering a sensitive component, even if you’ve happily put on an ESD wrist strap and work on a grounded surface, the components will experience a high voltage from the tip of the USB-powered soldering iron and it’s game over for sensitive devices if any other pin happens to get touched or finds another path to ground. Taking ESD precautions but forgetting to ground the USB soldering iron can actually make the problem worse; the photo below shows an actual measured voltage.

image

What’s the Solution?

Simply put, the iron can be grounded. It’s also good to ground yourself, and so any USB soldering kit should contain a wrist strap too.

Many USB soldering irons come with a grounding solution, with a bit of wire that the user is expected to screw onto the iron and then the other end is connected to a ground point. That might be a bit impractical though!

Another option is to place a special USB cable in-line. The special cable has the shield or 0V wire broken out to a connector, ready for attaching to a ground point. This gets a bit awkward, especially with USB-C powered soldering irons; I’ve not seen such an in-line cable for USB-C (Edit: They certainly exist, I didn't have one).

I decided to take a simpler approach. The solution is to merely take a normal USB cable, cut it, and attach the shield to the grounding point. This works if the soldering iron is plugged into a USB power source that has more than one USB socket.

image

This is what it looks like:

image

Building It

To build the grounding cable, I took a normal USB cable and cut it into two. I used a USB-C / USB 2.0 cable, so that I could plug in either the USB-A or the USB-C connector depending on what is available. Before the cable is cut, a multimeter should be used to check that the metal shields are connected, because some USB cables leave the shields disconnected. I used an Amazon Basics cable.

I also took a normal earth bonding cable, and cut the end off, so that I could solder it to the shielding braid in the USB cable. Note that some earth bonding cables use tinsel wire, which is a bit more awkward to solder, but not too difficult; it just needs a bit of heat.

The photo below shows how I did the assembly. None of the work is very critical, just make sure that the red, green and white cables do not touch each other. I also tried to keep the 0V wire separate from the braid (some cables will connect these anyway; the Amazon Basics cable I used has them connected. Finally, I used heatshrink to protect it all.

image

Using It

The photo below shows the final cable.

image

As a test, I plugged it in and re-measured the voltage present on the tip of the soldering iron; now it’s just 1.3V, much better!

image

Useful Items

ESD grounding cord 

Anti-Static Wrist Strap  

Earth bonding plug UK 

Earth bonding plug EU 

(Can't find an earth bonding plug for the US and other regions, but please leave a link if you have a recommendation!).

  • Sign in to reply
Parents
  • jaybeuff
    jaybeuff over 3 years ago

    Sorry for reviving from the dead but couldn’t one use one of these cables modified to usbc plugged into a second isbc port?    
    image

    www.amazon.com/.../B07Z1DXW7B

    Would take up less space than the two larger dedicated esd ground/earthing plug mentioned already.

    I did find a nice usbc charger that had a US 110v mains port on its side but it sadly does not output 12v.  Only 5/9/15/20 with 45w max.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jaybeuff
    jaybeuff over 3 years ago

    Sorry for reviving from the dead but couldn’t one use one of these cables modified to usbc plugged into a second isbc port?    
    image

    www.amazon.com/.../B07Z1DXW7B

    Would take up less space than the two larger dedicated esd ground/earthing plug mentioned already.

    I did find a nice usbc charger that had a US 110v mains port on its side but it sadly does not output 12v.  Only 5/9/15/20 with 45w max.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 3 years ago in reply to jaybeuff

    Hi Jay,

    The cable you show in the photo would be fine, with the USB-C connector at one end as you say. I just happened to cut an existing USB-C cable because I didn't have a connector on its own, hence the ugly heat-shrunk joining of cables. The cleaner option would be to take a cable like you show and a USB-C connector.

    Regarding chargers, many of the recent Ugreen chargers seem to offer 12V (but not 100% sure if they all do from that manufacturer), whereas Anker ones do not unfortunately.

    If anyone reading this knows of others that output 12V, it would be great if they could leave a comment with the manufacturer/model details.