Test & Tools
  • Technologies
  • More
Test & Tools
Blog Easy Grounding for USB Soldering Irons
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 5 Jan 2023 12:45 AM Date Created
  • Views 12515 views
  • Likes 13 likes
  • Comments 23 comments
  • usb-c
  • earth bonding
  • usb-c pd
  • grounding
  • soldering iron
  • usb pd
  • esd
Related
Recommended

Easy Grounding for USB Soldering Irons

shabaz
shabaz
5 Jan 2023

Table of Contents

  • Introduction
  • What’s the Problem?
  • What’s the Solution?
  • Building It
  • Using It
  • Useful Items


Introduction

USB powered soldering irons are handy tools, however, they are fundamentally different to normal mains-powered soldering irons in that the tip is not grounded by default. This is not a major issue if the iron is battery-powered, but it can be a big problem if the iron is plugged into a mains-powered USB supply or USB phone charger. This blog post explains why, and what can be done about it.

What’s the Problem?

The problem is, some electronic components are sensitive to electrostatic discharge (ESD) and other voltage sources. It doesn’t even need to be a very high voltage; MOSFET gates for instance, could be damaged by a few tens of volts.

When the USB soldering iron is connected to a mains-powered USB source, due to the nature of how power supplies and phone chargers are built, there usually isn’t a good path to ground from either the USB 0V connection or from the USB metal shield. Instead, there can be a high voltage present on the 0V connection, relative to ground.

The photo shows this. The meter has one end connected to the tip of the soldering iron (plugged into a USB power source), and the other end of the meter was just held in the hand. The voltage, at 44V, is high enough that the warning indicator is present on the meter.

image

If you’re soldering a sensitive component, even if you’ve happily put on an ESD wrist strap and work on a grounded surface, the components will experience a high voltage from the tip of the USB-powered soldering iron and it’s game over for sensitive devices if any other pin happens to get touched or finds another path to ground. Taking ESD precautions but forgetting to ground the USB soldering iron can actually make the problem worse; the photo below shows an actual measured voltage.

image

What’s the Solution?

Simply put, the iron can be grounded. It’s also good to ground yourself, and so any USB soldering kit should contain a wrist strap too.

Many USB soldering irons come with a grounding solution, with a bit of wire that the user is expected to screw onto the iron and then the other end is connected to a ground point. That might be a bit impractical though!

Another option is to place a special USB cable in-line. The special cable has the shield or 0V wire broken out to a connector, ready for attaching to a ground point. This gets a bit awkward, especially with USB-C powered soldering irons; I’ve not seen such an in-line cable for USB-C (Edit: They certainly exist, I didn't have one).

I decided to take a simpler approach. The solution is to merely take a normal USB cable, cut it, and attach the shield to the grounding point. This works if the soldering iron is plugged into a USB power source that has more than one USB socket.

image

This is what it looks like:

image

Building It

To build the grounding cable, I took a normal USB cable and cut it into two. I used a USB-C / USB 2.0 cable, so that I could plug in either the USB-A or the USB-C connector depending on what is available. Before the cable is cut, a multimeter should be used to check that the metal shields are connected, because some USB cables leave the shields disconnected. I used an Amazon Basics cable.

I also took a normal earth bonding cable, and cut the end off, so that I could solder it to the shielding braid in the USB cable. Note that some earth bonding cables use tinsel wire, which is a bit more awkward to solder, but not too difficult; it just needs a bit of heat.

The photo below shows how I did the assembly. None of the work is very critical, just make sure that the red, green and white cables do not touch each other. I also tried to keep the 0V wire separate from the braid (some cables will connect these anyway; the Amazon Basics cable I used has them connected. Finally, I used heatshrink to protect it all.

image

Using It

The photo below shows the final cable.

image

As a test, I plugged it in and re-measured the voltage present on the tip of the soldering iron; now it’s just 1.3V, much better!

image

Useful Items

ESD grounding cord 

Anti-Static Wrist Strap  

Earth bonding plug UK 

Earth bonding plug EU 

(Can't find an earth bonding plug for the US and other regions, but please leave a link if you have a recommendation!).

  • Sign in to reply
Parents
  • Andrew J
    Andrew J over 3 years ago

    Can I clarify?  You:

    • cut the USB cable in two so you could use either connector
    • For each of the cut ends, you trimmed away the outer sheathing, ensured that the coloured wires were not exposed, trimmed down the 0V bare wire so it couldn’t touch anything, trimmed back the foil and twisted the braid together to form “a wire”.  Left you with two identical ends of exposed braid.
    • cut the end off the grounding wire, trimmed back the sheath to expose the internal wire
    • soldered both the twisted braids and the exposed ground wire together
    • covered the joint in heat shrink.

    I’m assuming you are earthing the USB power source that the soldering iron is plugged into which implies the USB sockets on that source share a common ground? Would that work if the USB sockets were on a laptop or PC?  Could you create a in-line ground point in the cable actually used to power it - I.e the cable has three connectors: to the iron, to the USB port and to the grounding point - guess this might get a bit clumsy?  Sorry, I feel a bit dumb, I just didn’t get it from the pictures.  It’s a great post and a great idea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Andrew J

    Hi Andrew,

    Sorry, I was trying to write minimal amount because of the site and editor tools, didn't even write a summary!

    You're right, it needs a better explanation. Hopefully the diagram below helps. As Jan says, a desktop PC would be earthed, but due to other power supplies having either having no earth connection, and isolated transformer, it will end up having a voltage capacitively coupled from the mains side.

    The cable with three connectors that you refer to, I ended up calling  "in-line" in the blog post. That's a good option.  This blog post is just another option to add to the list, a normal USB cable is more likely to be found at home, so it could be easier to just chop up a spare cable. It would be fine to use an in-line cable and peel off the insulation at a portion, and splice on the third connection.

    The method I used has the disadvantage that it wastes a USB port while you're soldering.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to shabaz

    (Can't edit; added the diagram to the blog post)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to shabaz

    I guess if you were going to attach a grounding wire to the USB cable powering the iron, you might as well as h it to the ground point of the iron.  There would be some handling advantage to exposing the shielding right by the connector connected to the power source and connecting to ground from there, particularly if the power plug and grounding plug were next to each other in the extension lead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Andrew J

    That would be ideal. I wish the USB soldering iron manufacturers would provide the solution as part of their USB soldering iron kits, i.e. the USB cable with the connection broken out, plus the wrist strap, otherwise I can imagine a load of people using the iron as if it were a normal mains-powered iron, and wondering why their circuits are now partially faulty. I think beginners are more likely to buy a USB soldering iron, because they may be students, wishing to have a compact light solution, so it's unfortunate that the grounding isn't part of the supplied kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 3 years ago in reply to Andrew J

    That would be ideal. I wish the USB soldering iron manufacturers would provide the solution as part of their USB soldering iron kits, i.e. the USB cable with the connection broken out, plus the wrist strap, otherwise I can imagine a load of people using the iron as if it were a normal mains-powered iron, and wondering why their circuits are now partially faulty. I think beginners are more likely to buy a USB soldering iron, because they may be students, wishing to have a compact light solution, so it's unfortunate that the grounding isn't part of the supplied kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Andrew J
    Andrew J over 3 years ago in reply to shabaz

    It would seem reasonable, right!?!?