Test & Tools
  • Technologies
  • More
Test & Tools
Blog mini project: PICO-PI programmable Lab Switch - 4: Your Homework - extra pins
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 20 Oct 2022 7:02 PM Date Created
  • Views 1847 views
  • Likes 7 likes
  • Comments 8 comments
  • pico_freertos_scpi_switch
Related
Recommended

mini project: PICO-PI programmable Lab Switch - 4: Your Homework - extra pins

Jan Cumps
Jan Cumps
20 Oct 2022

In this series, I design a programmable lab switch based on RP2040, that can turn a set of signals or supplies on or off. Over USB. SCPI compatible.
In the previous post I gave you homework, but you didn't do it Slight smile. So I'll pick up task 1 and 2:

  • very easy: extend the array of pins. Currently it's an array of 1 element (the LED), but you can define many. All GPIOs if you want.
    The input validation will automatically adapt to the array size and only stack an error if you pass an index out of array range in the command
    Don't forget to initialise these pins as outputs in the main() function
  • very easy: write code that initialises the pins automatically: loop over all array items and set them as outputs.

Task 1: extend the array of pins

Currently it's an array of 1 element (the LED), but you can define many. All GPIOs if you want.
The input validation will automatically adapt to the array size and only stack an error if you pass an index out of array range in the command
Don't forget to initialise these pins as outputs in the main() function

This is easy. I had prepared the code to deal with more than one pin. It originally only had a single definition: the on-board LED. But I had already (visionary :) ) placed it in an array:

// supported pins
uint pins[] = {PICO_DEFAULT_LED_PIN};

Let's add another pin. GP22 on pin 29 of the Pico. Why: because it's a pure GPIO pin, no other function. You can add any number of pins more if you want (homework).

uint pins[] = {PICO_DEFAULT_LED_PIN, 22};

Let's also move the definition out of the scpi sources, and place it in its own source file gpio/gpio_utils.c, where we also will put the code of task 2.

#include "hardware/gpio.h"

#include "gpio_utils.h"

// supported pins
uint pins[] = {PICO_DEFAULT_LED_PIN, 22};


uint32_t pinCount() {
    return sizeof(pins)/sizeof(pins[0]);
}

void setPinAt(uint32_t index, bool on) {
    gpio_put(pins[index], on);
}

You can see that I've taken the opportunity to add 2 helper functions, so that the scpi code doesn't have to know how many pins we have and how we store them. Here's the corresponding header, gpio/gpio_utils.h I created a corresponding header file:

#ifndef _GPIO_UTILS_H
#define _GPIO_UTILS_H


uint32_t pinCount();
void setPinAt(uint32_t index, bool on);

#endif // _GPIO_UTILS_H

The code in the scpi parser now becomes very easy:

#include "gpio_utils.h"


// ...

  // retrieve the output index
  SCPI_CommandNumbers(context, numbers, 1, 0);
  if (! ((numbers[0] > -1) && (numbers[0] < pinCount()))) {
    SCPI_ErrorPush(context, SCPI_ERROR_INVALID_SUFFIX);
    return SCPI_RES_ERR;
  }

  /* read first parameter if present */
  if (!SCPI_ParamBool(context, &param1, TRUE)) {
    return SCPI_RES_ERR;
  }

  setPinAt(numbers[0], param1 ? true : false);
  
// ...  

You see the use of pinCount() and setPinAt() helpers here. Cleaner, simpler to maintain, and change the set of supported pins.

Task 2: write code that initialises the pins automatically

loop over all array items and set them as outputs.

In the original code, I configured the pin that I used in the main file. Now that we have the utility files, let's create an initialisation function that will work for 1 pin and many pins:

void initPins() {
    for (uint32_t i = 0; i < pinCount(); i++) {
        gpio_init(pins[i]);
        gpio_set_dir(pins[i], 1);
        gpio_put(pins[i], 0);
    }
}

I've put it in the header file too, so that it can be called from main. 

In the initialisation code, you get this:

    // ...
    stdio_init_all();
    initPins();
    initUART();
    // ...

Show all blog posts

  • Sign in to reply
Parents
  • dougw
    dougw over 3 years ago

    I works for me when somebody else does my homework for me. Relaxed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 3 years ago

    I works for me when somebody else does my homework for me. Relaxed