Test & Tools
  • Technologies
  • More
Test & Tools
Blog Mini Tool Vice / Flat Clamp Quick Review
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 15 Mar 2024 1:13 AM Date Created
  • Views 2974 views
  • Likes 8 likes
  • Comments 1 comment
  • vise
  • pcb_holder
  • PCB vises
  • pcb vices
  • vice
  • pcb holder
  • vises
Related
Recommended

Mini Tool Vice / Flat Clamp Quick Review

shabaz
shabaz
15 Mar 2024


Doug mentioned vices (  PCB Holders ) , and I picked up a small tool vice recently. It’s low-cost (£15) which is good, but very small, therefore it is a niche product. It won’t hold boards greater than about 49-50mm long, so that’s a showstopper for a lot of PCBs.

The photo below shows how it could be used (but not how I will use it).

The tool is lightweight (220 grams) but shouldn’t slide around on typical ESD mats.

image

Is it any good? I’d say it is average. On the plus side, the finish is excellent. It’s all aluminium. The sliding jaw moves with very little effort, it is easy-to-use.

image

The decent finish extends to the underside.

image

The knob is aluminium too.

image

All the topmost surfaces have M5 tapped holes (spaced 20 mm apart), which is excellent, although you might find (as I did) that some of the holes need re-tapping if you don’t want to force the screw in. The base of the vice has M5 clearance untapped holes.

image

What’s not to like? I think the main Achille’s heel is that the vice uses a simple threaded rod that is quite thin (just under 6 mm). A slight knock will probably bend it. However, until that time comes, I think this vice will be quite nice to use. High-end clamps will be of all-steel construction, and will have a proper leadscrew.

Another negative is that the jaws, as supplied, are not fit for PCB usage, but I knew that at the time of purchase from a visual inspection of the product photos. My plan is to make plastic jaws that will screw onto the top.

image

Is it worth the £15? I think it’s worth £8.99. If you want a ready-to-go tool vice, and don’t really need such a compact one, and prefer an aluminium one that is slightly larger and more practical, then such tools are already available at a similar price (or less).

image

If you want very stable mounting to build a testbed, then there are no two ways around it. You'll need to skip the alu and go for decent steel tool vices; check out the photo by michaelkellett  in the comments here: PCB Holders  

Thanks for reading!

  • Sign in to reply
  • shabaz
    shabaz over 2 years ago

    I gave it a shot today, making custom jaws. I went with aluminium rather than plastic in the end.

    Not sure how I got both measurements wrong! They were nice round numbers.

    image

    I won't fix it, since it's minor. A side-benefit is that I don't need to make a vertical central notch for the times I need that, because the red notch is still usable.

    image

    Personally I'd prefer screws to be completely flush on the top of the vice,  but I have a lot of M5 bolts so it was time to use some.

    That vertical red notch is handy for circular connector clamping:

    image

    PCB in these new jaws: