Test & Tools
  • Technologies
  • More
Test & Tools
Blog My Kingdom for a good pair of flush cutters.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 6 Nov 2018 5:18 AM Date Created
  • Views 14495 views
  • Likes 15 likes
  • Comments 22 comments
  • flush_cutter
  • aven
Related
Recommended

My Kingdom for a good pair of flush cutters.

jw0752
jw0752
6 Nov 2018

One of my favorite tools is the Flush Cutter. I like them so much that I have seven of them right now. Yes besides the Multimeters and Bench Power Supplies I have also have a flush cutter addiction.

 

image

 

In the course of my daily play in the shop I am constantly working with soldering components and clipping leads. A good flush cutter fits the hand well and has a spring action that opens as one's grip is relaxed. The cutter jaws must close evenly and not allow any sunlight to pass through the closure. A sharp cutting edge on the jaw will cut the lead without snapping it off. This is important as it keeps the cut lead from acquiring kinetic energy from the cutting action and shooting off across the room. The metal of the jaw must be substantial and there should be no lateral play in the pivot point. If there is lateral play in the pivot point the cutting edges will skew and twist the lead as they attempt to cut it. This is not pretty and makes one regret having paid money for the tool. The metal of the cutter must be hard enough to hold its sharpness through a large number of clippings and yet not so hard that it becomes brittle and chips easily. If the metal of the cutter isn't hard enough then the edge will loose its sharpness quickly and not make a good cut. The machining of the tip of the cutter must be exact so that a small diameter wire can be cut with the very end. This is necessary when cutting wires that are laying along a hard surface.

 

Until today I have never had a cutter that met all of these desirable characteristics.

 

Enter the AVEN  10826F10826F Flush Cutter

 

https://www.newark.com/aven/10826f/tapered-cutter-flush-with-relief/dp/77R0845?ost=Aven++10826F&krypto=Sj%2BpzdBxkiJWpvwtYjEGjVfCbaYGgFBQwHCH8rV2iVIEjaMFETh0yoM1KVN9pb8BZPPTXdKNPFnZTvn7EmnkLF%2FakFZ86Z4lNhZFpQ46rNEd1TRPlEjIZxciR9XE%2Fc5QlRkkjfGbPw4bcHhZ75ct1R150T6gVw3AqHpvYzr2NA%2BnBpZY8epvrdf5dswNZac98wL8kWMoYSdgdRfxr0QUyxqAeT4gQ4nIWi48OxZy%2F8btqUpejamLc%2BYd1%2Fshp93xU%2Fp4Gzfu7ZhKzAmF6QPRhRqniBxU3rcmDTJYGYmjFGjmnOZ4VbG%2F9fdzndpQMp%2FdmYb787zSS2il3KNAtdAqGVQgzjYoKOvC%2BJ4vBDjlP7JBFk7zSpJE6CWT%2Fe77ZPle8MdHkCtBb%2BasiuqSlO09n2cBeKP64kT2IvBYLCw4ku8%3D&ddkey=https%3Aen-US%2FElement14_US%2Fsearch

 

I had a chance to look at a pair of these flush cutters at the recent Embedded Systems Show that I attended and decided to give them a try. At $25 they are the most expensive flush cutters that I have ever used but after testing them out it became apparent that I have been wasting my money for many years on cheaper compromises. The first test I ran was to see if I could cut a piece of 30 GA wire (0.25 mm) that was laid flat on a piece of glass with the tip of the AVEN 826.

 

image

 

The 826 engaged the wire and I could feel the cut as it separated the wire. If you look closely at the wire to the right of the 826 you will see a slight bend. This bend is the result of attempting to cut the same wire twice with my next best flush cutters which cost me $16.

 

The 826 pliers are made of special hardened cast steel as opposed to the stamped metal usually associated with flush cutters. The picture above is a good illustration of the difference. Furthermore the pivot point of the 826 is secured with a fastener and not a rivet as is common on the lower priced tools. Here are a couple pictures of the AVEN pivot point.

 

imageimage

If I try to move the handles of the $16 cutters laterally I can feel a definite looseness that does not exist when I try the same test with the AVEN.

 

If these features weren't enough the AVEN cutter also has special ESD resistant hand grips which is a feature I didn't even realize existed. Up to now just being insulated was enough.

 

image

 

If you like Flush Cutters like I do and if the pair you are currently using is in need of replacement don't make the mistake I have been making for years and get a pair of the $16 cutters. There really isn't that much difference in cost between a quality compromise and a pair of flush cutters that are going to make you smile.

 

image

 

AVEN  10826F10826F

 

John

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +8
    The thing I have out of proportion to all other tools I own is hammers. I have many claw hammers, ball peen hammers, roofing hammer, cobblers hammer, mallets, sledge, mauls, pick... All but two or three…
  • dougw
    dougw over 7 years ago +7
    Great topic. I don't know how you put your finger on a great topic like this. It would never occur to me to discuss side cutters, but now that you mention it, I definitely could say a lot... I will just…
  • luislabmo
    luislabmo over 7 years ago +7
    Hi John, This is a nice review!. I've been lucky enough to get my favorite flush cutters as a first time buyer, the Hakko CHP-170 Micro Cutter . Probably not as good as the AVEN but in my opinion they…
Parents
  • hlipka
    hlipka over 7 years ago

    Knipex is a well-known and highly regarded brand here in Germany. Usually you will not go wrong buying them.

    But for electronics tools I have grown fond of another brand: Engineer Inc. from Japan. I own the NS-03 side cutter (or 'micro nipper' as they call it), and several other tools from their product line. They are quite expensive, but for now they are all worth it.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to hlipka

    I agree with you. Engineer Inc. manufactures very good stuff for electronics. I also own few tools from them and they are very good.

     

    Luis

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hlipka
    hlipka over 7 years ago in reply to luislabmo

    They also have a number of tools that are otherwise hard to find (e.g. their low-profile ratchets and wrenches, the screw-removal pliers or the ceramic-tipped pliers). You don't need them that often, but when you do they are indispensable.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to hlipka

    Yup, that is right. I think one of those hard to find rarities is their solder sucker with Silicone Tip, and you can get replacement tips for it. I don't own it yet but is something in my wish list.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • luislabmo
    luislabmo over 7 years ago in reply to hlipka

    Yup, that is right. I think one of those hard to find rarities is their solder sucker with Silicone Tip, and you can get replacement tips for it. I don't own it yet but is something in my wish list.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • hlipka
    hlipka over 7 years ago in reply to luislabmo

    I can only recommend to buy it. Its so much better than the regular solder suckers that it is really worth its money. I have mine for maybe three years now (maybe even longer), and are still using the first tip (and it comes with one replacement tip). Did throw out my old solder sucker right away after using the new one.