Test & Tools
  • Technologies
  • More
Test & Tools
Blog My Kingdom for a good pair of flush cutters.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 6 Nov 2018 5:18 AM Date Created
  • Views 14483 views
  • Likes 15 likes
  • Comments 22 comments
  • flush_cutter
  • aven
Related
Recommended

My Kingdom for a good pair of flush cutters.

jw0752
jw0752
6 Nov 2018

One of my favorite tools is the Flush Cutter. I like them so much that I have seven of them right now. Yes besides the Multimeters and Bench Power Supplies I have also have a flush cutter addiction.

 

image

 

In the course of my daily play in the shop I am constantly working with soldering components and clipping leads. A good flush cutter fits the hand well and has a spring action that opens as one's grip is relaxed. The cutter jaws must close evenly and not allow any sunlight to pass through the closure. A sharp cutting edge on the jaw will cut the lead without snapping it off. This is important as it keeps the cut lead from acquiring kinetic energy from the cutting action and shooting off across the room. The metal of the jaw must be substantial and there should be no lateral play in the pivot point. If there is lateral play in the pivot point the cutting edges will skew and twist the lead as they attempt to cut it. This is not pretty and makes one regret having paid money for the tool. The metal of the cutter must be hard enough to hold its sharpness through a large number of clippings and yet not so hard that it becomes brittle and chips easily. If the metal of the cutter isn't hard enough then the edge will loose its sharpness quickly and not make a good cut. The machining of the tip of the cutter must be exact so that a small diameter wire can be cut with the very end. This is necessary when cutting wires that are laying along a hard surface.

 

Until today I have never had a cutter that met all of these desirable characteristics.

 

Enter the AVEN  10826F10826F Flush Cutter

 

https://www.newark.com/aven/10826f/tapered-cutter-flush-with-relief/dp/77R0845?ost=Aven++10826F&krypto=Sj%2BpzdBxkiJWpvwtYjEGjVfCbaYGgFBQwHCH8rV2iVIEjaMFETh0yoM1KVN9pb8BZPPTXdKNPFnZTvn7EmnkLF%2FakFZ86Z4lNhZFpQ46rNEd1TRPlEjIZxciR9XE%2Fc5QlRkkjfGbPw4bcHhZ75ct1R150T6gVw3AqHpvYzr2NA%2BnBpZY8epvrdf5dswNZac98wL8kWMoYSdgdRfxr0QUyxqAeT4gQ4nIWi48OxZy%2F8btqUpejamLc%2BYd1%2Fshp93xU%2Fp4Gzfu7ZhKzAmF6QPRhRqniBxU3rcmDTJYGYmjFGjmnOZ4VbG%2F9fdzndpQMp%2FdmYb787zSS2il3KNAtdAqGVQgzjYoKOvC%2BJ4vBDjlP7JBFk7zSpJE6CWT%2Fe77ZPle8MdHkCtBb%2BasiuqSlO09n2cBeKP64kT2IvBYLCw4ku8%3D&ddkey=https%3Aen-US%2FElement14_US%2Fsearch

 

I had a chance to look at a pair of these flush cutters at the recent Embedded Systems Show that I attended and decided to give them a try. At $25 they are the most expensive flush cutters that I have ever used but after testing them out it became apparent that I have been wasting my money for many years on cheaper compromises. The first test I ran was to see if I could cut a piece of 30 GA wire (0.25 mm) that was laid flat on a piece of glass with the tip of the AVEN 826.

 

image

 

The 826 engaged the wire and I could feel the cut as it separated the wire. If you look closely at the wire to the right of the 826 you will see a slight bend. This bend is the result of attempting to cut the same wire twice with my next best flush cutters which cost me $16.

 

The 826 pliers are made of special hardened cast steel as opposed to the stamped metal usually associated with flush cutters. The picture above is a good illustration of the difference. Furthermore the pivot point of the 826 is secured with a fastener and not a rivet as is common on the lower priced tools. Here are a couple pictures of the AVEN pivot point.

 

imageimage

If I try to move the handles of the $16 cutters laterally I can feel a definite looseness that does not exist when I try the same test with the AVEN.

 

If these features weren't enough the AVEN cutter also has special ESD resistant hand grips which is a feature I didn't even realize existed. Up to now just being insulated was enough.

 

image

 

If you like Flush Cutters like I do and if the pair you are currently using is in need of replacement don't make the mistake I have been making for years and get a pair of the $16 cutters. There really isn't that much difference in cost between a quality compromise and a pair of flush cutters that are going to make you smile.

 

image

 

AVEN  10826F10826F

 

John

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +8
    The thing I have out of proportion to all other tools I own is hammers. I have many claw hammers, ball peen hammers, roofing hammer, cobblers hammer, mallets, sledge, mauls, pick... All but two or three…
  • dougw
    dougw over 7 years ago +7
    Great topic. I don't know how you put your finger on a great topic like this. It would never occur to me to discuss side cutters, but now that you mention it, I definitely could say a lot... I will just…
  • luislabmo
    luislabmo over 7 years ago +7
    Hi John, This is a nice review!. I've been lucky enough to get my favorite flush cutters as a first time buyer, the Hakko CHP-170 Micro Cutter . Probably not as good as the AVEN but in my opinion they…
  • genebren
    genebren over 7 years ago in reply to Gough Lui

    Gough,

     

    Those Knipex cutters look really nice.  Oh no, now I have to chose, or do I?

     

    Pull out that PS-900.  I absolutely love mine.  I have been using it for  ~1 year and it sure works better than my old Weller.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago

    I've heard good things about Knipex ones - these don't look too expensive and could probably be decent:

    https://au.element14.com/knipex/78-03-125/cutter-side/dp/413403501?st=Connect27-ALL-PRODUCTS

    I say "could", because I actually bought a set from element14 back last when they had a special. But I could never bring myself to use them. As a bit of a serial tool abuser ... I wasn't going to take out the "best" stuff for my everyday work. As a result, I live with the Duratool stuff:

    https://au.element14.com/duratool/pl-501/cutter-micro-5/dp/115600101

     

    It does exactly all those "nasty" things you mentioned - there's a bit of play in the pivot after a few uses, so the blades don't come together "exactly" and let light through. They don't bite-down quite exactly and do fling wire scraps across the room. I've even managed to have a few jaws "snap" suddenly after a year or so of usage.

     

    But ... I don't mind this at all. While it has always been something I've been aware of, I've gotten used to operating with it - so I always "hold" the scrap or shield it to stop it flying, I don't apply silly amounts of force and I never expect a perfectly flush cut. Being as cheap as they are, I end up using them to cut all manner of things - at one stage I caught myself nibbling through a plastic enclosure with a pair of them out of desperation. I certainly wouldn't want to wreck a decent one doing that kind of "work". As someone who only has a limited supply of basic tools ... I guess I'm as much at fault as the cutters themselves image.

     

    Maybe I will take the Knipex ones out of the bag for a quick spin ... speaking of which, I also have a Metcal PS-900 station under my bed ... another one I wasn't willing to destroy ... so I use a Tenma combination hot-air and soldering iron station instead. I just can't be trusted with nice tools image.

     

    - Gough

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    John,

     

    Great blog!  I love high quality hand tools (actually almost any tool).  I recently picked up some PLATO cutters (https://www.newark.com/plato/175/shear-cutter-1mm/dp/98H3232?st=plato%20175) as part of a prize package (cool tools bench awards), which I really like.  Although, I used tried the cutting of 30 gauge wire placed on glass and they did not quiet do as well (nicked but did not cut the wire).  I will have to investigate these cutters and see if there is a set out there that needs a new home.

     

    Thanks for the heads up a high quality tool!

    Gene

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 7 years ago

    Nice blog, they certainly look like good quality cutters. I just use the two mini-side cutters;

     

    image

     

    The green handled 45 degree cutters stay at home and are what I generally use on the odd bits and pieces of electronics I build. They are many years old now from the now defunct Maplin stores we used to have in the UK.

     

    The Knipex cutters go in my works tool bag and seem to spend more time cutting off tyraps rather than electronics work.

     

    After that my side cutters grow up a little bit.

     

    Kind regards.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to luislabmo

    Hi Luis,

     

    The Hakko cutters are very functional and I have used similar one for years and you can't beat that price. Unfortunately I have tried the AVEN and now I am spoiled.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>