Test & Tools
  • Technologies
  • More
Test & Tools
Blog My Kingdom for a good pair of flush cutters.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 6 Nov 2018 5:18 AM Date Created
  • Views 14486 views
  • Likes 15 likes
  • Comments 22 comments
  • flush_cutter
  • aven
Related
Recommended

My Kingdom for a good pair of flush cutters.

jw0752
jw0752
6 Nov 2018

One of my favorite tools is the Flush Cutter. I like them so much that I have seven of them right now. Yes besides the Multimeters and Bench Power Supplies I have also have a flush cutter addiction.

 

image

 

In the course of my daily play in the shop I am constantly working with soldering components and clipping leads. A good flush cutter fits the hand well and has a spring action that opens as one's grip is relaxed. The cutter jaws must close evenly and not allow any sunlight to pass through the closure. A sharp cutting edge on the jaw will cut the lead without snapping it off. This is important as it keeps the cut lead from acquiring kinetic energy from the cutting action and shooting off across the room. The metal of the jaw must be substantial and there should be no lateral play in the pivot point. If there is lateral play in the pivot point the cutting edges will skew and twist the lead as they attempt to cut it. This is not pretty and makes one regret having paid money for the tool. The metal of the cutter must be hard enough to hold its sharpness through a large number of clippings and yet not so hard that it becomes brittle and chips easily. If the metal of the cutter isn't hard enough then the edge will loose its sharpness quickly and not make a good cut. The machining of the tip of the cutter must be exact so that a small diameter wire can be cut with the very end. This is necessary when cutting wires that are laying along a hard surface.

 

Until today I have never had a cutter that met all of these desirable characteristics.

 

Enter the AVEN  10826F10826F Flush Cutter

 

https://www.newark.com/aven/10826f/tapered-cutter-flush-with-relief/dp/77R0845?ost=Aven++10826F&krypto=Sj%2BpzdBxkiJWpvwtYjEGjVfCbaYGgFBQwHCH8rV2iVIEjaMFETh0yoM1KVN9pb8BZPPTXdKNPFnZTvn7EmnkLF%2FakFZ86Z4lNhZFpQ46rNEd1TRPlEjIZxciR9XE%2Fc5QlRkkjfGbPw4bcHhZ75ct1R150T6gVw3AqHpvYzr2NA%2BnBpZY8epvrdf5dswNZac98wL8kWMoYSdgdRfxr0QUyxqAeT4gQ4nIWi48OxZy%2F8btqUpejamLc%2BYd1%2Fshp93xU%2Fp4Gzfu7ZhKzAmF6QPRhRqniBxU3rcmDTJYGYmjFGjmnOZ4VbG%2F9fdzndpQMp%2FdmYb787zSS2il3KNAtdAqGVQgzjYoKOvC%2BJ4vBDjlP7JBFk7zSpJE6CWT%2Fe77ZPle8MdHkCtBb%2BasiuqSlO09n2cBeKP64kT2IvBYLCw4ku8%3D&ddkey=https%3Aen-US%2FElement14_US%2Fsearch

 

I had a chance to look at a pair of these flush cutters at the recent Embedded Systems Show that I attended and decided to give them a try. At $25 they are the most expensive flush cutters that I have ever used but after testing them out it became apparent that I have been wasting my money for many years on cheaper compromises. The first test I ran was to see if I could cut a piece of 30 GA wire (0.25 mm) that was laid flat on a piece of glass with the tip of the AVEN 826.

 

image

 

The 826 engaged the wire and I could feel the cut as it separated the wire. If you look closely at the wire to the right of the 826 you will see a slight bend. This bend is the result of attempting to cut the same wire twice with my next best flush cutters which cost me $16.

 

The 826 pliers are made of special hardened cast steel as opposed to the stamped metal usually associated with flush cutters. The picture above is a good illustration of the difference. Furthermore the pivot point of the 826 is secured with a fastener and not a rivet as is common on the lower priced tools. Here are a couple pictures of the AVEN pivot point.

 

imageimage

If I try to move the handles of the $16 cutters laterally I can feel a definite looseness that does not exist when I try the same test with the AVEN.

 

If these features weren't enough the AVEN cutter also has special ESD resistant hand grips which is a feature I didn't even realize existed. Up to now just being insulated was enough.

 

image

 

If you like Flush Cutters like I do and if the pair you are currently using is in need of replacement don't make the mistake I have been making for years and get a pair of the $16 cutters. There really isn't that much difference in cost between a quality compromise and a pair of flush cutters that are going to make you smile.

 

image

 

AVEN  10826F10826F

 

John

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +8
    The thing I have out of proportion to all other tools I own is hammers. I have many claw hammers, ball peen hammers, roofing hammer, cobblers hammer, mallets, sledge, mauls, pick... All but two or three…
  • dougw
    dougw over 7 years ago +7
    Great topic. I don't know how you put your finger on a great topic like this. It would never occur to me to discuss side cutters, but now that you mention it, I definitely could say a lot... I will just…
  • luislabmo
    luislabmo over 7 years ago +7
    Hi John, This is a nice review!. I've been lucky enough to get my favorite flush cutters as a first time buyer, the Hakko CHP-170 Micro Cutter . Probably not as good as the AVEN but in my opinion they…
  • jw0752
    jw0752 over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    You comment on the ESD has peaked my curiosity as to just what the resistance of the ESD material in the handles is. Tonight I will see if I can make an experiment using the megger to measure the resistance, tool metal to hand of the grips.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to fmilburn

    Hi Frank,

     

    I had an old engine rebuilder tell me once that you can fix anything if you have a big enough hammer. I believe he had a twinkle in his eye when he said it though. It is amazing how the human penchant for tool building can take an idea as simple as the hammer and morph it into so many specialized applications.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to dougw

    Hi Doug,

     

    I am going to get some 40 gauge wire and see if I can pick it up with the pliers in my tool cabinet. I have serious doubts that I have any that precise. Before my retirement I had access to a lot of medical grade tools and so I have a good selection of forceps and tweezers that help with some of the specialized material handling problems. Now that I have had a chance to check out the AVEN cutters I will have to take a look at some of their needle nose pliers as well.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 7 years ago

    Hi John,

     

    This is a nice review!. I've been lucky enough to get my favorite flush cutters as a first time buyer, the Hakko CHP-170 Micro Cutter. Probably not as good as the AVEN but in my opinion they meet all the criteria except shooting the pins flying (wire is fine, pins go flying -not a lot but they do), not a bad trade considering they only cost $5 in the US. I think your review was posted at the right time... according to Newark the CHP170 are no longer manufactured. Probably they will be out of the market soon.

     

    Luis

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi John,

     

    Excellent tool review! We're lucky being engineers, we can get decent tools if we search them out like you have. A friend was shopping for round-nosed pliers for jewellery and some of those specialist stores charge high prices for mediocre tools.. I told her I would find her engineering round-nosed pliers instead since they will be better made!

    Incidentally, ESD cutters or pliers need to be hidden away from general DIY users.. they borrow them, and wonder why there is a tingle or worse, when they inevitably use them on live wiring!

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>