Test & Tools
  • Technologies
  • More
Test & Tools
Blog Pomona Insulation Piercing Clips
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 28 Jul 2019 11:32 PM Date Created
  • Views 3964 views
  • Likes 12 likes
  • Comments 16 comments
  • piercing_clip_connector
  • insulation piercing
  • banana plug
  • wire_piercing
  • pomona
Related
Recommended

Pomona Insulation Piercing Clips

shabaz
shabaz
28 Jul 2019

A friend gave me a couple of Pomona Insulation Piercing ClipsPomona Insulation Piercing Clips which I thought were pretty neat. Apparently they are quite popular with the automotive repair/test crowd.

The clips were something I had not seen before, so thought maybe it would be good to share some pics/video if anyone else has not seen these before either.

 

In brief, they can connect to banana plugs (there is also a version of clip compatible with multimeter test leadsversion of clip compatible with multimeter test leads) and then the other end can be hooked over an insulated wire, and by turning the red or black end of the clip, a sharp needle pierces the insulation for making contact with the conductor.

 

The damage is fairly minimal, and the repair depends of course on the industry/application and environment. It may need a small insulation repair, since the insulation it is compromised.

 

image

 

Here's a close-up showing the insulation being pierced:

image

They feel well-made, and I like the ergonomics too. The pointy nose is nice too for pushing into a nest of wires. I get the feeling it would be very easy to use this one-handed, by using the thumb and index finger to push back on the lever, while pushing into the wires, and hooking it on. After that, the lever can be released and then the black or red end of the clip needs screwing in (possible one-handed, but depends on if it will disturb the wire or not - you may want to do that part two-handed).

 

Here's a 7-minute video showing me using it with a few wires (the clip is designed for 14-22AWG wires, but it seems fine with thinner wires too).

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

There are versions for long-distance probing/poking image (up to 24 inch!):

image

Thanks for reading!

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 7 years ago in reply to jw0752 +7
    Aliexpress to the rescue ! https://www.aliexpress.com/wholesale?catId=0&initiative_id=AS_20190729000340&SearchText=insulation+piercing+test+clip MK
  • jw0752
    jw0752 over 7 years ago +6
    Hi Shabaz, They looked really useful until I saw the price. I think my application will need to be a bit more profitable before I invest. John
  • shabaz
    shabaz over 7 years ago in reply to jw0752 +6
    Hi John! Most Pomona stuff is pricey here, but this one looks expensive universally. I just noticed Fluke have the identical product on their price-book too, at an even more unmentionable price!
Parents
  • luislabmo
    luislabmo over 7 years ago

    This reminds me many years ago I saw an Electrician doing some measurements on the main voltage lines at home by poking them with Sewing pins. Maybe situations like these inspired such a useful tool.

    Luisimage

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to luislabmo

    It seems that this ancestor method was cheaper than ever ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to luislabmo

    It seems that this ancestor method was cheaper than ever ...