Test & Tools
  • Technologies
  • More
Test & Tools
Blog Programmable Electronic Load - Current Sense Circuit
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 16 May 2020 10:29 AM Date Created
  • Views 7759 views
  • Likes 9 likes
  • Comments 32 comments
  • shunt circuit
  • programmable electronic load
  • electronic load
  • programmable
Related
Recommended

Programmable Electronic Load - Current Sense Circuit

Jan Cumps
Jan Cumps
16 May 2020

Detailed review of the current shunt circuit of the Programmable Electronic Load.

image

The circuit and measurements are discussed here.

 

Circuit

 

The current measurement circuit reads the voltage over a 50 mΩ shunt resistor that's in series with the load circuit.

 

image

That voltage (always negative, because the resistor is "below" the circuit's analog ground) is amplified by a non-inverting OpAmp circuit, with gain 7.8.

 

Test Setup

 

A DMM measures the voltage of the shunt and the output of the OpAmp. Both relative to that analog ground.

image

The measurement is automated.

At every iteration, the shunt voltage and the output of the OpAmp are logged.

A relay switches the DMM probe between the two measurement points.

image

Automated flow detail: switch DMM probe, then take a sample.

 

I've also added a gain calculation.

imageimage

Gain is calculated as the ratio between output and input. Then logged.

 

Measurement Results

 

All data is written to the attached spreadsheet.

The extract below shows 101 measurements.

The DAC that controls the eLoad is set to 0.

A first measurement of current (I take that from the PSU), shunt and OpAmp output voltage are written.

Then, the DAC is 100 times increased, each time with 100. ANd the measurements are repeated.

The attached version (9.xlsx) has more measurements (All eLoad ADCs, and some more stats from the PSU).

 

image

101 samples. PSU = 5 V, DAC initial = 0, steps 100, step 100

 

 

Here's a graph of the output vs input. The line represents the gain.

image

And a graph of the OpAmps gain, with as axis the shunt voltage.

image

Attachments:
eload_dp832a_shunt_circuit_characterisation_9.xlsxeload_dp832a_shunt_circuit_characterisation_9.xlsx
eload_dp832a_shunt_circuit_characterisation_18.zip
eload_dp832a_shunt_circuit_characterisation_19.zip
eload_dp832a_dmm6500_current_2 - workingcopy.zip
  • Sign in to reply

Top Comments

  • Andrew J
    Andrew J over 6 years ago +3
    Interesting. Is this using your compensation approach for the DAC? I presume that the current is being logged by Labview from the Rigol PSU rather than being measured? I think you can do a lot with this…
  • jc2048
    jc2048 over 6 years ago +3
    This is your gain curve but with the vertical axis scaled so we can see what it's doing in more detail. With the exception of a few very odd measurements [settling time? noise?] it has a clearly defined…
  • Jan Cumps
    Jan Cumps over 6 years ago +3
    I've placed the resistor R32 back: As you can see, the board has gone through heavy storms by now. Input: (chart Y axis in µV) Output: (chart Y axis in mV) For those who get stress when seeing a bouncy…
Parents
  • jc2048
    jc2048 over 6 years ago

    This is your gain curve but with the vertical axis scaled so we can see what it's doing in more detail.

     

    image

     

    With the exception of a few very odd measurements [settling time? noise?] it has a clearly defined shape. At higher values, it's clearly asymptotic to a gain of somewhere just below 7.6.

     

    The reason for the shape is that the amplifier has a small voltage offset. At low values, the offset plays a large part in affecting the gain calculation, at high values, much less so.

     

    Here is a plot of incremental gain values. This is generated by taking successive pairs of readings and working out the slope of the curve between the pair. Ignoring the odd measurements, the gain is something like 7.53 or 7.54.

     

    image

     

    That lets us see the gain without the offset getting in the way. The op amp looks like it is doing what it should with the gain. It can't take into account the offset because it doesn't know anything about it.

     

    If you were to remove the offset before doing your absolute gain calculation, then your absolute gain curve would flatten until it was horizontally level.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to jc2048

    jc2048  wrote:

     

    ....

     

    With the exception of a few very odd measurements [settling time? noise?] it has a clearly defined shape. ...

    It's noise.

    I used a delay after setting the dac, and a delay each time I switched between shunt voltage and OpAmp output voltage. So settling should be covered.

    imageimage

     

    I tried to avoid as much as possible by using noise mitigating options of my meter (average filter with 10 measurement averages, measuring during the 10 power line cycles).

    image

     

    Still, I used patch wires and soldered in wires to get at measure points, so noise is expected.

     

    If you were to remove the offset before doing your absolute gain calculation, then your absolute gain curve would flatten until it was horizontally level.

    I will try to do that - first get an idea of that offset.

    I also removed that R32 680K resistor we discussed before - to go back as close as possible to the original design :

     

    image

    I can put it back and see if the offset disappears. The resistor R32 would drop the gain from 7.8 to 6.8 - not a disaster.

    Or when needed -  try and offset the offset...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to jc2048

    jc2048  wrote:

     

    ....

     

    With the exception of a few very odd measurements [settling time? noise?] it has a clearly defined shape. ...

    It's noise.

    I used a delay after setting the dac, and a delay each time I switched between shunt voltage and OpAmp output voltage. So settling should be covered.

    imageimage

     

    I tried to avoid as much as possible by using noise mitigating options of my meter (average filter with 10 measurement averages, measuring during the 10 power line cycles).

    image

     

    Still, I used patch wires and soldered in wires to get at measure points, so noise is expected.

     

    If you were to remove the offset before doing your absolute gain calculation, then your absolute gain curve would flatten until it was horizontally level.

    I will try to do that - first get an idea of that offset.

    I also removed that R32 680K resistor we discussed before - to go back as close as possible to the original design :

     

    image

    I can put it back and see if the offset disappears. The resistor R32 would drop the gain from 7.8 to 6.8 - not a disaster.

    Or when needed -  try and offset the offset...