Test & Tools
  • Technologies
  • More
Test & Tools
Blog Quickly Solve Simultaneous Equations up to several variables using just a calculator (or Excel).
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kkazem
  • Date Created: 14 Dec 2021 5:43 AM Date Created
  • Views 4351 views
  • Likes 7 likes
  • Comments 5 comments
  • Design
Related
Recommended

Quickly Solve Simultaneous Equations up to several variables using just a calculator (or Excel).

kkazem
kkazem
14 Dec 2021

Often times, it's necessary to solve simultaneous equations and this can be for optimizing a voltage divider using two outer resistors and a center adjustment pot, or or countless other purposes in electronics, physics, and science. Using just a scientific calculator or a spreadsheet, it's quite easy and fast to solve a 3, 4, 5, variable or even more, simultaneous equations. Few of us would want to do this by hand as we were taught in  engineering school. Personally, I use an HP48 or 49 Scientific Calculator to solve these, but there are many brands of scientific calculators that have a Matrix Calculation capability. Specifically, the calculator needs to perform an inverse matrix multiplication, which is effectively a matrix division. I'll give an example here. 

EXAMPLE: SOLUTION TO 3-VARIABLE, SIMULTENEOUS EQUATIONS:

Here's an example set of 3 equations in 3 unknowns. For the solution to work, there needs to be at least one equation for each independent variable. 

  5*X +    9*Y + 14*Z = 31

12*X +   2*Y  -   4*Z =    8

  3*X + 16*Y  + 21*Z = 19

We first put this in standard form as follows:

|  5      9   14  |      | X |       | 31 |

| 12     2    -4  |      | Y |  =   |  8  |

|  3   16    19 |      | Z |        | 19 |

I apologize for how bad the matrix form looks above, but there are no drawing tools I could use to make a proper left and right matrix bracket, so the best I could do was to use the vertical line character.

To solve this, we simply put it into the calculator with the right-side of the equal sign first, followed by the larger matrix, then divide. When I say divide, this isn't strictly correct as there is no true division in matrix operations. It's actually doing a matrix inverse on the large matrix, then taking the smaller, 3 number column vector by the matrix using a right, matrix multiplication. On the HP48 calculator, it get's entered as follows using the matrix editor:

| 31 |

|   8 |

| 19 |

/

|    5    9  14 |

|  12   2    -4 |

|   3   16  19 |

with the result being a 3 number column matrix with the answers to the variables X, Y, and Z. Here is the result from the HP48 calculator as follows:

X = 2.48428

Y = -3.6101

Z = 3.64779

If you plug these values for X, Y, and Z back into any of the original equations, you'll find that they satisfy the equations.

  • Sign in to reply
Parents
  • javagoza
    javagoza over 4 years ago

    This is one of the absurd and stupid reasons why programmable calculators and / or with matrix functions are not allowed in Spain in college entrance exams.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsjawale24
    rsjawale24 over 4 years ago in reply to javagoza

    Not just Spain, even in Indian colleges up to 12th standard and entrance exams calculators or any kind are not allowed. However, once you enter engineering college, you are allowed to use only a non-programmable scientific calculator.  The Casio FX991-ES is the most popular calculator among Indian engineers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rsjawale24
    rsjawale24 over 4 years ago in reply to javagoza

    Not just Spain, even in Indian colleges up to 12th standard and entrance exams calculators or any kind are not allowed. However, once you enter engineering college, you are allowed to use only a non-programmable scientific calculator.  The Casio FX991-ES is the most popular calculator among Indian engineers.