Test & Tools
  • Technologies
  • More
Test & Tools
Blog Researchers Design Solar-Powered MOF-based device to Produce Water from Air
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 26 Apr 2017 9:39 PM Date Created
  • Views 1480 views
  • Likes 3 likes
  • Comments 5 comments
  • mit
  • hmi
  • water
  • on_campus
  • water filter
  • cabeatwell
  • university
  • human life
  • solar
Related
Recommended

Researchers Design Solar-Powered MOF-based device to Produce Water from Air

Catwell
Catwell
26 Apr 2017

image

MIT/Berkeley’s water-harvesting device uses porous metal-organic frameworks and sunlight to transform air into water at a rate of about 3-liters a day. (Image credit MIT)

 

It’s all in the MOFs- transforming air into water isn’t some kind of alchemic wizardry, nor is it done with tech from the future but rather it’s an ingenious solution using compounds of metal clusters and organic ligands. Yep, that’s the wonders of chemistry or rather the magic of “metal-organic frameworks” (MOFs), which researchers from MIT and Berkeley harnessed to develop a device that transforms air into water.

 

The technology would be a great solution for those living in arid or desert climates where water is scarce or nonexistent, or perhaps as a survival aid in situations where potted water is unavailable. Whatever the case may be, the device doesn’t require a power source or the inclusion of a freezer to harvest water but only needs air and sunlight, something most arid climates have in abundance.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Let me break it down for you regarding the mechanics of how it works- housed inside of an acrylic box is the metal-organic framework material, which is porous like a sponge and has hydrophilic, water attracting properties. The top of the box is painted black and heats the air inside at the top of the box while the air at the bottom retains the same temperature as the outside area around it. The air trapped in the MOF is released as a vapor due to the temperature differential and transformed into water as it cools and collects at the bottom of the cube, in much the same fashion as modern CPU heatsinks work.

 

Tests have shown that just over two pounds of the material could produce as much as three liters of water every twelve hours in a climate with 20% humidity or enough for one person to live on per day. All that’s needed is for users to simply open the box, collect the water and let fresh air in- wash, rinse, repeat. Live in a climate with more or less humidity? No problem, the MOFs can be ‘tuned’ to function with the relative humidity by combining different metals with different compounds to achieve optimal results.

 

“By carefully designing this material, we can have surface properties that can absorb water very efficiently at 50 percent humidity, but with a different design, it can work at 30 percent,” stated MIT grad student Hyunho Kim who is part of the development team behind the device. He goes on to say, “By selecting the right materials, we can make it suitable for different conditions. Eventually, we can harvest water from the entire spectrum.”

 

Of course, the researchers are still working to refine their MOF design as it currently can only collect about 25% of its own weight in water but they hope to up that percentage by 50% for arid climates in the near future.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

 

  • Sign in to reply
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    The "Water Seer" came to mind the minute I saw this too, the amount of energy required to cool water in gas form down enough to transition it through to liquid form is immense,  Just look at how long it can take a DE-Humidifier to extract a couple of liters from a room, and this is powered and also forcing air over a condenser

     

    Thermal energy will pass from the hot to the cold side, you're also not cooling the cold side where the water is to condense, you need to create the scenario where the differential is enough to cross the dew point

     

    This definitely smells the same as "Water Seer", the science will not add up. Can it get water from the Air, quite probably but 3 liters a day every day, and when there is only 20% humidity to begin with, that's a whole other story.

     

    and how is the "Hot" air created by the black side going to travel Down hill to get to the colder side of the device? the black would need to be up top in order to get the sun, also by heating up the air, you will change its relative humidity (That's why its relative) and then when it is cooled again, it will go back to where it was

     

    The Magic dust would have to be pretty special to overcome the conservation of energy laws!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to Catwell

    So it's hard to see what is being offered here - condensing water out of air with some kind of cooling system is nothing new.

    When universities put out video interviews claiming some whizzy world saving technology but kind of short on detail and hard facts it should trigger your hype detectors.

    This looks like a typical Uni bid for attention - either career enhancement or grant money.

     

    It's probably the same as the Waterseer - same idea but different tech dressing (man in white coat talking about funny molecules)  - you'll know if its real when you see one outside and working.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 9 years ago in reply to michaelkellett

    Michael,

     

    Heat transfer for sure. The top of the box heats up, while the bottom has to be the environment temp. I assume it is for maintaining the ambient temp at the bottom.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    The science is good, we just need to see if the technology scales and supports a cost effective implementation.

     

    The approach is similar to a wind trap idea, where you move air with moisture through a structure where there is an enhanced environment for water droplet formation.

     

    If you set the device up next to a good source of evaporating sea water, you could greatly improve its collection capability.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago

    There's some sort of con going on here - what are the unexplained thick wires and heatpipes doing ?

     

    These are not mentioned in the video or in your explanation.

     

    MK