Test & Tools
  • Technologies
  • More
Test & Tools
Blog Review of Keithley 182-M sensitive voltmeter (nanovoltmeter)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tin_xdevs
  • Date Created: 24 Sep 2015 4:11 AM Date Created
  • Views 7011 views
  • Likes 5 likes
  • Comments 14 comments
  • precision
  • test
  • reference
  • voltage
  • nanovoltmeter
  • review
  • keithley
  • smu
  • engineering
  • teardown
  • calibration
Related
Recommended

Review of Keithley 182-M sensitive voltmeter (nanovoltmeter)

tin_xdevs
tin_xdevs
24 Sep 2015

Intro

 

One of main Keithley Instruments expertise are low-level signal measurements. Since very beginning company had instruments as null-detectors, microvolt voltmeters, electrometers. As of today, current nanovoltmeter is Model 2182A, which features two channels with range down to 100mV with 7½ resolution. Predecessor of this instrument was sensitive voltmeter Model 182, which we will look on today.

 

It’s possible to get one of these from secondary market for about $1K USD or lower. I had chance to get recently calibrated Model 182-M version from one of EEVBlog forums member, and we will take a close look on it's internal construction and details. It was also owned and calibrated by EEVBlog member acbern. Always interesting to follow used test gear life and travel across different owners.

 

This is specialty instrument, not a replacement of usual multimeter, such as Model 2000 or 2001 by any means. The only function is DC voltage measurement, but it does this function much better than conventional multimeter. No resistance, current or AC measurements present, so if you need any of that, there are variety of Keithley’s special meters/sources.

Other Keithley instruments dedicated to low voltage measurements are modern Model 2182/2182A and obsolete Model 1801 preamp module for Model 2001/2002 series DMMs.

Measurement capability

 

Here’s summary from spec for provided ranges and accuracy on Model 182.

 

RangeResolutionAccuracy 24 hoursAccuracy 1 yearTransfer stability 5min
3 mVDC   1 nV20 + 16 ppm with REL60+16 ppm with REL5+9 ppm with REL 
30 mVDC   10 nV20 +  6 ppm with REL60+6 ppm with REL3+2 ppm with REL 
300 mVDC   100 nV15 +  6 ppm with REL55+6 ppm with REL3+2 ppm with REL 
3 VDC   1 µV10 +  4 ppm with REL50+6 ppm with REL3+2 ppm with REL 
30 VDC   10 µV10 +  4 ppm with REL50+6 ppm with REL3+2 ppm with REL 

 

These specs pretty impressive, if you consider age of design (90's). Our meter, as visible from datecode marks on various IC was manufactured in 1992. Old, but not obsolete!

Maximum input voltage is 120VDC for 10 seconds, or 35VDC continuous, so do not try to measure high-voltage circuits with nanovoltmeters.

Specified noise can be as low as 15nV peak-peak with source resistanceDMMs, which is not available anymore, can offer lower noise and higher sensitivity.

Input impedance is at least 10 GΩ, with bias current.

 

There is analog output function for external datalogging device, with 0.15% accuracy and digitally adjustable gain, so Model 182 can act as an voltage amplifier with some limitations.

Meter have auto ranging function, and can read ±3029999 counts.

Manuals

 

It’s worth to take a look on official manuals and specs.

 

Keithley Model 182 Quick Start manual, 182-903-01, Revision B
Keithley Model 182, 182-901-01 Revision E, June 1993 Instruction manual
Keithley Model 182, 182-901-01 Revision A, October 1990, Operations manual
Keithley Model 182 Specification, Revision B
Keithley Model 182LS Specification, Revision A – Model 182LS does not have functional analog filter

Exterior

 

image

 

Meter is somewhat mix of old-style Keithley gear with square tactile buttons, and newer style with nice dot-matrix dual-line VFD screen and half-rack chassis form factor. While VFD screen looks like one used in Model 2001/2002/24xx/26xx series instruments, it’s not the same one. Perhaps Model 182 was first instrument to try this type of displays, before it was widely implemented for newer devices.

 

image

 

Rear panel have mains power input, line voltage switch, fuse holder, GPIB IEEE-488 port, and three BNC ports for analog output, external trigger input and meter complete output. There are no fans, vent holes or any external heatsinks in Model 182. One of reasons for this is to completely isolate internal boards from any possibility of airflow. This is part of design to avoid thermal EMF generation on low-voltage signal path.

Our meter is very clean and in almost perfect condition, screen is bright. Always happy to see well cared instruments.

 

image

 

Menu system is simple and intuitive to use.

 

image image

Interior & teardown

 

I will not go to full disassembly on this meter, as it’s still recently calibrated and I would like to keep it in spec. Even minor contamination of such sensitive analog circuitry parts can easily spoil calibration, so extra care with handling is required.

 

image

 

Model 182-M have extra 9V battery to power part of input front-end amplifier, so input impedance kept >10GΩ even if main voltmeter power switched off. Regular Model 182 does not have this part.

 

image image


ADC is based on charge-balance multi-slope integration operation principle, similar to one used in most of 6½-digit and more bench DMMs. Manual have simplified ADC diagram, as below:

Digital board

 

image image

 

Main process is widely used Motorola MC68HC000FN10 in PLCC package, paired with Hitachi HM62256ALFP-10T SRAMs, forming totally 64KB of RAM. PLCC package U506 nearby is dual UART from EXAR, XR68C681CJ.

Analog Devices AD7840JP is analog output 14-bit DAC, with internal 3V buried zener reference. Reference temperature coeffient is ±60 ppm/K. Reference output is routed externally to DAC’s input, so it should not be too difficult to add external reference for this function, if better stability is required. Perhaps a future mod? image

Analog Devices AD707JR nearby is ultralow drift output amplifier for DAC.

 

Digital board is powered from LM2940CT-5.0V LDO U514. There is also onboard DC-AC module for AC filament and +60VDC voltage generation. It’s exactly same as in other Keithley instruments with dual-line VFD.
System clock is supplied from 20MHz oscillator Y500.

Power supply

 

image

 

Main power supply is rather interesting and using dual transformer approach. Mains transformer converts line voltage to low AC voltage for second transformer and also supply +7V to digital regulator.

 

Secondary transformer helps to prevent mains coupled noise from coming into analog circuits. This second transformer used to generate +15,-15,+5 and +40, -40 voltages. It also provide +15V power for LM399 ovenized reference.

Similar approached was adopted in modern instruments as well, such as Fluke 8508A and Keithley DMM7510.

Analog board

 

image

 

Whole analog circuit section is covered by aluminum shield to further isolate EMI, airflow and protect sensitive parts.

 

image image


ADC controller is based on Motorola MCU MC68HC11F1N with its own ROM 182-802-B03. This 8-bit MCU have internal 1KB RAM, 8-channel 8-bit ADC and runs at 7.68MHz.

 

image

 

But it’s the front-end, where all the real analog magic happens..

 

The very front end section is even further covered by separate plastic cover. It a good example of system engineering required to implement highly sensitive analog circuits to get reliable performance and stability.

 

image image

 

1% 500 Ω resistor sitting at the input terminal have copper leads and crimped to copper PCB connectors to avoid thermal EMF development. Input nets are further guarded by unmasked tracks on PCB.
Small modular PCB is a separately powered front-end, so meter’s input impedance stays >10 GΩ even with mains power removed. This is special part of Model 182-M version only.

We can also spot some wirewound resistors, likely used to adjust gain for range switching. Most of opamps are Burr-Brown OPA602, but there is also LT1007 used as preamp

Voltage reference is selected LM399 ovenized 6.95V zener, similar to one used in Keithley Model 2000/2001 units.

 

image

 

There are few Vishay foil resistors as well, perhaps setting zener current.

image image

 

Input port wire is pass thru filter ferrite to reduce RFI and noise a little, and crimped right down to PCB.

 

image image

Firmware dumps

 

image image

 

Keithley 182-M firmware A04, 27C512 ROM 182-800-A04 dump
Keithley 182-M firmware A04, 27C512 ROM 182-801-A04 dump

Keithley 182-M ADC firmware dump, 27C256 ROM 182-802-B03

 

Also captured calibration ROM from U522 X24C16S SO16 EEPROM. To do so hold CPU reset low, power on meter and read I2C chip with external programmer. I shorted CPU’s pin 20 to GND and hooked MiniPro TL866 programmer to perform this task.

 

Calibration EEPROM dump from I2C ROM

Calibration info

 

My meter come with this calibration data:

Date : 04/06/2015
Temperature : 20.3 ±2C
Used source : Datron 4808 AB038, calibration Sept 2014

Signal level182-M ReadingDeltaMaxDeltaDeviationStatus
0.19 VDC0.18999919.0E-070.0000118.2PASS
1.9  VDC1.8999742.6E-050.00011223.2PASS
19.00 VDC18.999584.2E-040.0011536.5PASS
-0.19 VDC-0.1899981-1.9E-060.000011-17.3PASS
-1.9  VDC-1.899965-3.5E-050.000112-31.3PASS
-19   VDC-18.99943-5.7E-040.00115-49.6PASS
19  mVDC0.0189999732.7E-080.000001162.3PASS
1.9 mVDC0.0018999712.9E-080.00000014120.6PASS
-19  mVDC-0.018999959-4.1E-080.00000116-3.5PASS
-1.9 mVDC-0.001899938-6.2E-080.000000141-44.0PASS

 

It’s unclear to me why calibration was done at 20C, instead of standard 23C, like meter’s specification and manual.

Calibration for Model 182 for 3mV and 30mV ranges is internal ratiometric, and for higher ranges direct. Calibration source must be able to provide 300mV, 3V and 30V signals.

Calibration constants can be also read by sending GPIB command U11X.

 

Output on my meter is as below

 CAL+4.826974E-01,+4.826965E-01,-1.136970E-07,+4.852434E-01,+4.852453E-01,-9.680330E-08,+4.811439E-01,+4.811463E-01,-3.695733E-07,+4.801486E-01,+4.801503E-01,-3.498665E-06,+4.364472E-01,+4.364473E-01,-7.152183E-04,+1.009753E+00,+3.296010E+00,+4.000000E+00

image

Python application to gather data from Keithley Model 182-M

 

Model 182 does not use SCPI language common in more recent instruments, and rely on abbreviated commands instead.

 

Command reference shown below in table

 

Command

Function
B05½-digit resolutionB23½-digit resolution
B16½-digit resolutionB34½-digit resolution
D0Filter damping offD1Filter damping on
N0Filters offN1Filters on
O0Analog Filter offO1Analog Filter on
R0Enable AutorangeR13mV range
R230mV rangeR3300mV range
R43V rangeR530V range
R6N/AR7N/A
R8Disable Autorange
S0Line-cycle integration rateS1Medium integration rate
S2Fast integration rateX Execute other commands
Z0Reading relative offZ1Reading relative on
Z2,valueUse value for relativeZ3Use previous value

 

To execute command, follow “Command”+X syntax. For example R4X will set meter to 3V measurement range
Meter returns reading strings, with typical format : NDCV+1.234567E+00
It’s also possible to program multiple commands at once, for example B1R1S0X will set 6½-digit resolution, 3mV range and line-cycle integration rate.

# xDevs.com Python test GPIB app for Keithley 182M
# http://xdevs.com/review/k182m/
import sys
import Gpib
import time

with open('3mv.csv', 'wb') as o:

    inst = Gpib.Gpib(0,1) # Instrument GPIB Address = 17
    inst.clear()
    o.write("k182;\r\n")
    min = 0
    inst.write("Y2B1F0D1P3Q1000O1N0R1S2W0X")
    inst.write("Y2B1F0D1P3Q1000O1N1R1S2W0X")
    while min <= 1000:
        min+=1
        inst.write("X")
        data = inst.read()
        val = data.split('NDCV')
        time.sleep(1)
        print("%s" % val[1])
        o.write(";%s" % val[1])
        if (min == 1000):
            min = 0

 

This program collects data every sample with meter configuration at 3mV range, analog filter on, digital filter slow, with trigger delay 1s.

Performance verification

 

For this task I’ll use EDC MV106 DC Voltage standard, which have 100mV, 1V and 10V ranges, and we compare readings with long-scale DMM.

Overall setup photo:

 

image

 

EDC MV106 DC voltage standard box on top right, to supply various VDC levels.  
Keithley Model 2002 8½-digit DMM for comparison
Keithley Model 2400 SMU

 

Test with zero and 3mV from SMU

 

image image

 

1mV sourced from SMU and EDC MV106:

 

image image

Input port and connections

 

As most of nanovoltmeters, this meter using special type connector, Amphenol Industrial 97 series 97-3102A-16-11 (4-129). Mating male cable connetor is available on Digikey for no less than $40 USD.

In task of measuring microvolts it’s very important to make proper connection to DUT. The most common sources of error in low voltage measurements are thermoelectric voltages (thermoelectric EMFs) generated by temperature differences between  junctions  of different metal conductors. This includes PCB traces (copper-tin), wiring, connectors, and test component leads. There is good example of thermal EMF impact shown in this Fluke application note from Martin L. Kidd

I made custom triax cable using medical grade CNMC low-noise triax wire.

image

Test with DC voltage standard

 

2VDC and 3mVDC from MV106

 

image image

 

Rest of testing would be covered more in detail in Part 2 of review

 

Analog output function

 

One of special features of Keithley nanovoltmeters is gain-adjustable analog output.
Model 182’s analog output voltage is generated by 14-bit DAC from digital code, supplied from main processor.
Gain and relative function for this output value can be adjusted from front-panel or remotely, allowing to fit wide usage scenarios.

With gain = 1.000000, full-range will provide 3VDC output signal. This means if meter using 30mV range, 30mV signal will result having 3VDC on analog output port. If gain results in higher voltage, maximum output voltage would be ±3.3VDC.
Gain range : 0.001 to 999999.999 with 0.001 resolution.

Maximum output current is 5mA, so loading source should be no less than 1kΩ. Output voltage is in range 0 to ±3VDC.

 

Conclusion

 

This specialty instrument is not an everyday use tool, but for low-level measurement tasks it can do what conventional long-scale DMM can’t.

If you have any comments or experiments to see with this kind of gear, please let us know in comments.

I also have published this review on my site, just like with other gear reviews, this helps me to keep all stuff in one place.

  • Sign in to reply

Top Comments

  • tin_xdevs
    tin_xdevs over 11 years ago in reply to e14 Contributor +1
    I have 2002 on my table. That is NOT a RS232, that's is TTL Digital I/O. You can check the manual for details. Only communication port on Keithley 2001/2002 available is GPIB IEEE-488.
Parents
  • DAB
    DAB over 11 years ago

    Great post.

     

    It is amazing how many useful design practices you can learn by looking inside a good quality instrument like this one.

     

    Took me back to my laboratory days working with precision instruments taking detailed measurements during experiments.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    Great post.

     

    It is amazing how many useful design practices you can learn by looking inside a good quality instrument like this one.

     

    Took me back to my laboratory days working with precision instruments taking detailed measurements during experiments.

     

    DAB