Test & Tools
  • Technologies
  • More
Test & Tools
Blog Scientists can now Track Space Debris 24-Hours a Day
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 10 Aug 2020 6:26 PM Date Created
  • Views 1261 views
  • Likes 4 likes
  • Comments 3 comments
  • nasa
  • space garbage
  • space
  • orbital debris
  • cabeatwell
  • tof
  • time of flight
  • innovation
Related
Recommended

Scientists can now Track Space Debris 24-Hours a Day

Catwell
Catwell
10 Aug 2020

image

The new method of tracking space junk involves using high-powered lasers that detect diffused reflections bouncing back from the debris orbiting up to 36,000 kilometers away. (Image credit: NASA)

 

There’s a good chance that no matter where you are on the planet, there will be a piece of garbage nearby. On the top of Mount Everest, deserted islands, the North and South Poles, even in the most desolate of places, there is always a piece of refuse not far away. The same is true in space, in both low and high orbits, only debris traveling at 27,000 mph around the planet can be deadly and costly. Scientists have been tracking portions of floating garbage for decades, which range in size from small screws to discarded rocket stages.

 

Lasers have been deployed on the ground to track objects in space, but ranging the debris was only possible for a few short hours during twilight, as the sunlight made it virtually impossible. Now, scientists from the Austrian Academy of Sciences Space Research Institute have developed a new technique of detection that can be used during daytime hours, significantly expanding the amount of time floating junk can be tracked. It may even pave the way for visualizing and mapping the debris in each orbital range.

 

The scientists developed the new technique by calibrating their telescopes using two stars with different levels of brightness, which allowed them to increase the visibility of debris in orbit. Once the calibrations were complete, they then started tracking objects beginning above 150 in incremental elevations, adjusting for the amount of light as they went. They then used a computer program to detect illuminated objects from different light sources, which also takes into account daylight interference.

 

The scientists had to continuously apply corrections to the images, based on the target’s predicted flight paths and TOF (Time of Flight). Using the software, they needed to apply time biases repeatedly, center their SLR (Satellite Laser Ranging) telescopes, and shift the detection time. The new technique produced four successful trials, with each tracking a piece of old Soviet-era rockets between March and October of last year. The new detection method could also provide additional information about targets, including their rotational behavior, direction, and period.    

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • colporteur
    colporteur over 6 years ago +1
    I recall reading an article on the size of new satellites and the difficulty of tracking them. It seems the string of satellites constellation they were putting in orbit would consist of small suit case…
  • Catwell
    Catwell over 6 years ago in reply to dubbie +1
    We need some sort garbage truck up there.
  • Catwell
    Catwell over 6 years ago in reply to dubbie

    We need some sort garbage truck up there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago

    I find the concept of being able to do more with essentially the same technology, but with a dash of clever thinking, very inspiring. It encourages us all to consider being able to take our existing systems and with some clever thinking and tinkering, make it better. Maybe I should patent that - Thinking and Tinkering (Tat), or the modern version, iTaT and eTaT.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 6 years ago

    I recall reading an article on the size of new satellites and the difficulty of tracking them. It seems the string of satellites constellation they were putting in orbit would consist of small suit case vehicles. Current technology was finding it difficult to track them in their orbit. That is not a problem in the vastness of space, right?

     

    A few objects floating around in the expanse of space won't be an issue. Space junk, especially space junk that has disintegrate and become very small space debris, are like bugs floating across the open highway. If one of them hits the car you get a splat. If one of them hits a motorcycle rider, without leathers, who has opened up the bike throttle to sail down the highway with speed, there is a strong possibility there is a ditch is in their future.

     

    Space walks not only involve the harshness of space but also the detritus explorers have left behind, that is now floating around waiting to smack the astronaut up the side of the head like a bullet shot from a gun.

     

    There is a joke "What is the last thing that passes a flies mind when his head hits the windshield of a car? His butt! Think of walking in space  "Ouch what the hell was that?", as the suit decompresses and the body contained within boils.

     

    Thanks CA for the article great share!