Test & Tools
  • Technologies
  • More
Test & Tools
Blog Troubleshoot my Electronic Load - part 1: MOSFET and Voltage Reference
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 2 Jul 2019 7:56 PM Date Created
  • Views 2660 views
  • Likes 8 likes
  • Comments 10 comments
  • msp432
  • eload
  • scpi
  • electronic load
Related
Recommended

Troubleshoot my Electronic Load - part 1: MOSFET and Voltage Reference

Jan Cumps
Jan Cumps
2 Jul 2019

My electronic load failed. I was trying new hardware and software options. At a certain moment the power MOSFET died.

There was no magic smoke, but the source, drain and gate are all shorted (source, drain and gate all measure a few Ohms in both directions).

I am not 100% sure of what has happened, but I think that a bad contact at the gate or current sense resistor, while the FET was supplied with 40 V, did it. No sound, no smell. Just an instantaneous death.

image

In this post, I'm checking what's been damaged and - hopefully - how to fix it.

Depending on what's defect, this may become an interesting or boring blog. That's how it goes with repairs.

(also a shoutout to dougw: this may fit into an e14 repair group)

 

 

Known Defects

 

The power MOSFET is definitely destroyed. The three pins all measure close to short - while they should be very high resistance.

The fact that the drain is almost shortcut to the gate is a worry. High power may have been injected into the control circuit. Let's see...

My process is to first fix the known defect components, then slowly test all other components starting from the source on.

(Sometimes - in particular with low power defects and circuits where most of the functionality is working) I do the opposite. Start from the output and trace back to where the signal is intact.

In this case, I risk blowing the whole thing again when the control circuit is unstable. So I start from the beginning, with the power part disconnected.

 

Replace the Power Mosfet

 

The FET is known to be bad, so I have to replace it.

The package is soldered on a big copper fill. With vias, it's connected to an even bigger copper plane on the back side. That plane has the size of the heat sink that's mounted on the backside of the PCB.

image

To remove the device (the picture above shows the new MOSFET that I placed during the repair exercise) you have to get the whole copper plane area above the melting temperature of (in my case lead-free) solder.

To do that, I first removed the heat sink (and the fan that's mounted on it).

Then I placed the board above a pre-heater for a good 10 minutes. I drowned the FET in flux.

I then removed the solder from the two pads using a 400° C heated solder iron and desoldering braid.

I turned my hot air gun to 500° C (for fast rework without hindsight) and removed the FET.

Then I cleaned up the pads with the iron and the braid. I cleaned the pads afterwards with isopropanol - to remove flux and burn residue.

 

After that I re-tinned the big copper pour - just enough to have solder plating on it. (I am using non-leaded solder).

I also tinned one of the two FET pins (the right one).

Then, I placed the FET and soldered it in place by heating that right pad.

Next, I properly soldered the left pad and reworked the right one too - to have decent quality joints on both.

I re-applied a royal amount of flux, applied solder with a 400° C iron around the FET and over the edge of the metal back plate, then heated the big pour on the front side with 500° C hot air until the solder became liquid and seeped around and under the FET.

I let the whole area cool down to the pre-heat temperature, and turned the board around.

Then I bombarded the back copper poor (where the heat sink should fit snugly) with 500° until all solder residue had flown through the vias to the other side of the board - ensuring a good thermal bridge from FET to heat sink.

 

When the back plane was level (no solder bumps left) I let the whole module down.

I re-applied thermal paste and put the heat sink with ventilator back in place.

 

ADC Board Part 1: Voltage Reference

 

Because the resistance between gate and the two other FET pins were shot, anything could have happened to the upstream circuit.

I have to check the DACs, ADCs, voltage reference IC and input activation switch (and some other silicon -  I don't believe anything passive has suffered).

 

The results of monitoring the reference can be seen below.

I have powered the IC from the LaunchPad that controls the load.

In normal circumstances, it's powered from the load's control board, but I haven't tested that yet.

image

image: capture of the voltage reference. It has been behaving good for two hours (between 2.64230 and 2.64130 V - good enough for Belgium)

 

In the next post, I'll test the remaining parts of the ADC/DAC board.

 

Related Blog
Programmable Electronic Load
Troubleshoot my Electronic Load - part 1: MOSFET and Voltage Reference
Troubleshoot my Electronic Load - part 2: DAC/ADC
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago +3
    spoiler alert: the load works again. I checked the controller board and all functions worked fine. I connected it to the power board with the new MOSFET and back in business...
  • Andrew J
    Andrew J over 7 years ago +2
    I shall follow your investigation with interest to see how you go about it. Hopefully get some insights for when I need to do it.
  • shabaz
    shabaz over 7 years ago +2
    Hi Jan, I'm wondering if it could be ESD or inductance related perhaps. My ECU needed a MOSFET swap-out, that too had the 3-way short that you mention. In my case, it was going to one of the coils, that…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to genebren

    I've been there before, genebren. I'm confident I can fix it. (and I used the shopping cart I won in one of the P14 contests to fund some spare MOSFETs).

    Troubleshooting is a great way to fully understand how the components behave in real life - a learning opportunity. I don't see it as a drama, more as a fun exercise to do.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    I'm not expecting ESD - it happened with the FET in circuit and was a high current incident.

    During the incident, no inductance was involved. The load was directly connected to a linear DC source.

    I'm suspecting - based on the setup at the time, the things I was working on and the symptoms while it happened - that It was a bad contact in the drive or feed back circuit that drove the FET in a zone that it can't handle.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi Jan,

     

    I'm wondering if it could be ESD or inductance related perhaps. My ECU needed a MOSFET swap-out, that too had the 3-way short that you mention. In my case, it was going to one of the coils, that had clearly deteriorated. I'm guessing (can't be sure) in my case that a very high voltage was generated with nowhere to discharge, which killed the MOSFET. I could be totally wrong, I don't really know what killed it. I have the coil somewhere for a possible autopsy.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    Jan,

     

    That is quite a setback.  I hope that you are successful in putting everything back together again.  Hopefully there will be answers that can help you improve the design.

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 7 years ago

    I shall follow your investigation with interest to see how you go about it.  Hopefully get some insights for when I need to do it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<