Test & Tools
  • Technologies
  • More
Test & Tools
Blog Ultra-thin Sensor Enhances Human Touch
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 26 Feb 2020 6:41 PM Date Created
  • Views 881 views
  • Likes 4 likes
  • Comments 1 comment
  • touch
  • hmi
  • on_campus
  • cabeatwell
  • biomimicry
  • university
  • sensor
  • innovation
Related
Recommended

Ultra-thin Sensor Enhances Human Touch

Catwell
Catwell
26 Feb 2020

image

The virtually aided tactile enhancement system (VATES) allows more motion control. (Image Credit: Rongrong Bao.)

 

Humans rely on the sense of touch to manipulate objects, but that can be restricted due to injuries or wearing gloves. This can be problematic for surgeons who often have trouble manipulating soft tissues while wearing gloves. Astronauts also have issues handling equipment during spacewalks at the International Space Station. Researchers from China have developed an advanced tactile sensor that’s so sensitive it allows the wearer to feel the touch of a flower petal, light brush of a feather, a tiny wire that can’t be seen with the naked eye, and even droplets falling on a finger. The researchers published their findings in the Applied Physics Reviews on February 18, 2020.

 

The piezoresistive, crack-based sensor was inspired by a spider’s legs that are connected to sensing organs. The pattern of cracks found in the exoskeleton enables the spider to detect the smallest movements in its proximity. Likewise, the ultrathin crack-based strain sensor (UCSS) uses cracks formed in numerous thin layers of flexible polymer film coated with silver. The cracks in the silver coating are responsible for generating parallel channels that conduct electricity, which causes the sensor to become extremely sensitive to movement.

 

The researchers carried out experiments with the system, which showed that sensors made of thinner layers generated higher sensitivity while thicker layers exhibited a larger sensing range. To create a more balanced effect, researchers designed UCSSs made of 15-micron thick polymer layers and 37-nanometer thick silver coatings.

 


When the sensor was placed on a glove, researchers discovered it could monitor tiny movements. (Image Credit: Rongrong Bao.)image

 

The team also created a visually aided tactile enhancement system (VATES) by connecting UCSSs to a signal acquisition circuit and readout device. Afterward, they attached USCSSs to a glove, either on the bank of a hand or on a fingertip, which created “electronic skin.” This allowed tiny movements, like the tip of a person’s finger moving across surfaces, to be monitored. Further tests also demonstrated that the UCSSs were able to detect facial movements, like blinking, frowning, and smiling.

 

They also suggest UCSSs could be implanted in many different applications, including electronic whiskers, which could map wind flow patterns. They could also be used in wearable sensors for heartbeat and pulse detection or to enhance the sense of touch on prosthetics. 

 

“These results demonstrate the wide applications of our ultrathin strain sensor in e-skin and human-machine interfaces,” said Caofeng Pan of the Beijing Institute of Nanoenergy and Nanosystems at the Chinese Academy of Sciences.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply
  • dubbie
    dubbie over 6 years ago

    This looks interesting and if it actually works it could be really good for robotic manipulation. I worked on something similar many years ago, although much more 'coarse' and based on mechanically activated switches. It is a concept that is needed for good robotic manipulation of flexible and delicate items, such as people.

     

    Dubbie