Test & Tools
  • Technologies
  • More
Test & Tools
Forum Show us your junk!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 143 replies
  • Subscribers 394 subscribers
  • Views 16592 views
  • Users 0 members are here
Related

Show us your junk!

neuromodulator
neuromodulator over 7 years ago

I love junk, specially when it can be fully restored, has interesting parts or uses interesting technology. Most of the junk I get, comes from the university, its dumped because its either too old or it doesn't work anymore. I'll start this thread by showing one of my latest junk acquisitions:

 

imageimageimage

 

 

This is an autotransformer made by a company called "The Superior Electric Co" from Bristol, Connecticut. It was apparently build in the 60s (according to what I found in the net) and supports a max of 1.2 kva. The autotransformer works as expected but of course it shows its age, the rubber cable is not in the best condition and so isn't its paint. In the future I may repaint it and replace the cable but for now its good enough as it is.

 

Have you also found nice junk? Show us!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to neuromodulator +13
    Here is the first processor controlled instrument I designed. Intel 8748, code hand assembled on paper and entered into Intel desktop dev system by hand in hex. Not really junk, but not very useful now…
  • dougw
    dougw over 7 years ago +12
    While looking for something else deep in the "archives" I came across my favourite scientific calculator. (circa 1975) It still works fine. The LEDs were so power hungry I eventually built a power supply…
  • genebren
    genebren over 7 years ago +11
    In the spirit of your original request (show us your junk!), here is some of my junk. One of my many past jobs was working for a life sciences company that built instrumentation for various forms of testing…
Parents
  • shabaz
    shabaz over 7 years ago

    This is old junk I definitely can live without : )

    A turn of the century laptop.. I bought it used, it is a Pentium with MMX : ) I have not been able to power it up for years because the supply had died, but I tried it with a bench PSU today and it worked : )

    Booted up to Windows 95 : ) I didn't run it for long because I cannot remove the battery, the door is stuck. Still, it's Ni-Cd, about the most rugged battery technology ever.

    It has a floppy drive slot : ) and a cdrom which ejects into the lap (visible at the lower-right). The in-built trackball was great though.

    image

    It doesn't have a lot on it.. (after I finished with it, my mum just used it for driving theory training CDROM stuff for a while).

    There's this ancient PCB cad package, that actually worked, but very primitive. Also it's got a 56002 compiler that I may copy off before finally throwing it out.

    image

    There's no USB socket. But it has one of the first ever Wi-Fi cards.! The current software on the PC is for WEP, so I cannot connect to any network : (

    image

     

    Here's another piece of now-useless junk.. it was home-built microcontroller board, using a 68HC11 chip. There's a nest of wiring between the PCB sandwich. One IC is missing, it's a MAX232 chip (the serial port is at the lower-left). The big chip is EEPROM (this particular microcontroller had external address/data bus capability).

    image

    • Cancel
    • Vote Up +10 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago in reply to shabaz

    I quite liked the 68HC11 - our first suspension controller for Rolls Royce (pre BMW) used one.

    Later versions used the Siemens (now Infineon) 166  - much faster and with more stuff on chip.

     

    The 8 bit Motorola processors were really nice (for 8 bitters)  - the 6809 was really good but a bit too late.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to michaelkellett

    It was an awesome chip.. really fun to work with. 

    I had for a few months a job to work on an earlier processor, 68HC705, which I think was used in some Ford ECUs. My job was not automotive, but radio based.. it was used in a transceiver, but the source code was long ago misplaced with no version control! So, I had to disassemble it, in order to add a new feature (a new bank of channels, if the user held a button down at power-up).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago in reply to michaelkellett

    image

     

     

    Windows 95, 16M ram, has floppy drive, CMOS battery dead.

    I have two of these - bought to run a particular piece of software (now forgotten what !).

     

    Offers welcome !

     

    MK

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • rsjsouza
    rsjsouza over 7 years ago in reply to shabaz

    Wow! A windowed 68HC11!

     

    Twenty years ago I worked with the K4 variant - windowed EPROM, lots of PWMs and quite good memory for the time. Their assembly was really easy to use.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rsjsouza
    rsjsouza over 7 years ago in reply to shabaz

    Wow! A windowed 68HC11!

     

    Twenty years ago I worked with the K4 variant - windowed EPROM, lots of PWMs and quite good memory for the time. Their assembly was really easy to use.