Test & Tools
  • Technologies
  • More
Test & Tools
Forum Which flux?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 386 subscribers
  • Views 2358 views
  • Users 0 members are here
Related

Which flux?

hafcanadian
hafcanadian over 5 years ago

My SRA no-clean #312 flux pen came up dry the other day.  To finish my project of resoldering broken wires on a great grandchild’s two AA battery toy, I put some of Dad’s old tinners fluid in the pen and dabbed some on the solder points and wire ends.  Much to my joy they cleaned up unusually bright, and soldered with unusual ease. 

Curious, I later read about “tinners fluid” and discovered why.  The acidic nature of it no doubt cleaned almost too well, and in the instance of electronics it presented a corrosion potential bar none, and could dissolve adjacent materials on any circuit board.  No wonder the black plastic tip-holder on the pen partly disintegrated!  Fortunately no soldering was necessary on a pcb, just a small speaker contact and a battery box contact.  So I went back and applied an electronics cleaner and protectant.

 

Before reordering another alcohol based flux pen, that obviously doesn’t function as effectively on metal as acid flux but is necessary to not damage surrounding infrastructure, I thought I’d better ask here what flux the experts would recommend.  I’m no soldering expert and have a frustrating tremor.  I need solder to respond to heat cleanly, but often it immediately oxidizes before adhering to wire or board metal.  It’s hard for me to hold the iron tip steady on point long enough.  I’m constantly cleaning the iron tip in brass “wool” but it’s not long before the tip oxidizes over.  Working quickly is hard due to the tremor not meshing with small targets. 

 

The tinners fluid job went so much more smoothly I hardly believed it.  Perhaps a deftly-placed heat sink helped.  Regardless, I can’t be using acid fluid again on anything aside from copper pipes or something.  Should I order another pen or are there other options?  One thing I don’t like is the pen’s “felt” applicator tip wears to mush so delicate application becomes more and more difficult.

 

Joel

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 5 years ago +8
    Flux for (Pb)lead-free applications tend to be more aggressive, so that is something to consider. Instead of a flux pen, you might consider the gel-like SMD291 SMD291 from ChipQuik. It is tacky which helps…
  • baldengineer
    baldengineer over 5 years ago in reply to hafcanadian +3
    Ideally, both. Remember, “no clean” flux just means the residue left behind is inert (and non conductive.) It is still a good idea to clean it.
  • hafcanadian
    hafcanadian over 5 years ago in reply to baldengineer +1
    Thanks James. I will have the SMD291 by tomorrow. Should I still use my flux remover pen after soldering, or just wipe with a Q-tip or a Kemwipe dampened with 70% alcohol?
Parents
  • baldengineer
    baldengineer over 5 years ago

    Flux for (Pb)lead-free applications tend to be more aggressive, so that is something to consider.

     

    Instead of a flux pen, you might consider the gel-like SMD291SMD291 from ChipQuik. It is tacky which helps more of it to stay in place when applying it. (Compared to a flux pen that oozes all over the place.)

     

    Since it is in a syringe it will take you a little more effort to apply with one hand. But I think you'll be happier with how it gets applied especially if your hand shakes a little bit. At least you will be able to clearly see where it goes.

     

    SMD291 is my go-to flux. (Works fine for through-hole too.)

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 5 years ago

    Flux for (Pb)lead-free applications tend to be more aggressive, so that is something to consider.

     

    Instead of a flux pen, you might consider the gel-like SMD291SMD291 from ChipQuik. It is tacky which helps more of it to stay in place when applying it. (Compared to a flux pen that oozes all over the place.)

     

    Since it is in a syringe it will take you a little more effort to apply with one hand. But I think you'll be happier with how it gets applied especially if your hand shakes a little bit. At least you will be able to clearly see where it goes.

     

    SMD291 is my go-to flux. (Works fine for through-hole too.)

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
Children
  • hafcanadian
    hafcanadian over 5 years ago in reply to baldengineer

    Thanks James.  I will have the SMD291 by tomorrow.

     

    Should I still use my flux remover pen after soldering, or just wipe with a Q-tip or a Kemwipe dampened with 70% alcohol?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 5 years ago in reply to hafcanadian

    Ideally, both.

     

    Remember, “no clean” flux just means the residue left behind is inert (and non conductive.)

     

    It is still a good idea to clean it.

    • Cancel
    • Vote Up +3 Vote Down