Products
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
Test & Tools
  • Technologies
  • More
Test & Tools
Forum Can bus decording in Picpscope
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 462 views
  • Users 0 members are here
  • in
  • bus
  • picpscope
  • decording
  • can
Related

Can bus decording in Picpscope

dsohal
dsohal over 17 years ago

The latest beta version of PicoScope is now available for download from Pico Labs. This version includes a  totally new CAN Bus decoding function, which can read CAN bus packets at a  variety of data rates.

The CAN (Controller Area Network) Bus is widely used in automotive,  industrial and medical control systems for reliable signalling between control  units in electrically noisy environments. It is a serial protocol, usually with  differential signalling although a single-wire version also exists. The  PicoScope CAN Bus decoding feature is aimed at vehicle designers, aftermarket  equipment designers and advanced troubleshooters, who need to look at more than  just fault codes.

Here are some of the highlights:

  • Graphical in-view display - the decoded data is displayed  directly below the raw waveform, making it possible to see error packets in a  long stream of data at the same time as checking for noise and glitches
  • Tabular display - lists all the CAN packets in the current  view, or the entire waveform buffer, with data columns that can be hidden if not  needed
  • Filtering - to reduce clutter, PicoScope can list only  those packets that match your criteria
  • "Start from" - monitors the data stream until a specified  packet type occurs, then starts capturing
  • Works with standard PicoScopes - there's no need to upgrade  your hardware: just download our free software update. Performance and memory  capacity will of course depend on the specifications of your scope. We recommend  using scopes with deep memory, such as the 4000 and 5000 Series.
  • Single-ended and differential modes - choose whether to  decode CAN High or CAN Low, useful for single-wire CAN systems, or use two scope  channels to decode the full differential CAN signal
  • Adjustable data rate - decode any speed of CAN Bus from  kilobits to megabits
  • Save to file - save a table of CAN data in comma-separated  text format

As an added bonus, this release also includes another new feature:

  • Zoom overview - when you are zoomed in, a small overview  window shows the current display area marked on a picture of the whole waveform.  You can drag and resize this area instead of using the zoom tools.

Download PicoScope 6.3.4 beta, free of  charge, from Pico Labs now. No registration required.

Please let us know what you think of the new software. You can contact us on  the forum.

PicoLog updated

PicoLog is  our data logging software for Windows. It works with all our data loggers, and  can save data to a file or display it in spreadsheet and graphical  formats.

R5.20.8 is the latest maintenance release of PicoLog. Bugs fixed  include: "Corruption of .plw files", "repeat immediate mode" and "PicoLog pause  button causes program to crash and close".

Download PicoLog  R5.20.8