Test & Tools
  • Technologies
  • More
Test & Tools
Forum I recently bought a PicoScope 2203. While playing with it for the first time, I noticed some switching sound coming from inside. Is there a relay internally that produces this noise?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 385 subscribers
  • Views 499 views
  • Users 0 members are here
  • that
  • 2203.
  • noticed
  • while
  • the
  • inside.
  • from
  • this
  • first
  • there
  • is
  • sound
  • coming
  • for
  • with
  • switching
  • produces
  • playing
  • time
  • it
  • recently
  • internally
  • picoscope
  • a
  • some
  • bought
  • i
  • relay
  • noise?
Related

I recently bought a PicoScope 2203. While playing with it for the first time, I noticed some switching sound coming from inside. Is there a relay internally that produces this noise?

dsohal
dsohal over 16 years ago
Yes, this noise is caused by the relays that select the input range. The amount  of switching depends on the software in use and the input range that is  selected. This is part of the normal operation of the scope.
  • Sign in to reply
  • Cancel
  • koh
    koh over 16 years ago

    The scopes have relays which switch between the high and low voltage ranges on each channel. When running, the input signal is fed through from one input connector to both channel’s A to D converters in parallel to get twice the bandwidth. Then the other input connector is routed through the same pair of A to D converters and so on in a cycle. At any one time, the unused input connector and pre-amplifier chain is set to the highest voltage (lowest gain) condition to avoid injecting cross-talk onto the live channel. If either channel is set to +/-1V or lower, then the gain relay will cycle continuously. The only way to have two channels in use without the relay noise is to have both set to any voltage greater than +/-1V (+/-2V to +/-20V, they can be different).