• Products and Partners
    Products and Partners
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
Test & Tools
  • Technologies
  • More
Test & Tools
Forum Keithley Introduces Low-Cost, Full-Featured USB-to-GPIB Interface Adapter
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 453 views
  • Users 0 members are here
Related

Keithley Introduces Low-Cost, Full-Featured USB-to-GPIB Interface Adapter

PRismaPR
PRismaPR over 16 years ago

For high resolution Image http://www.ggcomm.com/KEI/NR/KUSB488B_HR.JPG

or contact info@prismapr.com

 

Keithley Introduces Low-Cost, Full-Featured USB-to-GPIB Interface Adapter

 

Cleveland Ohio June 24 2010 Keithley Instruments Inc(NYSE:KEI a world leader in advanced electrical test instruments and systems has introduced the Model   USB-to-GPIB Interface Adapter The Model  KUSB-488BKUSB-488B which complements Keithley’s precision measurement instruments is priced at$495 USD which is less than competitive versions helping test engineers and researchers lower their cost of test measurement and ownership To minimize the cost associated with switching to a new adapter the Model KUSB-488B’s driver library is fully command-compatible with Keithley’s traditional GPIB command set and National InstrumentsTM(NITM command set making it plug-and-play compatible with existing applications The driver library is also compatible with Keithley’s PCI-based Model  KPCI-488LPAKPCI-488LPA GPIB interface making it easy to switch from either a PCI or USB approach to GPIB control protecting users software investment and lowering their overall cost of test

 

The   provides complete support for Windows 2000/XP/Vista The  KUSB-488BKUSB-488B also supports industry-standard VISA(Virtual Instrument Software Architecture libraries to ensure compatibility with applications using VISA For OEMs a utility is included to install the driver software silently bypassing the normal installation so that the driver can be installed with the OEM’s software The interface ships with 32-bit dynamic link libraries for Application Development Environments(ADEs running under Windows XP/2000/Vista and drivers for the most current programming languages including Microsoft Visual Basic Visual C Visual Studio.NET Borland Delphi LabVIEW Version 7.0 and up(VISA and IEEE-488.2 and LabWindows/CVI Version 7.0 and up(VISA and IEEE-488.2 A diagnostic/interactive tool is included for quick verification of communication between the interface and a GPIB-capable instrument such as Keithley’s digital multimeters(DMMs SourceMeter instruments switch mainframes and cards low level measurement systems and a wide variety of other specialized test solutions

 

Availability

The Model  KUSB-488BKUSB-488B is available from stock

 

For More Information

For more information on Keithley's Model  KUSB-488BKUSB-488B USB-to-GPIB Interface Adapter contact the company at www.keithley.com.

 

About Keithley Instruments, Inc.

With more than 60 years of measurement expertise, Keithley Instruments has become a world leader in advanced electrical test instruments and systems. Our customers are scientists and engineers in the worldwide electronics industry involved with advanced materials research, semiconductor device development and fabrication, and the production of end products such as portable wireless devices. The value we provide them is a combination of products for their critical measurement needs and a rich understanding of their applications to improve the quality of their products and reduce their cost of test. * * * Products and company names listed are trademarks or trade names of their respective companies.

 

Reader Contact:

Keithley Instruments

Phone: +49-89-84 93 07-40

info@keithley.de

 

Editorial Contacts:

PRismaPR UK

Monika Cunnington

Phone: +44-1462-64 07 79

monika@prismapr.com

 

PRismaPR

Gabriele Amelunxen

Phone: +49-8106-24 72 33

info@prismapr.com

Attachments: