Products
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
Test & Tools
  • Technologies
  • More
Test & Tools
Forum DSO Nano Pocket Oscilloscope, quick and dirty review
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 698 views
  • Users 0 members are here
  • test
  • oscilloscope
  • software
Related

DSO Nano Pocket Oscilloscope, quick and dirty review

Catwell
Catwell over 16 years ago
Originally meant to house a MP3  player, Seeed Studio  instead fitted a fully functional Oscilloscope inside. Based on an ARM Cortex  M3, a 320x240 pixel display, SD card storage, USB, and best of this O-scope  has rechargeable batteries. Meaning, you can do a spot test on the fly, anywhere, and  store the wave form. With a sampling rate of 1Mhz, this is a great tool for small circuitry design. In fact an associate of mine bought one of these  solely to test output of micro controller projects. He said it has come in handy countless times.
 
My immediate opinion of the build  quality is it feels cheap, but solidly put together, no cracking or squeaking plastic. It’s quite light weight, I was afraid I might break it at first.
 
As soon as I turned it on, I was  impressed. It looks as though a switch debounce sample was saved to the  SD card, and by default loaded the wave form; see below.
image
It took about a half hour of reading the manual and  tinkering to get operational. All operations are done via two buttons and a D-pad.  I did find myself touching the DSO Nano’s screen to operate. I suppose I am a  victim of the recent touch screen revolution. But, I’m fine with the buttons.  Navigation is easy and clear.
 
Before this, I had bought a USB  based O-scope that needed a computer/laptop to run. I was happy with its mobility, but soon found  that having to be near AC outlets to power the laptop and scope to be  annoying at times. The DSO nano, does away with all tethering issues. For example, I  took it over to a box of components I have laying around, hooked it up to the  output of a stepper motor and sampled pulse I generated by spinning the motor  by hand (below), easy and quick is the only way to define the experience. As you  can see, the motor generated about 2.5V.
 
The fact that I was able to quickly set up the test, save the file, and return to my PC makes me wish I had one of these years  ago. Being tethered to an aging, large O-scope in the same old testing area is a  bit inconvenient, now that I think about it. Now the testing lab can be  anywhere, anytime, I want.
image
The only bad experience I had was  the screen produced some artifacts that stayed on the screen during the stepper motor test the  whole time. It didn’t get in the way of seeing the wave form, but I just  didn’t like seeing the errors. I reset the DSO Nano and the problem was cleared. I  assume the next firmware update will solve this issue.
 

Within minutes I put this O-scope to  use. Walked away from my workbench, took a sample, saved the wave for, and returned. This  alone gets my seal of approval. If you are just a hobbyist, tinkerer, hacker, or a salaried design engineer, I whole heartedly recommend the DSO Nano Oscilloscope. It will satiate your gadget lust, at least for a little while. MSRP $89 USD

 

All we need now is the same  technology on our touchscreen phones.

Cabe
 
Features:
 
Display
2.8″ Color   TFT LCD
Display   Resolution
320×240
Display   Color
65K
Analog   bandwidth
0 - 1MHz
Max sample   rate
1Msps 12Bits
Sample   memory depth
4096   Point
Horizontal   sensitivity
1uS/Div~10S/Div (1-2-5 Step)
Horizontal   position
adjustable   with indicator
Vertical   sensitivity
10mV/Div~10V/Div (with ×1 probe)
0.5V/Div~100V/Div (with ×10 probe)
Vertical   position
adjustable   with indicator
Input   impedance
>500KΩ
Max input   voltage
80Vpp (by ×1   probe)
Coupling
DC
Trig modes
Auto, Norma,   Single, None and Scan
Functionalities:
Automatic   measurement: frequency, cycle, duty, Vpp, Vram, Vavg and DC voltage
Precise   vertical measurement with markers
Precise   horizontal measurement with markers
Rising/falling   edge trigger
Trig level   adjustable with indicator
Trig   sensitivity adjustable with indicator
Hold/run   feature
Test signal
Built-in   10Hz~1MHz (1-2-5 Step)
Waveform   storage
SD card
PC   connection via USB
as SD card   reader
Upgrade
by bootloader   via USB
Power supply
3.7V   Chargeable Lithium battery / USB
Dimension   (w/o probe)
105mm X 53mm   X 8mm
 
What you get when you buy a DSO Nano. The O-scope, one set of test leads, and a velvet bag to carry it in.