Test & Tools
  • Technologies
  • More
Test & Tools
Forum Keithley launches new general purpose programmable power supply product line
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 323 views
  • Users 0 members are here
Related

Keithley launches new general purpose programmable power supply product line

PRismaPR
PRismaPR over 15 years ago

For high resolution image: http://www.ggcomm.com/KEI/2200_30_5_PR_HR.jpg or at info@prismapr.com

 

Press Release 25/2011

Keithley Launches New General Purpose Programmable Power Supply Product Line

 

Choice of five supplies from 86W to 150W • Max. output voltages from 20V to 72V • Excellent output and measurement resolution for low power testing

 

Cleveland, Ohio, 19 September 2011   * * *   Keithley Instruments, Inc., a world leader in advanced electrical test instruments and systems, announced today the availability of five new general-purpose programmable DC power supplies designed to complement the company’s existing line of specialty power supplies and source measurement instruments for component, module, and device characterization and test applications. The Series 2200 family combines superior voltage and current output accuracy at a cost-effective price, flexible operation, and features designed to enhance ease of use in a variety of device characterization or test applications. More information on the Series 2200 is available on Keithley’s website: http://www.keithley.com/data?asset=55901.

 

The five models in the Series 2200 line offer maximum voltage, current, and power output levels designed to address a wide range of sourcing requirements for characterizing components, circuits, modules, and complete devices:

•     Model 2200-20-5: 20V, 5A, 100W

•     Model 2200-30-5: 30V, 5A, 150W

•     Model 2200-32-3: 32V, 3A, 96W

•     Model 2200-60-2: 60V, 2.5A, 150W

•     Model 2200-72-1: 72V, 1.2A, 86W

 

High output accuracy

The voltage output accuracy of Series 2200 power supplies is specified at 0.03%; their current output accuracy is 0.05%. Both specifications are significantly better than those of competitive general-purpose supplies. In addition, their high output (1mV) and measurement (0.1mA) resolution makes them well-suited for characterizing low power circuits and devices in applications such as measuring idle mode and sleep mode currents to confirm devices can meet today’s ever-more-challenging goals for energy efficiency. Remote sense terminals on the back panel and less than 5mVp-p noise help ensure that the voltage programmed is the voltage that the supply actually outputs. A dual-line display shows both the programmed values and actual outputs for a continuous indication of the status of the power delivered to the load.

 

Flexible operation

Series 2200 supplies include a variety of features designed to enhance operating versatility. For example, each model provides 40 onboard memory locations for storing frequently used test setups for later recall and reuse. In addition, a built-in list mode function supports the programming and storage of up to seven custom test sequences of up to 80 steps. Once saved, a sequence can be triggered to run manually using the instrument’s front panel keys, automatically via an external trigger, or by using programmable interface commands. Competitive general-purpose power supplies don’t provide these capabilities.

 

Protection for the devices under test (DUTs)

Several Series 2200 features help protect DUTs from damage during testing, including a programmable voltage limit value that prevents the supply from outputting excessive voltage (even if a voltage higher than the limit is entered into the instrument) and a programmable over-voltage function that causes the output to drop to less than 1V if the over-voltage limit is reached.  These limits are in addition to the current limit setting function, which controls the level of current that can flow into the DUT. Also, a programmable timer can be used to turn off the output after a specified time interval, so tests can be preprogrammed to run unattended without worrying about excess voltage or power being applied to the DUT for an extended period of time.

 

Superior ease of use

Multiple methods for adjusting the supplies’ voltage and current settings are provided, including a direct-entry numeric keypad on the front panel. In addition, a rotary knob with adjustable step size simplifies studying the response of a device-under-test (DUT) to voltage or current changes.

 

Series 2200 power supplies can be controlled easily over either a standard GPIB or USB interface. The USB interface is test and measurement class (TMC) compliant, so users can employ the standard SCPI command syntax. Standard instrument drivers are included to simplify integrating the power supplies into an automated test environment.

 

Availability

Shipments are beginning in December 2011. Additional information on the Series 2200 family is available on Keithley’s website: http://www.keithley.com/data?asset=55901.

To learn more about Keithley, contact the company at: www.keithley.com.

 

About Keithley Instruments, Inc.

With more than 60 years of measurement expertise, Keithley Instruments has become a world leader in advanced electrical test instruments and systems. Our customers are scientists and engineers in the worldwide electronics industry involved with advanced materials research, semiconductor device development and fabrication, and the production of end products such as portable wireless devices. The value we provide them is a combination of products for their critical measurement needs and a rich understanding of their applications to improve the quality of their products and reduce their cost of test. In 2010, Keithley Instruments joined Tektronix as part of its test and measurement portfolio.

* * *

Products and company names listed are trademarks or trade names of their respective companies.

 

Keithley Instruments

Phone: +49 89 84 93 07 40

info@keithley.de

www.keithley.com

 

PRismaPR

Gabriele Amelunxen

Phone: +49 8106 24 72 33

info@prismapr.com

www.prismapr.com