Test & Tools
  • Technologies
  • More
Test & Tools
Forum congatec AG set to expand its product strategy with  ARM architecture
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 340 views
  • Users 0 members are here
  • freescale
  • congatec
  • computer-on-modules
  • i.mx
  • arm
  • Architecture
Related

congatec AG set to expand its product strategy with  ARM architecture

PRismaPR
PRismaPR over 14 years ago

Visit congatec at SPS/IPC/Drives in Nuremberg in Hall 8, Booth #528

image

Photo of Gerhard Edi and Text available: http://pr.congatec.com

 

Press Release 13/2011

congatec AG set to expand its product strategy with  ARM architecture

Cooperation with Freescale broadens future selection of Computer-on- Modules

 

Nuremberg, Germany, 22 November 2011 * * * congatec AG, a leading manufacturer of embedded computer modules, is set to expand its product portfolio with the addition of ARM technology. This will allow the company to offer products with extremely low power requirements in the future. As a first step in that direction, congatec is expanding its Qseven product family with Freescale processors.

Up until now, congatec has focused exclusively on x86-based COMs (Computer-on Modules). As part of its new product strategy, the company now plans to increasingly use ARM technology. Processor technology, which in the past only offered a choice between Intel and AMD, will now be extended to include Freescale and its ARM-based i.MX portfolio of products.

The COM concept integrates all generally available interfaces onto the computer module itself while any special interfaces are implemented on individually-tailored carrier boards. In complete contrast, the majority of existing ARM processors come with specialized interfaces designed to suit dedicated applications. These cannot be used by COMs in a standard format and are therefore neither interchangeable nor scalable. However, the new generation of ARM processors focuses on standard PC interfaces such as USB and PCI Express and will therefore be ideally suited to COMs.

The Qseven standard was designed from the very beginning around modern interfaces. Its specification was updated in September 2010 (Revision 1.20) to enable the development of 100% compatible ARM-based modules. The features offered by modern ARM processors and the interface definitions of the Qseven are a perfect match and require no additional I/Os. This allows the development of price/performance-optimized modules and also makes the modules suitable for a range of completely new applications – many of them related to mobile operation and deployment.

“In Freescale, we have found a reliable partner with whom we will be able to meet the requirements of our customers with regard to operating system support and long-term availability. Thanks to our close cooperation with Freescale, we are now in a position to begin the development of Qseven modules with extremely low levels of power consumption,” said Gerhard Edi, CEO of congatec AG. “In order to also give our customers a massive time-to-market advantage with this platform, we are investing heavily in software support for the ARM processors.”

Henri Richard, senior vice president of Sales and Marketing for Freescale said, “Our ecosystem of partners is an integral part of our go-to-market strategy. congatec is an ideal partner in every aspect of our collaboration, and our next generation i.MX products will be introduced into applications more quickly and easily thanks to congatec’s Qseven modules.”

The first products resulting from the Freescale collaboration are expected to be available by the middle of 2012.

About congatec AG

congatec AG has its head office in Deggendorf, Germany and is a leading supplier of industrial computer modules using the standard form factors Qseven, COM Express, XTX and ETX. congatec’s products can be used in a variety of industries and applications, such as industrial automation, medical technology, automotive supplies, aerospace and transportation. Core knowledge and technical know-how includes unique extended BIOS features as well as comprehensive driver and board support packages. Following the design-in phase, customers are given support via extensive product lifecycle management. The company’s products are manufactured by specialist service providers in accordance with modern quality standards. congatec currently has 112 employees and entities in Taiwan, USA and the Czech Republic. More information is available on our website at www.congatec.com

 

Reader Inquiries:

congatec AG

Christian Eder

Phone: +49-991-2700-0

info@congatec.com

www.congatec.com

 

Press contact:

PRismaPR (UK + Scandinavia)

Monika Cunnington

Phone: +44-1462-640779

monika@prismapr.com

www.prismapr.com

 

PRismaPR

Bettina Lerchenmüller

Phone: +49-8106-24 72 33

info@prismapr.com

www.prismapr.com