Test & Tools
  • Technologies
  • More
Test & Tools
Forum Keithley Expands Measurement Capability of S530 Parametric Test Systems
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 520 views
  • Users 0 members are here
  • test
  • instruments
  • &
  • systems
  • keithley
  • measurement
  • parametric
  • s530
Related

Keithley Expands Measurement Capability of S530 Parametric Test Systems

PRismaPR
PRismaPR over 14 years ago

image

For high resolution image:

http://www.ggcomm.com/KEI/S530_PR_HR.jpg

or at info@prismapr.com

 

Press Release 7/2012

 

Keithley Expands Measurement Capability of S530 Parametric Test Systems

 

48-Pin Full Kelvin Switching • Ring Oscillator, Pulsing, Low Voltage DMM Options

 

Cleveland, Ohio, March 29, 2012   * * *   Keithley Instruments, Inc., a world leader in advanced electrical test instruments and systems, continues to enhance the capabilities of its S530 Parametric Test Systems, the semiconductor industry’s most cost-effective solution for high speed production parametric test. Supported by the latest version of Keithley Test Environment software (KTE V5.4), the S530 can now be configured for 48-pin full Kelvin switching and with new integrated options for pulse generation, frequency measurements, and low voltage measurements. These new enhancements allow S530 systems to address an even broader range of production parametric test applications with one high speed, cost-effective test solution.

 

48-Pin Full Kelvin Switching Configuration

The S530 Low Current System employs a high performance switch matrix to direct signals between instruments and test pins, providing sub-picoamp measurement resolution and low current guarding all the way to the probe pin. The latest enhancements to this system now support a 48-pin full Kelvin (four-wire) switching configuration, doubling the full Kelvin pin-count previously available. By maintaining the signal integrity associated with full Kelvin switching and cabling while doubling the system’s maximum pin-count, the S530 combines precise high speed measurements with enhanced system configuration flexibility to ensure full test coverage well into the future.

 

Optional Ring Oscillator Measurement Capability

A new high speed, high resolution oscilloscope option supports ring oscillator testing over a broad frequency measurement range. With a sample rate of up to 400 megasamples/second, this new system option provides measurements from approximately 10kHz to 20MHz. Frequency measurement capability within parametric test systems has become increasingly important as a growing number of semiconductor fabs have incorporated ring oscillators into their overall process control monitoring test structures.

 

Optional Pulse Generation Capability

As more integrated circuits incorporate embedded memory such as flash into their design, semiconductor fabs have increasingly added memory structures and measurements to their process control monitoring routines. Testing these devices requires sourcing user-defined voltage pulses to program and erase memory cells, followed by precise DC measurements of the device. To address this need, the S530 uses the same sub-system chassis that currently hosts the capacitance-voltage (C-V) instrument card to integrate two, four, or six channels of pulse generation capability into the configuration, so it can produce a wide range of device testing waveforms and extend system flexibility.

 

Optional System DMM

Testing van der Pauw and metal structures as part of process control monitoring demands a combination of low voltage measurements, high measurement resolution, and excellent repeatability. For these applications, S530 systems now offer an optional 7-1/2-digit, low-noise digital multimeter optimized for low voltage measurements. It provides 10nV resolution on its lowest (100mV) range and 100nV resolution on its next lowest (1V) range. It also offers 7ppm DC voltage repeatability.

 

Choice of Low Current or High Voltage Systems

Two different S530 systems are available. The S530 Low Current System was developed for measuring characteristics such as sub-threshold leakage, gate leakage, etc. The S530 High Voltage System incorporates a source measurement unit (SMU) capable of sourcing up to 1000V at 20mA (20W max.) to any system pin. This version is optimized for the difficult breakdown and leakage tests that GaN, SiC, and Si LDMOS power devices demand. Although the new 48-pin Kelvin capability is unique to the low current system, all of the new measurement options are available for both systems.

 

For More Information

To learn more, visit http://www.keithley.com/products/semiconductor/parametrictestsys/ or contact the company at: www.keithley.com.

 

About Keithley Instruments, Inc.

With more than 60 years of measurement expertise, Keithley Instruments has become a world leader in advanced electrical test instruments and systems. Our customers are scientists and engineers in the worldwide electronics industry involved with advanced materials research, semiconductor device development and fabrication, and the production of end products such as portable wireless devices. The value we provide them is a combination of products for their critical measurement needs and a rich understanding of their applications to improve the quality of their products and reduce their cost of test. In 2010, Keithley Instruments joined Tektronix as part of its test and measurement portfolio.

 

* * *

Products and company names listed are trademarks or trade names of their respective companies.

 

Reader Contact:  

Keithley Instruments

Phone: +49-89-84 93 07-40

info@keithley.de

www.keithley.com

 

Editorial Contacts:

PRismaPR UK

Monika Cunnington

Phone: +44-1462-64 0779

monika@prismapr.com

www.prismapr.com

 

PRismaPR

Gabriele Amelunxen

Phone: +49-8106-24 72 33

info@prismapr.com

www.prismapr.com