Test & Tools
  • Technologies
  • More
Test & Tools
Forum Keithley Expands DMM Line, Adding Economical, Programmable 5-1/2-Digit Digital Multimeter
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 196 views
  • Users 0 members are here
Related

Keithley Expands DMM Line, Adding Economical, Programmable 5-1/2-Digit Digital Multimeter

PRismaPR
PRismaPR over 14 years ago

image

For high resolution image: http://www.ggcomm.com/KEI/2110_HR.jpg or at info@prismapr.com

 

Press Release 15/2012

Keithley Expands DMM Line, Adding Economical, Programmable 5-1/2-Digit Digital Multimeter

Capabilities usually found only in a 6-1/2-digit DMM now available at a break-through price in a 5-1/2-digit multimeter

 

Cleveland, Ohio, 17 September, 2012   * * *   Keithley Instruments, Inc., a world leader in advanced electrical test instruments and systems, continues to build on its long history in digital multimeter (DMM) design with an economical new offering. The Model 2110 5-1/2-digit Dual-Display Digital Multimeter is optimized for a variety of general-purpose system and bench design applications. When compared with leading 5-1/2-digit DMMs, the Model 2110 offers superior throughput (up to 10x faster), accuracy (up to 2x better DC voltage accuracy), a lower purchase price, and greater integration flexibility. System features such as external triggering, a built-in reading buffer, and an optional GPIB interface enhance ease of use. To learn more about the Model 2110 DMM, visit www.keithley.com/data?asset=57008.

 

A Rich Feature Set at a Value Price

The Model 2110’s capabilities include DC voltage (up to 1000V) and current (up to 10A), AC voltage (up to 750V) and current (up to 10A), two- and four-wire resistance (up to 100 mega-ohms), temperature, frequency (10Hz–300kHz) and period, and capacitance (1 nanofarad to 100 microfarad ranges) measurements. A variety of mathematical functions and diode and continuity test functions are also included. Programmable A-D converter and filter settings simplify optimizing the Model 2110’s signal-to-noise ratio to improve measurement accuracy. At the fast 4-1/2-digit setting, it takes up to 50,000 readings/second.

 

The instrument’s dual display can show the results from two measurements simultaneously, such as DC voltage and temperature, so users can monitor temperature fluctuations without interrupting other measurements. Its intuitive front panel makes it easy enough for students to use without sacrificing measurement performance or flexibility.

 

Temperature Measurement Support

Temperature is the most commonly measured parameter, and the Model 2110 includes support for making temperature measurements with RTDs, NTC thermistors, and B, C, E, J, K, N, R, S and T-type thermocouples. A built-in cold junction compensator ensures higher thermocouple measurement accuracy without the need for additional plug-ins.

 

Built-in Mathematical Functions and Included Test Tools

To simplify the process of converting raw measurement data into usable information, the Model 2110 includes the most often-used mathematical functions: percentage, average, min/max, null, limits, mX+B, dB, and dBm. The KI-Tool and KI-Link software tools included help users to control the instrument remotely, record measurements, and display time-series plots of the results, then import them into either MicrosoftRegistered Word or Excel files for creating reports. LabVIEWRegistered and IVI drivers provide further programming flexibility.

 

Remote Interfaces

With USB-only or USB/GPIB control options, the Model 2110 is simple to integrate into test systems with other instruments, such as Keithley’s growing line of Series 2200 DC Power Supplies. The TMC-compliant USB remote interface and the optional GPIB interface allow easy re-use of existing SCPI programs.

 

Wide Range of Applications

The Model 2110 DMM offers high value for applications in manual, semi-automatic, and automatic testing of low-cost electronic devices, circuits, modules, electrical components, and semiconductor components. Production, R&D, and test engineers, scientists, and students will find it useful for making a wide variety of measurements in the portable, bench, and system applications that don’t demand the ultra-high precision that Keithley’s other Series 2000 DMMs provide but that do require stable, accurate, and high speed measurements.

 

Pricing and Availability

The expected UK list price of the Model 2110 5-1/2-Digit Dual-Display DMM is £394 for the USB-only version and £480 for the USB/GPIB option with sales beginning immediately.

Expected list price in

France          USB-only version: €479, USB/GPIB option: €584

Italy          USB-only version: €485, USB/GPIB option: €591

Germany     USB-only version: €473, USB/GPIB option: €576

 

Units will ship from stock or within two weeks ARO. The instrument includes a one-year factory warranty and three- and five-year extended warranties are available.

 

For More Information

Additional information on the Model 2110 is available on Keithley’s website at http://www.keithley.com/data?asset=57008. To learn more about Keithley, contact the company at: www.keithley.com.

 

About Keithley Instruments, Inc. With more than 60 years of measurement expertise, Keithley Instruments has become a world leader in advanced electrical test instruments and systems. Our customers are scientists and engineers in the worldwide electronics industry involved with advanced materials research, semiconductor device development and fabrication, and the production of end products such as portable wireless devices. The value we provide them is a combination of products for their critical measurement needs and a rich understanding of their applications to improve the quality of their products and reduce their cost of test. In 2010, Keithley Instruments joined Tektronix as part of its test and measurement portfolio.

* * *

Products and company names listed are trademarks or trade names of their respective companies.

 

Reader Contact:

Keithley Instruments

Phone: +49-89-84 93 07-40

info@keithley.de

www.keithley.com

 

Editorial Contacts:

PRismaPR UK

Monika Cunnington

Phone: +44-20 8133 6148

monika@prismapr.com

www.prismapr.com

 

PRismaPR

Gabriele Amelunxen

Phone: +49-8106-24 72 33

info@prismapr.com

www.prismapr.com