Test & Tools
  • Technologies
  • More
Test & Tools
Forum Economical Dual- and Triple-Channel Programmable  Power Supplies from Keithley Outperform More Costly Competitive Supplies
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 365 subscribers
  • Views 228 views
  • Users 0 members are here
Related

Economical Dual- and Triple-Channel Programmable  Power Supplies from Keithley Outperform More Costly Competitive Supplies

PRismaPR
PRismaPR over 13 years ago

image

 

For high resolution image: http://www.ggcomm.com/KEI/2220_2230_HR.jpg or at info@prismapr.com

 

Press Release 16/2012

 

Economical Dual- and Triple-Channel Programmable  Power Supplies from Keithley Outperform More Costly Competitive Supplies

 

0.03% basic voltage and 0.1% basic current readback accuracy for higher data confidence • Isolated and independent outputs for greater testing flexibility • Easier to interpret displays

 

Cleveland, Ohio, 8 October 2012   * * *   Keithley Instruments, Inc., a world leader in advanced electrical test instruments and systems, announced today the addition of two multi-channel power supplies to the company’s Series 2200 line of programmable DC power supplies. Both combine the advantage of greater output accuracy than offerings from the market leader at prices that are substantially lower, as well as features that enhance ease of use in circuit design, university student labs, materials research, and device testing that requires the use of more than one power source. With these new models, Keithley now offers a range of one-, two-, and three-channel power supplies that complement its broad source and measurement instrumentation offering. More information on Keithley’s expanding DC power supply line is available on the company’s website at www.keithley.com/data?asset=57005.

 

The new supplies’ output levels are designed to address a wide range of sourcing requirements for characterizing components, circuits, modules, and complete devices. The Model 2230-30-1 supply provides two output channels, typically used for powering analog circuits, with each channel capable of outputting up to 30V/1.5A/45W, plus a 6V/5A/30W output channel, typically used for powering digital circuits. (In contrast, the market-leading three-channel supply’s analog outputs are limited to just 25V@1A.) The Model 2220-30-1 supply provides two output channels, each capable of outputting up to 30V/1.5A/45W. These maximum output levels, combined with voltage setting and reading resolution of 1mV and current setting and reading resolution of 1mA, allow generating a wider range of output power and reading a wider range of load currents with high precision.

 

Better Voltage and Current Output and Readback Accuracy than the Competition

With basic voltage setting accuracy and voltage readback accuracy of 0.03% for each output channel (compared to the market leader’s lower accuracy of 0.05%), Series 2200 multi-channel supply users can be confident the exact voltage they program for any channel is the level applied at the output terminals. Unlike the many competitive units that don’t offer remote sensing, rear-panel remote sense terminals on each channel of the new Series 2200 supplies compensate for voltage drops in the power supply leads to ensure that the correct voltage is delivered to the load terminals of the DUT, enhancing overall system accuracy. They also offer 0.1% basic current setting and readback accuracy (versus the market leader’s 0.15% accuracy) and less than 3mVp p ripple and noise to ensure high quality load current measurements.

 

Isolated and Independent Outputs for Greater Testing Flexibility than Competing Supplies

Each output channel is completely isolated, which allows the new supplies to power two isolated circuits with different reference points, eliminating the need for a second supply. Many competitive multi-channel supplies do not offer isolated channel outputs and cannot properly power isolated circuits. Each channel can also be turned on or off independently, so the supplies can be used to power up a circuit that requires turning on multiple voltage levels in a specified time sequence. A programmable timer allows setting up a test to run unattended, turning off the outputs after a specified interval.

 

Reconfigurable Outputs and Easier-to-Understand Output Displays

For applications that require supplying more than 30V or 1.5A, the new supplies’ 30V outputs can be combined in a variety of configurations, such as being wired in series to produce a 60V output with a maximum current output of 1.5A or wired in parallel to produce a 3A output at 30V. When configured this way, special display modes show the actual voltage and current for the combined pair. This is an important advantage over competitive units, which typically do not show the actual combined output, increasing the potential for confusion or incorrect interpretation of the displayed results. The new Keithley supplies also allow configuring the 30V outputs to test a bipolar circuit or maintain a user-defined ratio between the two outputs when using Tracking mode.

 

Protection for Delicate Devices under Test (DUTs)

Several features help protect fragile or experimental DUTs from damage during testing, including programmable voltage maximum values that prevent the accidental entry of a channel’s voltage above the pre-set value. These settings are in addition to the current limit setting function, which controls the level of current that can flow into the DUT, and each output channel’s limit can be set independently. In addition, all front panel controls can be locked using a user-definable password to prevent inadvertent changes during critical tests. Optimized for Test System Integration  The new multi-channel power supplies are designed to perform as effectively in automated test systems as they do in manual configurations. A USB TMC-compliant device port makes it easy to control each remotely from a variety of programming environments. For example, Tektronix Edition LabVIEW SignalExpressTm from National Instruments provides all the tools needed for basic instrument control, data logging, and analysis. This programming environment, which supports a wide range of Tektronix bench instruments, can be used to automate the entire test bench or test system by providing access to the features of multiple instruments from one intuitive software interface.

 

Flexible Operation and High Ease of Use

A variety of features enhance the operating versatility and simplify operation of the new supplies:

•     Instrument settings can be saved to one of 30 internal memory locations to save time when conducting repetitive tests.

•     A rotary knob with adjustable step size simplifies studying a DUT’s response to voltage or current changes. A numeric keypad offers an alternative method of entering values precisely.

•     Voltage and current outputs for all channels are shown simultaneously on the bright vacuum fluorescent display, unlike competitive units, which can display only one channel at a time.

•     Standard IVI-Com and LabVIEW instrument drivers ease integration into automated test environments.

 

Pricing and Availability

The expected list prices of the new power supplies are as follows, with immediate availability from Keithley sales partners:

UK          * Model 2220-30-1 Dual-Channel DC Power Supply: £635

* Model 2230-30-1 Triple-Channel DC Power Supply: £768

 

France      * Model 2220-30-1 Dual-Channel DC Power Supply: €772

* Model 2230-30-1 Triple-Channel DC Power Supply: €934

 

Italy           * Model 2220-30-1 Dual-Channel DC Power Supply: €779

* Model 2230-30-1 Triple-Channel DC Power Supply: €943

 

Germany     * Model 2220-30-1 Dual-Channel DC Power Supply: €761

* Model 2230-30-1 Triple-Channel DC Power Supply: €921

 

For More Information

More information on the latest additions to the Series 2200 family is available on Keithley’s website at www.keithley.com/data?asset=57005. To learn more about Keithley, contact the company at:  www.keithley.com. About Keithley Instruments, Inc. With more than 60 years of measurement expertise, Keithley Instruments has become a world leader in advanced electrical test instruments and systems. Our customers are scientists and engineers in the worldwide electronics industry involved with advanced materials research, semiconductor device development and fabrication, and the production of end products such as portable wireless devices. The value we provide them is a combination of products for their critical measurement needs and a rich understanding of their applications to improve the quality of their products and reduce their cost of test. In 2010, Keithley Instruments joined Tektronix as part of its test and measurement portfolio. * * *

 

Reader Contact:           

Keithley Instruments

Phone: +49-89-84 93 07-40

info@keithley.de

www.keithley.com

 

Editorial Contact:

PRismaPR UK

Monika Cunnington

Phone: +44-20 8133 6148

monika@prismapr.com

www.prismapr.com

 

PRismaPR

Gabriele Amelunxen

Phone: +49-8106-24 72 33

info@prismapr.com

www.prismapr.com