Test & Tools
  • Technologies
  • More
Test & Tools
Forum Keithley Combines a Curve Tracer’s Range and Simplicity with a Parameter Analyzer’s Flexibility and Precision
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 195 views
  • Users 0 members are here
Related

Keithley Combines a Curve Tracer’s Range and Simplicity with a Parameter Analyzer’s Flexibility and Precision

PRismaPR
PRismaPR over 13 years ago

image

For high resolution image: http://www.ggcomm.com/KEI/curvetracer_HR.jpg or at info@prismapr.com

 

Press Release 18/2012

 

Keithley Combines a Curve Tracer’s Range and Simplicity with a Parameter Analyzer’s Flexibility and Precision

 

Seven flexible parametric curve tracer solutions for power  device characterization

 

Cleveland, Ohio, 22 October 2012   * * *   Keithley Instruments, Inc., a world leader in advanced electrical test instruments and systems, has introduced seven instrumentation, software, and test fixture configurations for parametric curve tracing applications for characterizing high power devices at up to 3,000V and 100A. They’re optimized to provide the industry’s most cost-effective solution for characterizing the growing number of high power semiconductor devices, including those based on silicon carbide (SiC) and gallium nitride (GaN) technology. These systems offer the power required for the vast majority of high power device design and development applications, and are optimized to address the characterization and test needs of research, reliability, failure analysis, and power device applications engineers; power device designers; incoming inspection technicians; and many others. For more information on Keithley’s new parametric curve tracer configurations, visit www.keithley.com/data?asset=57244.

 

Lee Stauffer, a Keithley staff technologist, notes, “Many power device developers have told us they like the dynamic range and ease of use of a traditional curve tracer, but they know they need more flexibility in configuring the measurement channels, as well as the accuracy, capability, and graphical user interface that a modern parametric analyzer offers.”

 

In sharp contrast with solutions that require all instrumentation to be housed in a chassis, all seven Keithley configurations offer the flexibility to add new measurement channels economically as users’ needs evolve, with no need to return the system to the factory to install new hardware. For example, someone could start with an entry level Parametric Curve Tracer, then add the capabilities of additional System SourceMeterRegistered instruments, such as higher voltage and/or higher current, at a later date. Six different System SourceMeter instrument models can be mixed and matched to create the optimum combination of voltage, current and power for the user’s specific needs. Keithley’s TSP LinkRegistered virtual backplane technology makes it easy to incorporate any number of Source-Measure channels, all of which are fully and automatically synchronized with other SourceMeter instruments in the system.

 

All seven configurations include the latest version of Keithley’s ACS (Automated Characterization Suite) Basic Edition software, which supports Keithley’s newest SMUs and takes maximum advantage of the Series 2600B’s TSP-Link connection trigger model, which allows for 500ns trigger synchronization between instruments. This tighter synchronization capability maximizes the high speed pulse mode capabilities of the new Model 2651A and Model 2657A High Power System SourceMeter instruments. The Windows-compatible ACS Basic Edition package provides control and analysis tools well-suited for high power device characterization, including complete parametric test libraries for MOSFETs, BJTs, triacs, diodes, IGBTs, and other device types. The software’s “trace” mode, which uses an on-screen slider control that works much like the power control knob on a traditional analog curve tracer, allows users to control the level of voltage and current levels sourced interactively and to see how the power device responds in real time. The software’s “parametric” mode provides a “fill-in-the-blanks” GUI to configure a test precisely and a comprehensive set of tools for precise parameter extraction. All seven bundles also include all cabling and adapters required for system assembly, as well as a number of sample power devices useful for training and demonstration purposes.

 

Availability

Sales of the parametric curve tracer configurations will begin immediately and units will ship within four weeks ARO.

 

To learn more about the new parametric curve tracer configurations available from Keithley, visit Keithley’s website at www.keithley.com/data?asset=57244. To learn more about Keithley, contact the company at: www.keithley.com.

 

About Keithley Instruments, Inc.

With more than 60 years of measurement expertise, Keithley Instruments has become a world leader in advanced electrical test instruments and systems. Our customers are scientists and engineers in the worldwide electronics industry involved with advanced materials research, semiconductor device development and fabrication, and the production of end products such as portable wireless devices. The value we provide them is a combination of products for their critical measurement needs and a rich understanding of their applications to improve the quality of their products and reduce their cost of test. In 2010, Keithley Instruments joined Tektronix as part of its test and measurement portfolio.

* * *

Reader Contact:            

Keithley Instruments

Phone: +49 89 84 93 07 40

info@keithley.de

www.keithley.com

 

Editorial Contacts:

PRismaPR (UK, Scandinavia, Benelux)

Monika Cunnington

Phone: +44-20 8133 6148

monika@prismapr.com

www.prismapr.com

 

PRismaPR

Gabriele Amelunxen

Phone: +49-8106-24 72 33

info@prismapr.com

www.prismapr.com