Test & Tools
  • Technologies
  • More
Test & Tools
Forum Tektronix Announces 400G Multi-carrier Superchannel Coherent Modulation Analysis
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 229 views
  • Users 0 members are here
  • format
  • testing
  • superchannel
  • tektronix
  • modulation
  • 400g
Related

Tektronix Announces 400G Multi-carrier Superchannel Coherent Modulation Analysis

PRismaPR
PRismaPR over 13 years ago

image

image

image

 

 

Tektronix Announces 400G Multi-carrier Superchannel Coherent Modulation Analysis

 

Tektronix Optical Modulation Analyzers are Industry’s First  to Provide Support for New Superchannel Modulation Format Testing

 

BEAVERTON, Ore., March 13, 2013 – Tektronix, Inc., a leading worldwide provider of test, measurement and monitoring instrumentation, today announced a new software option for its OM4000 optical modulation analyzer series that offers automated test support for 400G multi-carrier coherent optical modulation. This software option will greatly reduce test times for researchers working on 400G and faster coherent optical systems while providing the flexibility to define carrier count, carrier spacing and modulation formats. It also provides compiled carrier measurement results and multi-carrier visualization for integrated analysis.

 

The new software is available to Tektronix customers as Option MCS on the OM4106D Coherent Lightwave Signal Analyzer and OM1106 Coherent Lightwave Signal Analyzer Software. The OM4106D is tightly integrated with Tektronix DPO70000D Series 33 GHz oscilloscopes and uses coherent detection to acquire fiber signals carrying up to 240 Gb/sec per wavelength.

 

“The explosive growth of mobile and cloud computing continues to drive long-haul optical communications bandwidth demands, leading to new designs which leverage existing infrastructure using coherent optical technology,” said Brian Reich, general manager Performance Oscilloscopes, Tektronix. “We see 400G as the next big milestone and superchannel technology as the most likely winner, at least in the near term. This new software will go a long way toward helping to advance multi-carrier modulation methodologies as new standards emerge.”

 

Multi-carrier 400G Gaining Support

With 100G now heading into deployment, network equipment manufacturers are investigating ways to achieve networks speeds of 400G and beyond. Instead of simply increasing the symbol rate of a single carrier, one proposal gaining momentum is to transmit in parallel by using multiple carriers at lower individual rates. Multi-carrier systems such as this have been dubbed superchannels. 

 

There is currently no industry consensus on how to build superchannels. Vendors differ on characteristics as basic as carrier count and carrier spacing to what modulation format should be used. Therefore, a measurement system must have the flexibility to adapt to all these formats. With Option MCS, Tektronix is the industry’s first test supplier to offer multi-carrier or superchannel support.

 

Fast, Automated Results

Option MCS software is designed for optimum ease-of-use and flexibility. To launch tests, the user simply enters multi-carrier variables such as number of carriers, carrier spacing, and modulation format in a simple table. The software automatically steps through each carrier; setting up the local oscillator and measurement parameters based on the information entered into the carrier information table. When all measurements are complete, the system provides the results from all carriers side-by-side for easy correlation and quick identification of problems.

 

Pricing & Availability

Option MCS will be available for £6,470 / starting at €7,770 and will operate on new or existing OM4106D systems beginning May 30, 2013.

 

Wondering what else Tektronix is up to? Check out the Tektronix Bandwidth Banter blog and stay up to date on the latest news from Tektronix on Twitter and Facebook.

 

About Tektronix

For more than sixty-five years, engineers have turned to Tektronix for test, measurement and monitoring solutions to solve design challenges, improve productivity and dramatically reduce time to market. Tektronix is a leading supplier of test equipment for engineers focused on electronic design, manufacturing, and advanced technology development. Headquartered in Beaverton, Oregon, Tektronix serves customers worldwide and offers award-winning service and support. Stay on the leading edge at www.tektronix.com.

# # #

Tektronix is a registered trademark of Tektronix, Inc. All other trade names referenced are the service marks, trademarks or registered trademarks of their respective companies.

 

Reader Contact:           

Tektronix

Barbara Rodrigues

Phone: +44-1 344 392 229

barbara.rodrigues@tektronix.com

www.tektronix.com

 

Editorial Contacts:

PRismaPR (UK)

Monika Cunnington

Phone: +44-20 8133 6148

monika@prismapr.com

www.prismapr.com

 

 

PRismaPR

Gabriele Amelunxen

Phone: +49-8106-24 72 33

info@prismapr.com

www.prismapr.com