Test & Tools
  • Technologies
  • More
Test & Tools
Forum Keithley Adds High Power Wafer-Level Testing to Automated Characterization Suite Software
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 480 views
  • Users 0 members are here
  • test
  • current
  • 2651a
  • testing
  • instruments
  • wafer-level
  • &
  • v5
  • and
  • voltage
  • 2657a
  • keithley
  • measurement
  • smu
  • high
  • acs
  • model
  • power
  • sourcemeter®
  • system
Related

Keithley Adds High Power Wafer-Level Testing to Automated Characterization Suite Software

PRismaPR
PRismaPR over 13 years ago

image

 

For high resolution image: http://www.ggcomm.com/KEI/ACS/prober_control_utility.jpg

or at info@prismapr.com

 

Press Release 1/2013

 

Keithley Adds High Power Wafer-Level Testing to Automated Characterization Suite Software

 

ACS V5.0 is latest addition to Keithley’s line of high power semiconductor test solutions

 

Cleveland, Ohio, 26 March 2013   * * *   Keithley Instruments, Inc., a world leader in advanced electrical test instruments and systems, announces enhancements to its Au-tomated Characterization Suite (ACS) software that support its expanding family of high power semiconductor characterization solutions. The ACS package is optimized for au-tomated wafer-level parameter test applications, including automated characterization, reliability analysis, and known good die testing. The ACS V5.0 update specifically lever-ages the high power capabilities of Keithley’s Model 2651A (high current) and Model 2657A (high voltage) System SourceMeterRegistered SMU instruments to enable automated wa-fer-level testing of high power semiconductor devices like power MOSFETs, IGBTs, BJTs, diodes, etc. To learn more, visit http://www.keithley.com/products/semiconductor/characterizationsoftware.

 

Keithley has incorporated a variety of enhancements into ACS V5.0:

• High power device libraries designed for use with the Models 2651A (up to 50A or 100A when connecting two units) and 2657A (up to 3,000V) System SourceMeter SMU instruments that support testing multi-terminal power components in conjunction with lower power Series 2600B SourceMeter SMU instruments or the Model 4200-SCS Parameter Analyzer to speed and simplify creating modules and sequences for testing power semiconductor devices like power MOSFETs, IGBTs, BJTs, diodes, etc.

• Support for hardware scan, recognition, and configuration management of the high power Models 2651A and 2657A so users can quickly connect these instru-ments to a PC, confirm connectivity, and begin testing.

• Support for Series 2600 SMU instruments equipped with the TSP-LinkRegistered inter-unit communication bus, leveraging the on-board test script processor (TSPRegistered) tech-nology for a multi-processor environment that provides high parallel throughput while speeding and simplifying test project development.

• Sample projects for tests such as high voltage wafer level reliability (WLR) that  build on the wide range of low power reliability test capabilities provided in earlier ACS releases, providing users with an excellent starting point for creating or modifying new tests quickly.

• Support for the ±200V C-V capability of the Model 4200-CVU-PWR C-V Power Package option for the Model 4200-SCS Parameter Analyzer to provide a broad range of I-V and C-V measurement capability for full characterization of semicon-ductor power components.

 

ACS Background

ACS combines multiple instruments into a unified test environment optimized for flexibil-ity, speed, and productivity in testing and analysis. Its intuitive GUI simplifies configuring test instrumentation, setting measurement parameters, making I V measurements, and displaying results. Users can go from creating a new test setup to characterizing new devices in a fraction of the time required by older test development approaches. Just as important, ACS provides all the tools needed to set up tests, analyze data, and export results—without ever leaving the ACS environment. ACS is designed for testing with semi and fully automatic probers; Keithley also offers ACS Basic Edition software for performing semiconductor device characterization with manual probers or test fixtures.

 

Availability

ACS V5.0 is available with a number of Keithley characterization instrument and system configurations. Users of earlier versions should contact their representative for assistance regarding ACS upgrades.

 

For More Information

Visit http://www.keithley.com/products/semiconductor/characterizationsoftware or contact the company at: www.keithley.com.

 

About Keithley Instruments, Inc.

With more than 60 years of measurement expertise, Keithley Instruments has become a world leader in advanced electrical test instruments and systems. Our customers are scientists and engineers in the worldwide electronics industry involved with advanced materials research, semiconductor device development and fabrication, and the production of end products such as portable wireless devices. The value we provide them is a combination of products for their critical measurement needs and a rich understanding of their applications to improve the quality of their products and reduce their cost of test. In 2010, Keithley Instruments joined Tektronix as part of its test and measurement portfolio.

 

* * *

 

Reader Contact:

Keithley Instruments

Phone: +49-89-84 93 07-40

info@keithley.de

www.keithley.com

 

Editorial Contacts:

PRismaPR (UK, Scandinavia & Benelux)

Monika Cunnington

Phone: +44-20 8133 6148

monika@prismapr.com

www.prismapr.com

 

PRismaPR

Gabriele Amelunxen

Phone: +49-8106-24 72 33

info@prismapr.com

www.prismapr.com