Test & Tools
  • Technologies
  • More
Test & Tools
Forum Recommendations for an Oscilloscope
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 52 replies
  • Subscribers 393 subscribers
  • Views 10428 views
  • Users 0 members are here
  • oscilliscope
  • robotics
  • beagle_black
  • rasperry_pi
Related

Recommendations for an Oscilloscope

interested1
interested1 over 13 years ago

Hello Everyone,

  I am in the market for my first oscilloscope.  I have used oscilloscopes before but not really taken to writing down the specs of the device or constructing exactly what I want in a scope.  To date I have gotten by without the device, but I now am in a good financial spot and the purchase of a sub-$500 'scope is reasonable provided I obtain some guide.  My requirements are rather vague, but can be generalized as a desire to purchase a scope that provides enough data sampling for robotics projects --I currently work with the Raspberry Pi and the Beagle Bone Black.  I am confident that the previous curtailment didn't reduce the field all that much, so I reiterate, I am willing to spend ~$500 on a scope, so please no suggestions of thousand dollar scopes.  I want something, which in the breadth of product offerings is probably quite basic, but nonetheless I would like to be able to have a scope to test my robotics and embedded Linux boards with...

 

A friend of mine suggested that I purchase something akin to the Instek GDS-1052-U Digital Storage Oscilloscope, 2 Channel, Color LCD, 50MHz, 250MS/s with USB or a less expensive USB Oscilloscope - MSO-19 Considering his knowledge of what I might be using the scope for, likely an intimacy more than I am expressing in my description for usage, I remain inquisitive for advice.  I mention these products and provide links only to better aid my previously vague explanation for my prospective usage.

 

As a final curtailment, I would really love to get a scope that I could use with Linux rather than Winblow$ as I really only use Linux or OSX boxes these days.  I am confident there are products that are not Winblow$ only, but the two scopes my buddy suggests both seem to urge my adoption of a OS that I want not part in!

 

Thank you for your responses and if I can better explain what I hope to accomplish with a scope please explain to me what I can provide to better resolve the specification I (unwittingly) desire in a scope.  I apologizes again for being less than committal or precise, but you have to begin from somewhere and my point of departure is that I would like a scope... thanks for working with me on a request that is perhaps an incomplete formulation.

 

David

 

P.S. I did try to search for a discussion on this topic; however, I couldn't find anything within the last year or two.  I figure this is a question that everyone has at some point and so why not posit the issue and revisit.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to interested1 +4
    Hi David, the 100MHz is even more simple these days and should work on all scopes: http://www.eevblog.com/forum/blog/changing-the-rigol-ds1052e-to-ds1102e-using-usb-the-dummy-guide/msg187918/#msg187918…
  • nermash
    nermash over 13 years ago +3
    If your budget is set at 500$ max, then it's no brainier. After many posts on EEVblog forum, there seem to be consensus that these budget dsos are best: Rigol DS1052E, Owon SDS7102, Siglent SDS1102 CML…
  • vsluiter
    vsluiter over 13 years ago +3
    Hey David (Scheltema -> Dutch roots?) I've been using the Rigol scope for a few years now, and -for its budget- it's really great. A few fellow engineers bought USB scopes years ago, all of which ended…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Forget the war of USB or Not USB, many of the highgrade solutions use USB!

    Take a look at QA100 https://www.quantasylum.com/content/Products/QA100.aspx

     

    I have used this scope for more than a year and it is a dream to work with it.

     

    In embedded MSO you dont need 600V probes, often is the reality -10V-+10V and the scope are made to share clock with the other instruments.

     

    " The QA100 is a PC-based oscilloscope for Windows XP, Vista, Windows 8 and later. This means the PC is used to collect, display and analyze your data. The connection to your PC happens over a USB High Speed link, and the high-speed transfer rate (up to 480Mbps) means screen update rates rivaling video games are possible. It also means you are looking at data on a high resolution desktop monitor in 32-bit color instead of a low-cost LCD panel that can display limited resolution. And best yet, your mouse and keyboard can drive the user interface and accomplish tasks in a fraction of the time it takes on a standalone scope. Sharing data has never been easier, with the ability to display comments directly on the screen fixed at a certain point in time. Add a note to the capture, copy the screen, drop it in an email and explain the problem to other engineers in less time than ever before."

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Forget the war of USB or Not USB, many of the highgrade solutions use USB!

    Take a look at QA100 https://www.quantasylum.com/content/Products/QA100.aspx

     

    I have used this scope for more than a year and it is a dream to work with it.

     

    In embedded MSO you dont need 600V probes, often is the reality -10V-+10V and the scope are made to share clock with the other instruments.

     

    " The QA100 is a PC-based oscilloscope for Windows XP, Vista, Windows 8 and later. This means the PC is used to collect, display and analyze your data. The connection to your PC happens over a USB High Speed link, and the high-speed transfer rate (up to 480Mbps) means screen update rates rivaling video games are possible. It also means you are looking at data on a high resolution desktop monitor in 32-bit color instead of a low-cost LCD panel that can display limited resolution. And best yet, your mouse and keyboard can drive the user interface and accomplish tasks in a fraction of the time it takes on a standalone scope. Sharing data has never been easier, with the ability to display comments directly on the screen fixed at a certain point in time. Add a note to the capture, copy the screen, drop it in an email and explain the problem to other engineers in less time than ever before."

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • aat14
    aat14 over 12 years ago in reply to e14 Contributor

    You will find an overview of all oscilloscope manufacturers including USB scopes on the website http://www.oscopes.info/

    Please look for the "Market" tab.

    This oscilloscope information platform provides also many links to websites explaining how an oscilloscope works, how to use it and how to do simple measurements.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to aat14

    Thanks for that it looks interesting ..however I did worry when a Lecroy was on the front page image