Test & Tools
  • Technologies
  • More
Test & Tools
Forum Recommendations for an Oscilloscope
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 52 replies
  • Subscribers 393 subscribers
  • Views 10428 views
  • Users 0 members are here
  • oscilliscope
  • robotics
  • beagle_black
  • rasperry_pi
Related

Recommendations for an Oscilloscope

interested1
interested1 over 13 years ago

Hello Everyone,

  I am in the market for my first oscilloscope.  I have used oscilloscopes before but not really taken to writing down the specs of the device or constructing exactly what I want in a scope.  To date I have gotten by without the device, but I now am in a good financial spot and the purchase of a sub-$500 'scope is reasonable provided I obtain some guide.  My requirements are rather vague, but can be generalized as a desire to purchase a scope that provides enough data sampling for robotics projects --I currently work with the Raspberry Pi and the Beagle Bone Black.  I am confident that the previous curtailment didn't reduce the field all that much, so I reiterate, I am willing to spend ~$500 on a scope, so please no suggestions of thousand dollar scopes.  I want something, which in the breadth of product offerings is probably quite basic, but nonetheless I would like to be able to have a scope to test my robotics and embedded Linux boards with...

 

A friend of mine suggested that I purchase something akin to the Instek GDS-1052-U Digital Storage Oscilloscope, 2 Channel, Color LCD, 50MHz, 250MS/s with USB or a less expensive USB Oscilloscope - MSO-19 Considering his knowledge of what I might be using the scope for, likely an intimacy more than I am expressing in my description for usage, I remain inquisitive for advice.  I mention these products and provide links only to better aid my previously vague explanation for my prospective usage.

 

As a final curtailment, I would really love to get a scope that I could use with Linux rather than Winblow$ as I really only use Linux or OSX boxes these days.  I am confident there are products that are not Winblow$ only, but the two scopes my buddy suggests both seem to urge my adoption of a OS that I want not part in!

 

Thank you for your responses and if I can better explain what I hope to accomplish with a scope please explain to me what I can provide to better resolve the specification I (unwittingly) desire in a scope.  I apologizes again for being less than committal or precise, but you have to begin from somewhere and my point of departure is that I would like a scope... thanks for working with me on a request that is perhaps an incomplete formulation.

 

David

 

P.S. I did try to search for a discussion on this topic; however, I couldn't find anything within the last year or two.  I figure this is a question that everyone has at some point and so why not posit the issue and revisit.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to interested1 +4
    Hi David, the 100MHz is even more simple these days and should work on all scopes: http://www.eevblog.com/forum/blog/changing-the-rigol-ds1052e-to-ds1102e-using-usb-the-dummy-guide/msg187918/#msg187918…
  • nermash
    nermash over 13 years ago +3
    If your budget is set at 500$ max, then it's no brainier. After many posts on EEVblog forum, there seem to be consensus that these budget dsos are best: Rigol DS1052E, Owon SDS7102, Siglent SDS1102 CML…
  • vsluiter
    vsluiter over 13 years ago +3
    Hey David (Scheltema -> Dutch roots?) I've been using the Rigol scope for a few years now, and -for its budget- it's really great. A few fellow engineers bought USB scopes years ago, all of which ended…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    I have bought an Analog Arts model SA925 a USB type oscilloscope (www.analogarts.com). I bought the device mostly for its spectrum analyzer capability. For about $300 it was the price that initially attracted my attention. Although it has about 200 MHz bandwidth, I hardly need that level of performance. Overall, I am happy with its performance. Nevertheless, I strongly recommend to you to meticulously read the specification of any device you planning to buy. So you do not fall victim to marketing gimmicks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 11 years ago in reply to e14 Contributor

    Hi Bernard,

    About the specifications: this scope has a max sampling rate (single shot) of 125MHz, it advertises as 200MHz "real" sample rate, an "effective sample rate" of 100GHz (which means you're taking more samples of a signal, with a variable trigger delay. The signal should be repetitive) and an analog bandwith of 200MHz.

    To me those numbers do not compute. For a single shot trigger the analog bandwith can be no higher than ~50Mhz, taking Nyquist into account without safety margins.


    I think that these guys also let the marketing misuse the specs....


    BTW: someone mentioned the Rigol DS1054Z, I bought it and received it two weeks ago. Haven't used it much yet, but it's certainly worth its money!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to vsluiter

    Hi Vsluiter,

                Well, If you are talking about the criteria imposed by the Nyquist theorem, who could argue with that. However, for a repetitive signal that criteria can be manipulated. Analog Arts oscilloscope correctly displays 150 MHz sine-wave in my set up. If you wish I can email you a plot of the signal. Now, that you mention it though, I do find it quite impressive. I am not quite sure how they do it. I am familiar with different methods of signal reconstructions, but none of them could work for really high frequencies since you need to generate extremely small delays, which are impossible. The application engineer, whom I talked to, was not open about how they do it, stating they have a patent pending on their technique. He did mention they somehow calculate the frequency of the signal (to .1ppm) before it is reconstructed. Anyway, for the money I paid, i am quite happy with the unit. For a lower price, I am getting higher bandwidth and spectrum analyzer feature.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    The way it works is well documented (known as equivalent time sampling). It is useful in the circumstance that the signal is repetitive as you say, which is a limitation.

    The spectrum analyzer feature is offered on many oscilloscopes nowadays.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 11 years ago in reply to shabaz

    Thanks for that link! There's also an explanation here: http://www.signalrecovery.com/Support-Center/FAQ/FAQ-Hardware/Effective-Sampling-Rate.aspx

    Still, the numbers do not compute well to me; a single shot update with a different sample rate than the "real sample rate"? And what about undersampling / aliasing? The analog bandwiith will allow signals to pass that cannot be correctly visualized on screen, and you won't be able to see whether you're undersampling or not.

     

    To be honest: I haven't checked my own scope's data so thoroughly, but I found these numbers to be raising some questions.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • vsluiter
    vsluiter over 11 years ago in reply to shabaz

    Thanks for that link! There's also an explanation here: http://www.signalrecovery.com/Support-Center/FAQ/FAQ-Hardware/Effective-Sampling-Rate.aspx

    Still, the numbers do not compute well to me; a single shot update with a different sample rate than the "real sample rate"? And what about undersampling / aliasing? The analog bandwiith will allow signals to pass that cannot be correctly visualized on screen, and you won't be able to see whether you're undersampling or not.

     

    To be honest: I haven't checked my own scope's data so thoroughly, but I found these numbers to be raising some questions.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 11 years ago in reply to vsluiter

    Hi Victor!

     

    I read an article a while back (sadly I can't remember where now) but basically although equivalent time sampling is highly useful, doing it well is a hard thing (requires very low jitter from the delayed periodic signal (generated from the input signal) which will cause the ADC to sample. And, as you suggest, there is the risk of misinterpreting the output when the signal actually isn't periodic, or only has some periodic elements - the resultant waveform display quality could look wrong for any of these cases (jitter, non-periodic or periodic with non-periodic components) and probably others too if I could remember it in detail.

    Fpga4fun (terrible site, I can't recommend their products because they have expensive "development" boards that they do not supply the entire schematics nor entire source code for) have a design using a 100MSPS ADC which uses equivalent time sampling to achieve higher than 50MHz waveform capture. They have a block diagram showing the periodic output from their ADC boards (no schematic of course..).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    I think this is the "secret sauce" in many scope designs and I'm sure that most signals tend to repeat at some point (exactly where seems to the the art).

    How exactly do you tell when the scope is making a good job of this and when is it just making funny pictures for your entertainment  seems to be even harder to decipher.

     

    OT: I was looking at the DVI output generator stuff sometime ago on FPGAs4fun and they do have some VHDL, have you tried any of their stuff?? I'm shure there is something missing on many of them?!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    After I discovered source was incomplete for some of their projects, and they stated that some parts were closed source (and their refusal to supply schematics) I didn't use their boards any more to be honest. I'm glad there are plenty of higher quality alternatives.


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    Indeed, I agree about the quality of trace thing. Nowadays it is well established that some particular math manipulations need to be done to convert the raw samples into a waveform and that you can't just dump to a screen and hope for the best, but probably early products, and possibly nowadays for some of the very small outfits, may not do this.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    At the end of the day there is no substitute for a stupidly fast ADC image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to vsluiter

    Thanks Shabaz. Well, as I mentioned I am familiar with the technique you mention. But achieving  consistent 10 picosecond time , 100 GHz, resolution (what Analog Arts oscilloscope does) is very challenging. I would appreciate any explanation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Bernard,

     

    I'm afraid I can't justify or explain it - perhaps Analog Arts may have a paper published where they explain their design?

    As you may know, a sample rate of 2.5 times the analog bandwidth is all that is needed to reproduce (with accuracy) the input waveform.

    As a result, the advertisement of 100GHz effective sample rate on a 200MHz analog bandwidth and 125MHz real sample rate scope is

    "marketing bluster" perhaps.

    Furthermore bear in mind, if there is jitter on their 10ps time between samples (which is conveniently ignored in their specs), that

    results in a bad (i.e. misleading) shaped waveform.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz

    I recently bought from Analog Arts. Their devices perform as advertised.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi! Welcome to the forum.

     

    Personally I wouldn't buy it. Just a personal, subjective opinion of course.

     

    This is because they are quite silent on waveform quality because it is well known that if there is jitter inside their product (conveniently absent from their specification) then

    equivalent time sampling will produce a poor result. Furthermore, equivalent time sampling only works well when the input signal has no  glitches or jitter too, let alone needing to be periodic. That's a fact, well established.

     

    The 125Msps of the Analog Arts oscilloscope only provides 50MHz of real-time bandwidth (i.e. usable for non-periodic signals). That's a fact too and not a subjective opinion of course.

     

    For near-similar amounts of money to the Analog Arts 125Msps 2-channel USB scope, it is possible to get a full-blown 4-channel 1Gsps oscilloscope with the same real-time bandwidth (DS1054Z) and built-in display, an order of magnitude more memory, and 30k waveforms updates per second, or a 2-channel 250Msps USB scope with twice the real-time bandwidth(Tenma  72-1016572-10165 of the Analog Arts product(i.e for non-periodic signals

     

    I'm not saying the Analog Arts product is bad, but what I am saying is that it is seems to be clearly easy to recommend alternatives which appear better, without looking too hard. This is just an opinion.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to shabaz

    Just noticed someone did a review and teardown of an Analog Arts 'scope. I've not watched it (got other things to do ; ) but a quick scan of the comments was interesting.

    https://www.youtube.com/watch?v=F-1uA4Iwce8