Test & Tools
  • Technologies
  • More
Test & Tools
Forum Keithley Provides Full Wafer-Level Support Including High Voltage Capacitance-Voltage Testing
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 360 views
  • Users 0 members are here
  • test
  • instruments
  • 8020
  • &
  • keithley
  • measurement
  • high
  • curve
  • interface
  • power
  • tracer
Related

Keithley Provides Full Wafer-Level Support Including High Voltage Capacitance-Voltage Testing

prisma
prisma over 11 years ago

image

Keithley Provides Full Wafer-Level Support Including High Voltage Capacitance-Voltage Testing for Its Parametric Curve Tracer Configurations

Reduces cabling confusion, prevents connection errors, improves safety in power device testing

 

CLEVELAND, OH – October 2014 – Keithley Instruments, Inc., a world leader in advanced electrical test instruments and systems, today introduced new enhancements to its Parametric Curve Tracer (PTC) configurations that incorporate high power SourceMeterRegistered Source Measure Unit (SMU) instruments. For test engineers responsible for configuring high power semiconductor test systems, the new Keithley Model 8020 High Power Interface Panel improves connectivity and simplifies complex measurements like high voltage capacitance-voltage (C-V) measurements. The Model 8020 reduces set-up times, minimizes opportunities for connection errors, improves operator and test hardware protection, and increases users’ confidence in the accuracy of their results. For more information, watch Keithley’s introductory video on the topic.

Characterizing high power semiconductor devices like power MOSFETs, IGBTs, diodes, etc. involves several different types of measurements: on-state (high current current-voltage), off-state (high voltage current-voltage), and capacitance-voltage (C-V) at high bias voltages. However, each of these measurements requires the use of different instrumentation, cabling, connectors, and probes (for wafer-level testing) or test fixtures (for packaged device testing).

In the past, no standardized solutions for combining high power instruments, interconnects, and probers/test fixtures suitable for all three test types in the same test station were commercially available. When changing from one measurement type to another, high power test system users once had to change the type of cables used manually, as well as critical hardware in the signal path between the device under test and the test instrumentation. High voltage C-V testing was particularly complicated because no standard or reliable measurement setups and methods were established. Test engineers often had to develop their own connection solutions through trial and error, which is not only expensive and time-consuming but can create an unsafe work environment, given the high outputs involved in testing power devices.

The configurable Model 8020 High Power Interface Panel allows test engineers to select the options that match their system’s probe station, positioners, or fixture. It also improves safety for both users and any low power SMU instruments in the system, simplifies incorporating different combinations of instruments, as well as taking the confusion out of adding elements like series resistors and bias tees to the signal path.

The Model 8020 simplifies changing from one measurement type to the next by allowing test engineers to connect all measurement instruments to it at once, making further connection changes unnecessary. When the Model 8020 is configured with optional C-V bias tees on the system’s 3kV and 200V channels, it acts as a high performance I-V/C-V switch, allowing users to perform both I-V and C-V testing without re-cabling.

The Model 8020 provides input connections for Keithley Model 2657A (3kV) and 2651A (50A) High Power SourceMeter SMU instruments, Model 2636B and 2612B SourceMeter SMU instruments, and Model PCT-CVU Multi-frequency C-V Meter. Various user-configurable output connectors are available to accommodate almost any probe station.

The Model PCT-CVU Multi-frequency C-V Meter, which supports C-V measurements from 10kHz to 2MHz, can be used to upgrade any Keithley PCT configuration to include 2- and 3-terminal capacitance measurements. It is designed for use with the new Model CVU-200-KIT bias tee kit to extend the voltage bias to 200V or the Model CVU-3K-KIT bias tee kit to extend it to 3kV to support both AC and DC testing in the Model 8010 or other high power test fixture.

The latest version (V 2.1) of Keithley’s ACS Basic Edition Component Test Software expands the package’s support for I-V and C-V measurements on devices like power MOSFETS, IGBTs, diodes, etc. It complements the advanced C‑V measurements the Model 8020 and new bias tee kits make possible.

Pricing and Availability
The Model 8020 High Power Interface Panel and other Parametric Curve Tracer System enhancements are configurable products. Pricing depends on the specific configuration selected. Orders can be accepted beginning on October 1, 2014, with availability in 6–10 weeks.

For More Information
More information on the Model 8020 High Power Interface Panel is available at www.keithley.com/data?asset=57244. To learn more about Keithley, contact the company at: www.keithley.com.

 

About Keithley Instruments, Inc.

With more than 60 years of measurement expertise, Keithley Instruments has become a world leader in advanced electrical test instruments and systems. Our customers are scientists and engineers in the worldwide electronics industry involved with advanced materials research, semiconductor device development and fabrication, and the production of end products such as portable wireless devices. The value we provide them is a combination of products for their critical measurement needs and a rich understanding of their applications to improve the quality of their products and reduce their cost of test. In 2010, Keithley Instruments joined Tektronix as part of its test and measurement portfolio.

* * *

Products and company names listed are trademarks or trade names of their respective companies.

 

Reader Contact:                       Editorial Contacts:

Keithley, a Tektronix company

PRismaPR (UK)

PRismaPR

Phone: +49-89-84 93 07-40

Monika Cunnington

Gabriele Amelunxen

info@keithley.de

  1. www.keithley.com

Phone: +44-20 8133 6148

monika@prismapr.com

  1. www.prismapr.com

Phone: +49-8106-24 72 33

info@prismapr.com

  1. www.prismapr.com