Test & Tools
  • Technologies
  • More
Test & Tools
Forum Feasability of Adding a Second Parallel Darlington?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 388 subscribers
  • Views 6428 views
  • Users 0 members are here
  • control
  • voltage
  • darlington
Related

Feasability of Adding a Second Parallel Darlington?

jw0752
jw0752 over 11 years ago

        I am currently working on a small circuit that controls the voltage to an electric dental lab handpiece. Please see the schematic below. This circuit has had a chronic problem with failure of the TIP-122 Darlington. The problem arises when the handpiece operator applies pressure which adds load to the motor and the motor then demands more current from the circuit. This circuit is very simple with basically no overload protection. The original design did not even have a flyback diode across the motor. My question is if it is practical to add another TIP-122 Darlington in parallel with the first one in order to improve current handling capacity. Does anyone have any experience with this type of modification? I also have a curiosity codicil to my question. If it is practical to add another Darlington, what would be the limiting factor to how many parallel Darlingtons can be added in this way? Any insights would be appreciated.

John

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    Hi John, a very good question, and the answer is fairly straight forward If the Darlington is getting overloaded due to exceeding the current limit of the Darlington then an additional one in parallel…
  • vsluiter
    vsluiter over 11 years ago +1
    Hi John, You say that the circuit has no short circuit protection, but the 3k resistor with a hFE of 1000 means some current limit: The supply is 36×√2 -(1.2V diode bridge drop) ≅ 50V. At startup the motor…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    Hi John, a very good question, and the answer is fairly straight forward

     

    If the Darlington is getting overloaded due to exceeding the current limit of the Darlington then an additional one in parallel would help to fix the problem (or two, or three image ), you must limit the base current separately though with its own 3K resistor and the emitter current through its own 1R resistor, this will prevent one Darlington hogging all the glory.The LM317 has more than enough drive to handle it

     

    basically the Darlington's are acting as emitter followers and will be outputting about 2 diode (B-E junctions) drops less than the output of the LM317 (So about 1.5V ish), as long as you don't exceed the output current of the LM317 or the power supply, add as many as you like in the way I described above. The other possibility is the current capability of the Darlington is not being exceeded but the heat sink is inadequate if the additional devices have their own then this should fix it but if not you may still experience issues so check the heat sink before investing in the additional drivers.

     

    The other option if room is an issue and the heat sink is ok, is to replace the current Darlington with a bigger more powerful one

     

    Hope this helps

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter, It certainly did. This is exactly the information that I was looking for. I really appreciate your taking the time to give me the details. I can see how important it is to use seperate base and emitter resistors. I ultimately took your secondary advice and searched for a slightly heftier Darlington in the same TO 220 casing and I will use that. Thanks again for your wisdom.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to jw0752

    More than welcome John

     

    regards

     

    peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to jw0752

    More than welcome John

     

    regards

     

    peter