Test & Tools
  • Technologies
  • More
Test & Tools
Forum Feasability of Adding a Second Parallel Darlington?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 388 subscribers
  • Views 6438 views
  • Users 0 members are here
  • control
  • voltage
  • darlington
Related

Feasability of Adding a Second Parallel Darlington?

jw0752
jw0752 over 11 years ago

        I am currently working on a small circuit that controls the voltage to an electric dental lab handpiece. Please see the schematic below. This circuit has had a chronic problem with failure of the TIP-122 Darlington. The problem arises when the handpiece operator applies pressure which adds load to the motor and the motor then demands more current from the circuit. This circuit is very simple with basically no overload protection. The original design did not even have a flyback diode across the motor. My question is if it is practical to add another TIP-122 Darlington in parallel with the first one in order to improve current handling capacity. Does anyone have any experience with this type of modification? I also have a curiosity codicil to my question. If it is practical to add another Darlington, what would be the limiting factor to how many parallel Darlingtons can be added in this way? Any insights would be appreciated.

John

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    Hi John, a very good question, and the answer is fairly straight forward If the Darlington is getting overloaded due to exceeding the current limit of the Darlington then an additional one in parallel…
  • vsluiter
    vsluiter over 11 years ago +1
    Hi John, You say that the circuit has no short circuit protection, but the 3k resistor with a hFE of 1000 means some current limit: The supply is 36×√2 -(1.2V diode bridge drop) ≅ 50V. At startup the motor…
Parents
  • mcb1
    mcb1 over 11 years ago

    John

    a quick answer before heading to work.

     

    I'm not surprised the darlington fails.

    This is only working because there is a drop across the series 1 ohm resistor.

     

    The transistor is turning on, then its emitter is rising such that it turns off, and its always operating in never really ON or OFF mode so it will heat up.

    My suggestion is to look at putting the motor and diode in the collector, and then tweak the regulator to detect the voltage across the 1 ohm, which will be between the emitter and ground.

     

    Adding a second darlington might load share, but the basics are wrong.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to mcb1

    If you do that, you will change it from being a current amplifier (Keeping the voltage regulated based on the two adjustments on the LM linear regulator, im assuming a course and fine adjustment)

     

     

     

    After the change the transistor would be working as a voltage amplifier and very dependent on temp and other factors

     

     

     

    The circuit John posted is a classic circuit to boost the capacity of a regulator, I have been using variations of it for over 30 years with no issues

     

     

     

    Look at any linear regulator circuit and you will see this, think of the LM as a voltage reference with a higher then normal output ability, the pattern is also the same as almost every single linear bench power supply out there just without current limiting so I don’t think John needs to change the topology of the design

     

     

     

    The rising and turning off in this case is supposed to happen and is the negative feedback, the voltage gain is ideally 1. With a massive current gain, look at the WIKI on common collector BJT for more details and a fuller description

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to mcb1

    If you do that, you will change it from being a current amplifier (Keeping the voltage regulated based on the two adjustments on the LM linear regulator, im assuming a course and fine adjustment)

     

     

     

    After the change the transistor would be working as a voltage amplifier and very dependent on temp and other factors

     

     

     

    The circuit John posted is a classic circuit to boost the capacity of a regulator, I have been using variations of it for over 30 years with no issues

     

     

     

    Look at any linear regulator circuit and you will see this, think of the LM as a voltage reference with a higher then normal output ability, the pattern is also the same as almost every single linear bench power supply out there just without current limiting so I don’t think John needs to change the topology of the design

     

     

     

    The rising and turning off in this case is supposed to happen and is the negative feedback, the voltage gain is ideally 1. With a massive current gain, look at the WIKI on common collector BJT for more details and a fuller description

     

     

     

    Peter